AM261x MCU+ SDK  26.00.00

Introduction

This module has APIs for USB device driver. See this page, USB, for using USB using tinyUSB APIs

Sub Modules

 APIs for Synopsys driver
 

Files

file  usb_init.h
 This file contains USB initialization APIs.
 
file  device_wrapper.h
 This file contains USB device wrapper APIs.
 

Data Structures

struct  usb_handle_t
 Structure representing the USB device handle. More...
 

Functions

void USB_init ()
 This function initializes the USB driver. More...
 
void USB_dwcTask ()
 This function handles triggered events from the USB driver. More...
 
void USB_deinit ()
 This function De-Initialization USB driver. More...
 
UsbPhy_ret_t usb_phy_power_sequence (void)
 Performs the USB PHY power-on sequence. More...
 
void USB_configureInterrupt (uint32_t intr)
 This function configures the interrupt. More...
 
void USB_disableInterrupt (uint32_t intr)
 This function disables the interrupt. More...
 
void USB_clearInterrupt (void)
 This function clears the MAIN0 interrupt. More...
 

Enumerations

enum  UsbPhy_ret_t { USB_PHY_OK = 0x01U, USB_PHY_ERR = 0x02U }
 This enumeration defines the return status for USB PHY. More...
 

Enumeration Type Documentation

◆ UsbPhy_ret_t

This enumeration defines the return status for USB PHY.

Enumerator
USB_PHY_OK 
USB_PHY_ERR 

Function Documentation

◆ USB_init()

void USB_init ( )

This function initializes the USB driver.

◆ USB_dwcTask()

void USB_dwcTask ( )

This function handles triggered events from the USB driver.

  • process the events, check for the event type (device, EP or invalid etc) and invokes the appropriate handler

◆ USB_deinit()

void USB_deinit ( )

This function De-Initialization USB driver.

◆ usb_phy_power_sequence()

UsbPhy_ret_t usb_phy_power_sequence ( void  )

Performs the USB PHY power-on sequence.

This function initializes the USB PHY by performing the necessary power-on sequence.

Returns
UsbPhy_ret_t indicating the status of the operation.

◆ USB_configureInterrupt()

void USB_configureInterrupt ( uint32_t  intr)

This function configures the interrupt.

Parameters
intrInterrupt number or identifier. Specifies the interrupt to be handled or configured.

◆ USB_disableInterrupt()

void USB_disableInterrupt ( uint32_t  intr)

This function disables the interrupt.

Parameters
intrInterrupt number or identifier. Specifies the interrupt to be handled or configured.

◆ USB_clearInterrupt()

void USB_clearInterrupt ( void  )

This function clears the MAIN0 interrupt.

Variable Documentation

◆ ep_in_buf

uint8_t ep_in_buf[DWC_MAX_EPS - 1U][DWC_MAX_PACKET_SIZE]
extern

Global buffers for USB IN endpoints. These buffers are used for data transmission from the device to the host.

◆ ep_out_buf

uint8_t ep_out_buf[DWC_MAX_EPS - 1U][DWC_MAX_PACKET_SIZE]
extern

Global buffers for USB OUT endpoints. These buffers are used for data reception from the host to the device.