AM261x MCU+ SDK  26.00.00
device_wrapper.h File Reference

Introduction

This file contains USB device wrapper APIs.

Go to the source code of this file.

Data Structures

struct  usb_handle_t
 Structure representing the USB device handle. More...
 

Macros

#define BOOTPARAM_TIMEOUT_MS   60000U
 

Enumerations

enum  UsbPhy_ret_t { USB_PHY_OK = 0x01U, USB_PHY_ERR = 0x02U }
 This enumeration defines the return status for USB PHY. More...
 

Functions

UsbPhy_ret_t usb_phy_power_sequence (void)
 Performs the USB PHY power-on sequence. More...
 
void USB_configureInterrupt (uint32_t intr)
 This function configures the interrupt. More...
 
void USB_disableInterrupt (uint32_t intr)
 This function disables the interrupt. More...
 
void USB_clearInterrupt (void)
 This function clears the MAIN0 interrupt. More...
 

Variables

uint8_t ep_in_buf [DWC_MAX_EPS - 1U][DWC_MAX_PACKET_SIZE]
 Global buffers for USB IN endpoints. These buffers are used for data transmission from the device to the host. More...
 
uint8_t ep_out_buf [DWC_MAX_EPS - 1U][DWC_MAX_PACKET_SIZE]
 Global buffers for USB OUT endpoints. These buffers are used for data reception from the host to the device. More...
 

Macro Definition Documentation

◆ BOOTPARAM_TIMEOUT_MS

#define BOOTPARAM_TIMEOUT_MS   60000U