AM261x MCU+ SDK  26.00.00

Introduction

These routines handle initialization of the CIL and PCD driver components and the DWC_usb3 controller.

Functions

int dwc_usb3_pcd_init (struct dwc_usb3_device *dev)
 
void dwc_usb3_pcd_remove (struct dwc_usb3_device *dev)
 
int dwc_usb3_pcd_check_snpsid (dwc_usb3_device_t *dev, u32 addr_ofs)
 This routine ensures the device is really a DWC_usb3 controller, by reading and verifying the SNPSID register contents. The value should be 0x5533XXXX, which corresponds to "U3", as in "USB3 version X.XXX". More...
 
int dwc_usb3_pcd_common_init (dwc_usb3_device_t *dev, volatile u8 __iomem *base, const dwc_usb3_core_params_t *core_params)
 This routine is called to initialize the DWC_usb3 CSR data structures. The register addresses in the device structures are initialized from the base address supplied by the caller. The calling routine must make the OS calls to get the base address of the DWC_usb3 controller registers. The core_params argument holds the parameters that specify how the core should be configured. More...
 
void dwc_usb3_pcd_common_remove (dwc_usb3_device_t *dev)
 
void dwc_usb3_pcd_device_init (dwc_usb3_device_t *dev, int soft_reset, int restore)
 This routine initializes the DWC_usb3 controller registers. More...
 
void dwc_usb3_pcd_device_remove (dwc_usb3_device_t *dev)
 This routine deinitializes the DWC_usb3 controller registers. More...
 

Function Documentation

◆ dwc_usb3_pcd_init()

int dwc_usb3_pcd_init ( struct dwc_usb3_device *  dev)

◆ dwc_usb3_pcd_remove()

void dwc_usb3_pcd_remove ( struct dwc_usb3_device *  dev)

◆ dwc_usb3_pcd_check_snpsid()

int dwc_usb3_pcd_check_snpsid ( dwc_usb3_device_t *  dev,
u32  addr_ofs 
)

This routine ensures the device is really a DWC_usb3 controller, by reading and verifying the SNPSID register contents. The value should be 0x5533XXXX, which corresponds to "U3", as in "USB3 version X.XXX".

The SNPSID value is also saved in dev->snpsid for later use in determining if any version-specific operations need to be performed.

This routine should be called before any other initialization routines, to ensure that the dev->snpsid value is set in case any of the other routines need it.

Parameters
devProgramming view of DWC_usb3 controller.
addr_ofsOffset to the Device registers in the CSR space. It is needed because this routine is called early, before the normal register access routines are functional.
Returns
0 if the SNPSID value is valid, -DWC_E_INVALID if not.

◆ dwc_usb3_pcd_common_init()

int dwc_usb3_pcd_common_init ( dwc_usb3_device_t *  dev,
volatile u8 __iomem *  base,
const dwc_usb3_core_params_t *  core_params 
)

This routine is called to initialize the DWC_usb3 CSR data structures. The register addresses in the device structures are initialized from the base address supplied by the caller. The calling routine must make the OS calls to get the base address of the DWC_usb3 controller registers. The core_params argument holds the parameters that specify how the core should be configured.

Parameters
devProgramming view of DWC_usb3 controller.
baseBase address of DWC_usb3 core registers.
core_paramsPointer to the core configuration parameters.
Returns
0 on success, negative error code on failure

◆ dwc_usb3_pcd_common_remove()

void dwc_usb3_pcd_common_remove ( dwc_usb3_device_t *  dev)

This routine frees any allocations made by dwc_usb3_pcd_common_init().

Parameters
devProgramming view of DWC_usb3 controller.

◆ dwc_usb3_pcd_device_init()

void dwc_usb3_pcd_device_init ( dwc_usb3_device_t *  dev,
int  soft_reset,
int  restore 
)

This routine initializes the DWC_usb3 controller registers.

If the soft_reset parameter is true, then this routine must be called in a context that allows dwc_msleep() to be used, because that function is called while waiting for the core to come out of reset.

This routine is called by dwc_usb3_pcd_init() when the driver is loaded, so it normally does not need to be called separately, except in special circumstances, such as when exiting from hibernation.

Parameters
devProgramming view of DWC_usb3 controller.
soft_resetTrue if doing a soft reset of the core.
restoreTrue if restoring register state after hibernation.

◆ dwc_usb3_pcd_device_remove()

void dwc_usb3_pcd_device_remove ( dwc_usb3_device_t *  dev)

This routine deinitializes the DWC_usb3 controller registers.

This routine is called by dwc_usb3_pcd_remove() when the driver is unloaded, so it normally does not need to be called separately,

Parameters
devProgramming view of DWC_usb3 controller.