The basic API functions cover general functionality such as creating, initializing, starting, and deleting an EtherCAT slave object. The slave object is a required input parameter for all other slave API functions. Also supported are API functions to retrieve the slave status and to register status and error handler callback functions.
Functions | |
void | EC_API_SLV_SSC_setLicense (char *pLicense_p, uint8_t length_p) |
Enter license key to run the unlimited version. More... | |
uint32_t | EC_API_SLV_getVersionStr (uint32_t bufLen_p, char *pBuffer_p, uint32_t *pUsedLen_p) |
Get version string. More... | |
uint32_t | EC_API_SLV_getVersionId (uint32_t bufLen_p, char *pBuffer_p, uint32_t *pUsedLen_p) |
Get Version Id (Shasum) More... | |
uint32_t | EC_API_SLV_stackInit (void) |
This is the function to initialize Stack backend. More... | |
EC_API_SLV_SHandle_t * | EC_API_SLV_new (void) |
This is the function to create a new EtherCAT Slave device instance. More... | |
uint32_t | EC_API_SLV_delete (EC_API_SLV_SHandle_t *pEcSlaveApi_p) |
This is the function to delete a created adapter. More... | |
uint32_t | EC_API_SLV_init (EC_API_SLV_SHandle_t *pEcSlaveApi_p) |
This is the function to initialize the EtherCAT Slave API. More... | |
uint32_t | EC_API_SLV_run (EC_API_SLV_SHandle_t *pEcSlaveApi_p) |
This is the function to run the EtherCAT Slave API. More... | |
uint32_t | EC_API_SLV_stop (EC_API_SLV_SHandle_t *pEcSlaveApi_p) |
This is the function to stop the EtherCAT Slave API. More... | |
uint32_t | EC_API_SLV_reset (EC_API_SLV_SHandle_t *pEcSlaveApi_p) |
Reset configuration to default values. More... | |
uint32_t | EC_API_SLV_getConfigStatus (EC_API_SLV_SHandle_t *pEcSlaveApi_p) |
This function reads the EtherCAT driver status. More... | |
uint32_t | EC_API_SLV_getCyclicStatus (EC_API_SLV_SHandle_t *pEcSlaveApi_p) |
This function reads if there is any error cyclic communication error. More... | |
EC_API_SLV_EEsmState_t | EC_API_SLV_getState (void) |
This is the function to read the EtherCAT Slave state machine. More... | |
uint32_t | EC_API_SLV_setState (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_EEsmState_t state_p) |
This is the function to request a EtherCAT state. More... | |
uint32_t | EC_API_SLV_setStationAlias (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t stationAlias_p) |
This is the function to set station alias. More... | |
uint8_t | EC_API_SLV_readByteEscRegister (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p) |
This is the function reads a byte from ESC Register. More... | |
uint16_t | EC_API_SLV_readWordEscRegister (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p) |
This is the function reads a byte from ESC Register. More... | |
uint32_t | EC_API_SLV_readDoubleWordEscRegister (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p) |
This is the function reads a byte from ESC Register. More... | |
void | EC_API_SLV_writeByteEscRegister (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p, uint8_t value_p) |
void | EC_API_SLV_writeWordEscRegister (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p, uint16_t value_p) |
void | EC_API_SLV_writeDoubleWordEscRegister (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p, uint32_t value_p) |
void | EC_API_SLV_mainLoopCyclic (void) |
Trigger stack mainloop. More... | |
void | EC_API_SLV_cbRegisterErrorHandler (EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBStackError_t cbFunc_p) |
uint32_t | EC_API_SLV_setErrorRegister (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_EErrorRegister_t errorRegister_p) |
Error register value defined in ETG1000.6 Error Register Table. More... | |