EtherCAT Slave  1.10.00

◆ EC_API_SLV_readDoubleWordEscRegister()

uint32_t EC_API_SLV_readDoubleWordEscRegister ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
uint16_t  escAddress_p 
)

This is the function reads a byte from ESC Register.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]escAddress_pThe ESC Address
Returns
uint32_t Returns the ESC value.
Example
#include <ecSlvApi.h>
// required variables
uint32_t alEscCtrlStatus = 0;
// the Call
alEscCtrlStatus = EC_API_SLV_readDoubleWordEscRegister(ecSlaveApi, 0x120);
See also
EC_API_SLV_readByteEscRegister, EC_API_SLV_readWordEscRegister
Examples
ESL_cia402Demo.c.
EC_API_SLV_readDoubleWordEscRegister
uint32_t EC_API_SLV_readDoubleWordEscRegister(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p)
This is the function reads a byte from ESC Register.
Definition: ecSlvApiStub.c:1190