EtherCAT Slave  1.10.00

◆ EC_API_SLV_setStationAlias()

uint32_t EC_API_SLV_setStationAlias ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
uint16_t  stationAlias_p 
)

This is the function to set station alias.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]stationAlias_pNode station alias
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
EC_API_EError_t retVal = 0;
// the Call
retVal = EC_API_SLV_setStationAlias(ecSlaveApi, 1001);
EC_API_EError_t
enum EC_API_EError EC_API_EError_t
EC_API_SLV_setStationAlias
uint32_t EC_API_SLV_setStationAlias(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t stationAlias_p)
This is the function to set station alias.
Definition: ecSlvApiStub.c:1055