EtherCAT Slave
1.10.00
◆
EC_API_SLV_writeByteEscRegister()
void EC_API_SLV_writeByteEscRegister
(
EC_API_SLV_SHandle_t
*
pEcSlaveApi_p
,
uint16_t
escAddress_p
,
uint8_t
value_p
)
Parameters
[in]
pEcSlaveApi_p
The pointer to the EtherCAT API instance.
[in]
escAddress_p
The ESC Address
[in]
value_p
New value
Example
#include <ecSlvApi.h>
// required variables
uint8_t alEscCtrlStatus = 8;
// the Call
EC_API_SLV_writeByteEscRegister
(ecSlaveApi, 0x120, alEscCtrlStatus);
See also
theReference
EC_API_SLV_writeByteEscRegister
void EC_API_SLV_writeByteEscRegister(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p, uint8_t value_p)
Definition:
ecSlvApiStub.c:1234
Basic Functions
generated by
1.8.17