#include <ecApiDef.h>
#include <ecSlvESI.h>
#include <ESL_os.h>
#include <ESL_BOARD_config.h>
#include <ESL_vendor.h>
#include <ESL_gpioHelper.h>
#include <ESL_foeDemo.h>
#include <ESL_soeDemo.h>
#include <ESL_eeprom.h>
#include <ESL_cia402Demo.h>
#include <ESL_esiParser.h>
#include <ecSlvApi.h>
#if !(defined MBXMEM)
#define MBXMEM
#endif
#ifdef OSAL_LINUX
#define SITARA_ESI_FILE "sitara.xml"
#define FAULHABER_ESI_FILE "Faulhaber_MC5004_012601_06.xml"
#define WEIDMULLER_ESI_FILE "Weidmueller_UR20_FBC.xml"
#define KUNBUS_ESI_FILE "Gateway_Component_EtherCAT_R02.xml"
#define PILZ_ESI_FILE "KUNBUS-PNOZ_m_ES_EtherCAT_V1_1.xml"
#else
#include "Sitara_Slave_Simple_CiA402.h"
#endif
#define I2C_IOEXP_ADDR 0x60 // The I2C address for GPIO expander
static void EC_SLV_APP_applicationRun(void* pAppCtxt_p);
#if !(defined DPRAM_REMOTE) && !(defined FBTL_REMOTE)
static OSAL_FUNC_UNUSED void EC_SLV_APP_boardPhyReset(void* pCtxt_p, uint8_t phyIdx_p, bool reset_p)
{
uint8_t module = (uint8_t)~0;
uint8_t pin = (uint8_t)~0;
switch(phyIdx_p)
{
case 0:
#if (defined APP_PHY00_RESET_MODULE) && (defined APP_PHY00_RESET_PIN)
{
module = APP_PHY00_RESET_MODULE;
pin = APP_PHY00_RESET_PIN;
}
#endif
#if (defined APP_PHY10_RESET_MODULE) && (defined APP_PHY10_RESET_PIN)
{
module = APP_PHY10_RESET_MODULE;
pin = APP_PHY10_RESET_PIN;
}
#endif
break;
case 1:
#if (defined APP_PHY01_RESET_MODULE) && (defined APP_PHY01_RESET_PIN)
{
module = APP_PHY01_RESET_MODULE;
pin = APP_PHY01_RESET_PIN;
}
#endif
#if (defined APP_PHY11_RESET_MODULE) && (defined APP_PHY11_RESET_PIN)
{
module = APP_PHY11_RESET_MODULE;
pin = APP_PHY11_RESET_PIN;
}
#endif
break;
default:
return;
}
if ((uint8_t)-1 == pin || (uint8_t)-1 == module)
{
OSAL_printf("Invalid PHY config %u\r\n", phyIdx_p);
OSAL_error(__FUNCTION__, __LINE__, OSAL_STACK_PHYDETECT_ERROR, true, 0);
}
if (reset_p)
{
OSAL_printf("Phy Reset: %u.%u\r\n", module, pin);
ESL_GPIO_write(pApplicationInstance->
gpioHandle, (ESL_GPIO_EModule_t)module, (ESL_GPIO_EPin_t)pin, ESL_GPIO_enPINSTATE_LOW);
}
else
{
OSAL_printf("Phy UnReset: %u.%u\r\n", module, pin);
ESL_GPIO_write(pApplicationInstance->
gpioHandle, (ESL_GPIO_EModule_t)module, (ESL_GPIO_EPin_t)pin, ESL_GPIO_enPINSTATE_HIGH);
}
}
#endif
static void EC_SLV_APP_appBoardStatusLed(void* pCallContext_p, void* pLedContext_p, bool runLed_p, bool errLed_p)
{
OSALUNREF_PARM(pLedContext_p);
if (NULL == pApplicationInstance)
{
goto Exit;
}
Exit:
return;
}
{
if (!pApplicationInstance)
{
goto Exit;
}
,EC_SLV_APP_appBoardStatusLed
Exit:
return error;
}
{
if (!pAppInstance_p)
{
goto Exit;
}
#if !(defined DPRAM_REMOTE) && !(defined FBTL_REMOTE)
#if (defined APP_PHY00_RESET_PIN) && (defined APP_PHY00_RESET_MODULE) && (defined APP_PHY01_RESET_PIN) && (defined APP_PHY01_RESET_MODULE)
{
ESL_GPIO_setConfigMode(pAppInstance_p->
gpioHandle, APP_PHY00_RESET_MODULE, APP_PHY00_RESET_PIN, ESL_GPIO_enDIRECTION_MODE_OUTPUT, ESL_GPIO_enIRQ_MODE_NONE);
ESL_GPIO_setConfigMode(pAppInstance_p->
gpioHandle, APP_PHY01_RESET_MODULE, APP_PHY01_RESET_PIN, ESL_GPIO_enDIRECTION_MODE_OUTPUT, ESL_GPIO_enIRQ_MODE_NONE);
}
#endif
#if (defined APP_PHY10_RESET_PIN) && (defined APP_PHY10_RESET_MODULE) && (defined APP_PHY11_RESET_PIN) && (defined APP_PHY11_RESET_MODULE)
{
ESL_GPIO_setConfigMode(pAppInstance_p->
gpioHandle, APP_PHY10_RESET_MODULE, APP_PHY10_RESET_PIN, ESL_GPIO_enDIRECTION_MODE_OUTPUT, ESL_GPIO_enIRQ_MODE_NONE);
ESL_GPIO_setConfigMode(pAppInstance_p->
gpioHandle, APP_PHY11_RESET_MODULE, APP_PHY11_RESET_PIN, ESL_GPIO_enDIRECTION_MODE_OUTPUT, ESL_GPIO_enIRQ_MODE_NONE);
}
#endif
#else
OSALUNREF_PARM(pAppInstance_p);
#endif
#if (defined GPIO_LEDRG0_BANK) && (defined GPIO_LEDRG0_PIN) && (defined GPIO_LEDLR0_BANK) && (defined GPIO_LEDLR0_PIN)
{
ESL_GPIO_setConfigMode(pAppInstance_p->
gpioHandle, GPIO_LEDRG0_BANK, GPIO_LEDRG0_PIN, ESL_GPIO_enDIRECTION_MODE_OUTPUT, ESL_GPIO_enIRQ_MODE_NONE);
ESL_GPIO_setConfigMode(pAppInstance_p->
gpioHandle, GPIO_LEDLR0_BANK, GPIO_LEDLR0_PIN, ESL_GPIO_enDIRECTION_MODE_OUTPUT, ESL_GPIO_enIRQ_MODE_NONE);
}
#endif
#if (defined GPIO_LEDRG1_BANK) && (defined GPIO_LEDRG1_PIN) && (defined GPIO_LEDLR1_BANK) && (defined GPIO_LEDLR1_PIN)
{
ESL_GPIO_setConfigMode(pAppInstance_p->
gpioHandle, GPIO_LEDRG1_BANK, GPIO_LEDRG1_PIN, ESL_GPIO_enDIRECTION_MODE_OUTPUT, ESL_GPIO_enIRQ_MODE_NONE);
ESL_GPIO_setConfigMode(pAppInstance_p->
gpioHandle, GPIO_LEDLR1_BANK, GPIO_LEDLR1_PIN, ESL_GPIO_enDIRECTION_MODE_OUTPUT, ESL_GPIO_enIRQ_MODE_NONE);
}
#endif
#if !(defined DPRAM_REMOTE) && !(defined FBTL_REMOTE)
#if (defined APP_PHY00_RESET_PIN) && (defined APP_PHY00_RESET_MODULE) && (defined APP_PHY01_RESET_PIN) && (defined APP_PHY01_RESET_MODULE)
{
EC_SLV_APP_boardPhyReset(pAppInstance_p, 0, true);
EC_SLV_APP_boardPhyReset(pAppInstance_p, 1, true);
}
#endif
#if (defined APP_PHY10_RESET_PIN) && (defined APP_PHY10_RESET_MODULE) && (defined APP_PHY11_RESET_PIN) && (defined APP_PHY11_RESET_MODULE)
{
EC_SLV_APP_boardPhyReset(pAppInstance_p, 0, true);
EC_SLV_APP_boardPhyReset(pAppInstance_p, 1, true);
}
#endif
#endif
Exit:
return;
}
{
if (!pAppInstance_p)
{
goto Exit;
}
#if !(defined DPRAM_REMOTE) && !(defined FBTL_REMOTE)
#if !(defined TIESC_PHYADDR_0) && !(defined TIESC_PHYADDR_1) && !(defined TIESC_PHYADDR_2) && !(defined TIESC_PHYADDR_3)
#error "EtherCAT without PHY is useless"
#endif
#if (defined TIESC_PHYADDR_0) && (defined TIESC_PHYADDR_1)
{
}
#endif
#if (defined TIESC_PHYADDR_2) && (defined TIESC_PHYADDR_3)
{
}
#endif
#if (defined TIESC_PHYADDR_4) && (defined TIESC_PHYADDR_5)
{
}
#endif
#endif
Exit:
return;
}
uint8_t EC_API_SLV_PendingErrorCb(
uint16_t Index,
uint8_t Subindex,
uint32_t length,
uint16_t* pData,
uint8_t bCompleteAccess
)
{
OSALUNREF_PARM(Subindex);
OSALUNREF_PARM(bCompleteAccess);
OSALUNREF_PARM(pData);
if(Index == 0x2000 && length == 2)
{
}
return 0;
}
{
if (!pAppInstance_p)
{
goto Exit;
}
{
OSAL_error(__FUNCTION__, __LINE__, OSAL_CONTAINER_NOMEMORY, true, 0);
goto Exit;
}
error = EC_SLV_APP_populateBoardFunctions(pAppInstance_p);
{
OSAL_printf("Populate board functions Error code: 0x%08x\n", error);
goto Exit;
}
#ifdef OSAL_LINUX
#else
error = (
EC_API_EError_t)ESL_ESI_parseFileRam(pAppInstance_p->
ptEcSlvApi, (
const uint8_t *)Sitara_Slave_Simple_CiA402_xml, Sitara_Slave_Simple_CiA402_xml_len);
#endif
{
goto Exit;
}
{
OSAL_printf("Slave Init Error Code: 0x%08x\n", error);
goto Exit;
}
#if (defined ENABLE_I2CLEDS) && (ENABLE_I2CLEDS == 1)
#endif
pAppInstance_p->
msec = 0;
pAppInstance_p->
prev = ESL_OS_clockGet();
Exit:
return;
}
{
if (pAppInstance_p)
{
}
}
static void EC_SLV_APP_applicationRun(void* pAppCtxt_p)
{
static uint8_t lastLed = 0;
pApplicationInstace->
diff = ESL_OS_clockDiff(pApplicationInstace->
prev, NULL);
if (pApplicationInstace->
diff)
{
#if (defined ENABLE_I2CLEDS) && (ENABLE_I2CLEDS == 1)
ESL_OS_ioexp_leds_write(pApplicationInstace->
ioexpLedHandle, ledPDData);
#endif
pApplicationInstace->
prev = ESL_OS_clockGet();
lastLed = lastLed ? lastLed << 1 : 1;
}
{
}
}