![]() |
0.01.00
|
This file defines the OpenThread Thread API (for both FTD and MTD). More...
Go to the source code of this file.
Typedefs | |
| typedef void(* | otReceiveDiagnosticGetCallback) (otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext) |
| This function pointer is called when Network Diagnostic Get response is received. More... | |
Functions | |
| OTAPI otError OTCALL | otThreadSetEnabled (otInstance *aInstance, bool aEnabled) |
| This function starts Thread protocol operation. More... | |
| OTAPI bool OTCALL | otThreadGetAutoStart (otInstance *aInstance) |
| This function queries if the Thread stack is configured to automatically start on reinitialization. More... | |
| OTAPI otError OTCALL | otThreadSetAutoStart (otInstance *aInstance, bool aStartAutomatically) |
| This function configures the Thread stack to automatically start on reinitialization. More... | |
| OTAPI bool OTCALL | otThreadIsSingleton (otInstance *aInstance) |
| This function indicates whether a node is the only router on the network. More... | |
| OTAPI otError OTCALL | otThreadDiscover (otInstance *aInstance, uint32_t aScanChannels, uint16_t aPanId, bool aJoiner, bool aEnableEui64Filtering, otHandleActiveScanResult aCallback, void *aCallbackContext) |
| This function starts a Thread Discovery scan. More... | |
| OTAPI bool OTCALL | otThreadIsDiscoverInProgress (otInstance *aInstance) |
| This function determines if an MLE Thread Discovery is currently in progress. More... | |
| OTAPI uint32_t OTCALL | otThreadGetChildTimeout (otInstance *aInstance) |
| Get the Thread Child Timeout used when operating in the Child role. More... | |
| OTAPI void OTCALL | otThreadSetChildTimeout (otInstance *aInstance, uint32_t aTimeout) |
| Set the Thread Child Timeout used when operating in the Child role. More... | |
| OTAPI const uint8_t *OTCALL | otThreadGetExtendedPanId (otInstance *aInstance) |
| Get the IEEE 802.15.4 Extended PAN ID. More... | |
| OTAPI otError OTCALL | otThreadSetExtendedPanId (otInstance *aInstance, const uint8_t *aExtendedPanId) |
| Set the IEEE 802.15.4 Extended PAN ID. More... | |
| OTAPI otError OTCALL | otThreadGetLeaderRloc (otInstance *aInstance, otIp6Address *aLeaderRloc) |
| This function returns a pointer to the Leader's RLOC. More... | |
| OTAPI otLinkModeConfig OTCALL | otThreadGetLinkMode (otInstance *aInstance) |
| Get the MLE Link Mode configuration. More... | |
| OTAPI otError OTCALL | otThreadSetLinkMode (otInstance *aInstance, otLinkModeConfig aConfig) |
| Set the MLE Link Mode configuration. More... | |
| OTAPI const otMasterKey *OTCALL | otThreadGetMasterKey (otInstance *aInstance) |
| Get the thrMasterKey. More... | |
| OTAPI otError OTCALL | otThreadSetMasterKey (otInstance *aInstance, const otMasterKey *aKey) |
| Set the thrMasterKey. More... | |
| OTAPI const otIp6Address *OTCALL | otThreadGetMeshLocalEid (otInstance *aInstance) |
| This function returns a pointer to the Mesh Local EID. More... | |
| OTAPI const uint8_t *OTCALL | otThreadGetMeshLocalPrefix (otInstance *aInstance) |
| This function returns a pointer to the Mesh Local Prefix. More... | |
| OTAPI otError OTCALL | otThreadSetMeshLocalPrefix (otInstance *aInstance, const uint8_t *aMeshLocalPrefix) |
| This function sets the Mesh Local Prefix. More... | |
| const otIp6Address * | otThreadGetLinkLocalIp6Address (otInstance *aInstance) |
| This function returns the Thread link-local IPv6 address. More... | |
| OTAPI const char *OTCALL | otThreadGetNetworkName (otInstance *aInstance) |
| Get the Thread Network Name. More... | |
| OTAPI otError OTCALL | otThreadSetNetworkName (otInstance *aInstance, const char *aNetworkName) |
| Set the Thread Network Name. More... | |
| OTAPI uint32_t OTCALL | otThreadGetKeySequenceCounter (otInstance *aInstance) |
| Get the thrKeySequenceCounter. More... | |
| OTAPI void OTCALL | otThreadSetKeySequenceCounter (otInstance *aInstance, uint32_t aKeySequenceCounter) |
| Set the thrKeySequenceCounter. More... | |
| OTAPI uint32_t OTCALL | otThreadGetKeySwitchGuardTime (otInstance *aInstance) |
| Get the thrKeySwitchGuardTime. More... | |
| OTAPI void OTCALL | otThreadSetKeySwitchGuardTime (otInstance *aInstance, uint32_t aKeySwitchGuardTime) |
| Set the thrKeySwitchGuardTime. More... | |
| OTAPI otError OTCALL | otThreadBecomeDetached (otInstance *aInstance) |
| Detach from the Thread network. More... | |
| OTAPI otError OTCALL | otThreadBecomeChild (otInstance *aInstance) |
| Attempt to reattach as a child. More... | |
| OTAPI otError OTCALL | otThreadGetNextNeighborInfo (otInstance *aInstance, otNeighborInfoIterator *aIterator, otNeighborInfo *aInfo) |
| This function gets the next neighbor information. More... | |
| OTAPI otDeviceRole OTCALL | otThreadGetDeviceRole (otInstance *aInstance) |
| Get the device role. More... | |
| OTAPI otError OTCALL | otThreadGetLeaderData (otInstance *aInstance, otLeaderData *aLeaderData) |
| This function get the Thread Leader Data. More... | |
| OTAPI uint8_t OTCALL | otThreadGetLeaderRouterId (otInstance *aInstance) |
| Get the Leader's Router ID. More... | |
| OTAPI uint8_t OTCALL | otThreadGetLeaderWeight (otInstance *aInstance) |
| Get the Leader's Weight. More... | |
| OTAPI uint32_t OTCALL | otThreadGetPartitionId (otInstance *aInstance) |
| Get the Partition ID. More... | |
| OTAPI uint16_t OTCALL | otThreadGetRloc16 (otInstance *aInstance) |
| Get the RLOC16. More... | |
| OTAPI otError OTCALL | otThreadGetParentInfo (otInstance *aInstance, otRouterInfo *aParentInfo) |
| The function retrieves diagnostic information for a Thread Router as parent. More... | |
| OTAPI otError OTCALL | otThreadGetParentAverageRssi (otInstance *aInstance, int8_t *aParentRssi) |
| The function retrieves the average RSSI for the Thread Parent. More... | |
| OTAPI otError OTCALL | otThreadGetParentLastRssi (otInstance *aInstance, int8_t *aLastRssi) |
| The function retrieves the RSSI of the last packet from the Thread Parent. More... | |
| void | otThreadSetReceiveDiagnosticGetCallback (otInstance *aInstance, otReceiveDiagnosticGetCallback aCallback, void *aCallbackContext) |
| This function registers a callback to provide received raw Network Diagnostic Get response payload. More... | |
| OTAPI otError OTCALL | otThreadSendDiagnosticGet (otInstance *aInstance, const otIp6Address *aDestination, const uint8_t aTlvTypes[], uint8_t aCount) |
| Send a Network Diagnostic Get request. More... | |
| OTAPI otError OTCALL | otThreadSendDiagnosticReset (otInstance *aInstance, const otIp6Address *aDestination, const uint8_t aTlvTypes[], uint8_t aCount) |
| Send a Network Diagnostic Reset request. More... | |
| OTAPI const otIpCounters *OTCALL | otThreadGetIp6Counters (otInstance *aInstance) |
| Get the IPv6 counters. More... | |
This file defines the OpenThread Thread API (for both FTD and MTD).