![]() |
0.01.00
|
This module includes functions for all Thread roles. More...
Typedefs | |
| typedef void(* | otReceiveDiagnosticGetCallback) (otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext) |
| This function pointer is called when Network Diagnostic Get response is received. More... | |
Functions | |
| OTAPI bool OTCALL | otDatasetIsCommissioned (otInstance *aInstance) |
| This function indicates whether a valid network is present in the Active Operational Dataset or not. More... | |
| OTAPI otError OTCALL | otDatasetGetActive (otInstance *aInstance, otOperationalDataset *aDataset) |
| This function gets the Active Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetGetPending (otInstance *aInstance, otOperationalDataset *aDataset) |
| This function gets the Pending Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetSetActive (otInstance *aInstance, const otOperationalDataset *aDataset) |
| This function sets the Active Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetSetPending (otInstance *aInstance, const otOperationalDataset *aDataset) |
| This function sets the Pending Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtActiveGet (otInstance *aInstance, const uint8_t *aTlvTypes, uint8_t aLength, const otIp6Address *aAddress) |
| This function sends MGMT_ACTIVE_GET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtActiveSet (otInstance *aInstance, const otOperationalDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength) |
| This function sends MGMT_ACTIVE_SET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtPendingGet (otInstance *aInstance, const uint8_t *aTlvTypes, uint8_t aLength, const otIp6Address *aAddress) |
| This function sends MGMT_PENDING_GET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtPendingSet (otInstance *aInstance, const otOperationalDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength) |
| This function sends MGMT_PENDING_SET. More... | |
| OTAPI uint32_t OTCALL | otDatasetGetDelayTimerMinimal (otInstance *aInstance) |
| Get minimal delay timer. More... | |
| OTAPI otError OTCALL | otDatasetSetDelayTimerMinimal (otInstance *aInstance, uint32_t aDelayTimerMinimal) |
| Set minimal delay timer. More... | |
| OTAPI otError OTCALL | otNetDataGet (otInstance *aInstance, bool aStable, uint8_t *aData, uint8_t *aDataLength) |
| This method provides a full or stable copy of the Leader's Thread Network Data. More... | |
| OTAPI otError OTCALL | otNetDataGetNextOnMeshPrefix (otInstance *aInstance, otNetworkDataIterator *aIterator, otBorderRouterConfig *aConfig) |
| This function gets the next On Mesh Prefix in the partition's Network Data. More... | |
| otError | otNetDataGetNextRoute (otInstance *aInstance, otNetworkDataIterator *aIterator, otExternalRouteConfig *aConfig) |
| This function gets the next external route in the partition's Network Data. More... | |
| OTAPI uint8_t OTCALL | otNetDataGetVersion (otInstance *aInstance) |
| Get the Network Data Version. More... | |
| OTAPI uint8_t OTCALL | otNetDataGetStableVersion (otInstance *aInstance) |
| Get the Stable Network Data Version. More... | |
| OTAPI otError OTCALL | otThreadSetEnabled (otInstance *aInstance, bool aEnabled) |
| This function starts Thread protocol operation. More... | |
| OTAPI bool OTCALL | otThreadGetAutoStart (otInstance *aInstance) |
| This function queries if the Thread stack is configured to automatically start on reinitialization. More... | |
| OTAPI otError OTCALL | otThreadSetAutoStart (otInstance *aInstance, bool aStartAutomatically) |
| This function configures the Thread stack to automatically start on reinitialization. More... | |
| OTAPI bool OTCALL | otThreadIsSingleton (otInstance *aInstance) |
| This function indicates whether a node is the only router on the network. More... | |
| OTAPI otError OTCALL | otThreadDiscover (otInstance *aInstance, uint32_t aScanChannels, uint16_t aPanId, bool aJoiner, bool aEnableEui64Filtering, otHandleActiveScanResult aCallback, void *aCallbackContext) |
| This function starts a Thread Discovery scan. More... | |
| OTAPI bool OTCALL | otThreadIsDiscoverInProgress (otInstance *aInstance) |
| This function determines if an MLE Thread Discovery is currently in progress. More... | |
| OTAPI uint32_t OTCALL | otThreadGetChildTimeout (otInstance *aInstance) |
| Get the Thread Child Timeout used when operating in the Child role. More... | |
| OTAPI void OTCALL | otThreadSetChildTimeout (otInstance *aInstance, uint32_t aTimeout) |
| Set the Thread Child Timeout used when operating in the Child role. More... | |
| OTAPI const uint8_t *OTCALL | otThreadGetExtendedPanId (otInstance *aInstance) |
| Get the IEEE 802.15.4 Extended PAN ID. More... | |
| OTAPI otError OTCALL | otThreadSetExtendedPanId (otInstance *aInstance, const uint8_t *aExtendedPanId) |
| Set the IEEE 802.15.4 Extended PAN ID. More... | |
| OTAPI otError OTCALL | otThreadGetLeaderRloc (otInstance *aInstance, otIp6Address *aLeaderRloc) |
| This function returns a pointer to the Leader's RLOC. More... | |
| OTAPI otLinkModeConfig OTCALL | otThreadGetLinkMode (otInstance *aInstance) |
| Get the MLE Link Mode configuration. More... | |
| OTAPI otError OTCALL | otThreadSetLinkMode (otInstance *aInstance, otLinkModeConfig aConfig) |
| Set the MLE Link Mode configuration. More... | |
| OTAPI const otMasterKey *OTCALL | otThreadGetMasterKey (otInstance *aInstance) |
| Get the thrMasterKey. More... | |
| OTAPI otError OTCALL | otThreadSetMasterKey (otInstance *aInstance, const otMasterKey *aKey) |
| Set the thrMasterKey. More... | |
| OTAPI const otIp6Address *OTCALL | otThreadGetMeshLocalEid (otInstance *aInstance) |
| This function returns a pointer to the Mesh Local EID. More... | |
| OTAPI const uint8_t *OTCALL | otThreadGetMeshLocalPrefix (otInstance *aInstance) |
| This function returns a pointer to the Mesh Local Prefix. More... | |
| OTAPI otError OTCALL | otThreadSetMeshLocalPrefix (otInstance *aInstance, const uint8_t *aMeshLocalPrefix) |
| This function sets the Mesh Local Prefix. More... | |
| const otIp6Address * | otThreadGetLinkLocalIp6Address (otInstance *aInstance) |
| This function returns the Thread link-local IPv6 address. More... | |
| OTAPI const char *OTCALL | otThreadGetNetworkName (otInstance *aInstance) |
| Get the Thread Network Name. More... | |
| OTAPI otError OTCALL | otThreadSetNetworkName (otInstance *aInstance, const char *aNetworkName) |
| Set the Thread Network Name. More... | |
| OTAPI uint32_t OTCALL | otThreadGetKeySequenceCounter (otInstance *aInstance) |
| Get the thrKeySequenceCounter. More... | |
| OTAPI void OTCALL | otThreadSetKeySequenceCounter (otInstance *aInstance, uint32_t aKeySequenceCounter) |
| Set the thrKeySequenceCounter. More... | |
| OTAPI uint32_t OTCALL | otThreadGetKeySwitchGuardTime (otInstance *aInstance) |
| Get the thrKeySwitchGuardTime. More... | |
| OTAPI void OTCALL | otThreadSetKeySwitchGuardTime (otInstance *aInstance, uint32_t aKeySwitchGuardTime) |
| Set the thrKeySwitchGuardTime. More... | |
| OTAPI otError OTCALL | otThreadBecomeDetached (otInstance *aInstance) |
| Detach from the Thread network. More... | |
| OTAPI otError OTCALL | otThreadBecomeChild (otInstance *aInstance) |
| Attempt to reattach as a child. More... | |
| OTAPI otError OTCALL | otThreadGetNextNeighborInfo (otInstance *aInstance, otNeighborInfoIterator *aIterator, otNeighborInfo *aInfo) |
| This function gets the next neighbor information. More... | |
| OTAPI otDeviceRole OTCALL | otThreadGetDeviceRole (otInstance *aInstance) |
| Get the device role. More... | |
| OTAPI otError OTCALL | otThreadGetLeaderData (otInstance *aInstance, otLeaderData *aLeaderData) |
| This function get the Thread Leader Data. More... | |
| OTAPI uint8_t OTCALL | otThreadGetLeaderRouterId (otInstance *aInstance) |
| Get the Leader's Router ID. More... | |
| OTAPI uint8_t OTCALL | otThreadGetLeaderWeight (otInstance *aInstance) |
| Get the Leader's Weight. More... | |
| OTAPI uint32_t OTCALL | otThreadGetPartitionId (otInstance *aInstance) |
| Get the Partition ID. More... | |
| OTAPI uint16_t OTCALL | otThreadGetRloc16 (otInstance *aInstance) |
| Get the RLOC16. More... | |
| OTAPI otError OTCALL | otThreadGetParentInfo (otInstance *aInstance, otRouterInfo *aParentInfo) |
| The function retrieves diagnostic information for a Thread Router as parent. More... | |
| OTAPI otError OTCALL | otThreadGetParentAverageRssi (otInstance *aInstance, int8_t *aParentRssi) |
| The function retrieves the average RSSI for the Thread Parent. More... | |
| OTAPI otError OTCALL | otThreadGetParentLastRssi (otInstance *aInstance, int8_t *aLastRssi) |
| The function retrieves the RSSI of the last packet from the Thread Parent. More... | |
| void | otThreadSetReceiveDiagnosticGetCallback (otInstance *aInstance, otReceiveDiagnosticGetCallback aCallback, void *aCallbackContext) |
| This function registers a callback to provide received raw Network Diagnostic Get response payload. More... | |
| OTAPI otError OTCALL | otThreadSendDiagnosticGet (otInstance *aInstance, const otIp6Address *aDestination, const uint8_t aTlvTypes[], uint8_t aCount) |
| Send a Network Diagnostic Get request. More... | |
| OTAPI otError OTCALL | otThreadSendDiagnosticReset (otInstance *aInstance, const otIp6Address *aDestination, const uint8_t aTlvTypes[], uint8_t aCount) |
| Send a Network Diagnostic Reset request. More... | |
| OTAPI const otIpCounters *OTCALL | otThreadGetIp6Counters (otInstance *aInstance) |
| Get the IPv6 counters. More... | |
This module includes functions for all Thread roles.
| typedef void(* otReceiveDiagnosticGetCallback) (otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext) |
This function pointer is called when Network Diagnostic Get response is received.
| [in] | aMessage | A pointer to the message buffer containing the received Network Diagnostic Get response payload. |
| [in] | aMessageInfo | A pointer to the message info for aMessage. |
| [in] | aContext | A pointer to application-specific context. |
| OTAPI otError OTCALL otDatasetGetActive | ( | otInstance * | aInstance, |
| otOperationalDataset * | aDataset | ||
| ) |
This function gets the Active Operational Dataset.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aDataset | A pointer to where the Active Operational Dataset will be placed. |
| OT_ERROR_NONE | Successfully retrieved the Active Operational Dataset. |
| OT_ERROR_INVALID_ARGS | aDataset was NULL. |
| OTAPI uint32_t OTCALL otDatasetGetDelayTimerMinimal | ( | otInstance * | aInstance | ) |
Get minimal delay timer.
| [in] | aInstance | A pointer to an OpenThread instance. |
| the | value of minimal delay timer (in ms). |
| OTAPI otError OTCALL otDatasetGetPending | ( | otInstance * | aInstance, |
| otOperationalDataset * | aDataset | ||
| ) |
This function gets the Pending Operational Dataset.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aDataset | A pointer to where the Pending Operational Dataset will be placed. |
| OT_ERROR_NONE | Successfully retrieved the Pending Operational Dataset. |
| OT_ERROR_INVALID_ARGS | aDataset was NULL. |
| OTAPI bool OTCALL otDatasetIsCommissioned | ( | otInstance * | aInstance | ) |
This function indicates whether a valid network is present in the Active Operational Dataset or not.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otDatasetSendMgmtActiveGet | ( | otInstance * | aInstance, |
| const uint8_t * | aTlvTypes, | ||
| uint8_t | aLength, | ||
| const otIp6Address * | aAddress | ||
| ) |
This function sends MGMT_ACTIVE_GET.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aTlvTypes | A pointer to the TLV Types. |
| [in] | aLength | The length of TLV Types. |
| [in] | aAddress | A pointer to the IPv6 destination, if it is NULL, will use Leader ALOC as default. |
| OT_ERROR_NONE | Successfully send the meshcop dataset command. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to send. |
| OTAPI otError OTCALL otDatasetSendMgmtActiveSet | ( | otInstance * | aInstance, |
| const otOperationalDataset * | aDataset, | ||
| const uint8_t * | aTlvs, | ||
| uint8_t | aLength | ||
| ) |
This function sends MGMT_ACTIVE_SET.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDataset | A pointer to operational dataset. |
| [in] | aTlvs | A pointer to TLVs. |
| [in] | aLength | The length of TLVs. |
| OT_ERROR_NONE | Successfully send the meshcop dataset command. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to send. |
| OTAPI otError OTCALL otDatasetSendMgmtPendingGet | ( | otInstance * | aInstance, |
| const uint8_t * | aTlvTypes, | ||
| uint8_t | aLength, | ||
| const otIp6Address * | aAddress | ||
| ) |
This function sends MGMT_PENDING_GET.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aTlvTypes | A pointer to the TLV Types. |
| [in] | aLength | The length of TLV Types. |
| [in] | aAddress | A pointer to the IPv6 destination, if it is NULL, will use Leader ALOC as default. |
| OT_ERROR_NONE | Successfully send the meshcop dataset command. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to send. |
| OTAPI otError OTCALL otDatasetSendMgmtPendingSet | ( | otInstance * | aInstance, |
| const otOperationalDataset * | aDataset, | ||
| const uint8_t * | aTlvs, | ||
| uint8_t | aLength | ||
| ) |
This function sends MGMT_PENDING_SET.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDataset | A pointer to operational dataset. |
| [in] | aTlvs | A pointer to TLVs. |
| [in] | aLength | The length of TLVs. |
| OT_ERROR_NONE | Successfully send the meshcop dataset command. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to send. |
| OTAPI otError OTCALL otDatasetSetActive | ( | otInstance * | aInstance, |
| const otOperationalDataset * | aDataset | ||
| ) |
This function sets the Active Operational Dataset.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDataset | A pointer to the Active Operational Dataset. |
| OT_ERROR_NONE | Successfully set the Active Operational Dataset. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to set the Active Operational Datset. |
| OT_ERROR_INVALID_ARGS | aDataset was NULL. |
| OTAPI otError OTCALL otDatasetSetDelayTimerMinimal | ( | otInstance * | aInstance, |
| uint32_t | aDelayTimerMinimal | ||
| ) |
Set minimal delay timer.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDelayTimerMinimal | The value of minimal delay timer (in ms). |
| OT_ERROR_NONE | Successfully set minimal delay timer. |
| OT_ERROR_INVALID_ARGS | If aDelayTimerMinimal is not valid. |
| OTAPI otError OTCALL otDatasetSetPending | ( | otInstance * | aInstance, |
| const otOperationalDataset * | aDataset | ||
| ) |
This function sets the Pending Operational Dataset.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDataset | A pointer to the Pending Operational Dataset. |
| OT_ERROR_NONE | Successfully set the Pending Operational Dataset. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to set the Pending Operational Dataset. |
| OT_ERROR_INVALID_ARGS | aDataset was NULL. |
| OTAPI otError OTCALL otNetDataGet | ( | otInstance * | aInstance, |
| bool | aStable, | ||
| uint8_t * | aData, | ||
| uint8_t * | aDataLength | ||
| ) |
This method provides a full or stable copy of the Leader's Thread Network Data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aStable | TRUE when copying the stable version, FALSE when copying the full version. |
| [out] | aData | A pointer to the data buffer. |
| [in,out] | aDataLength | On entry, size of the data buffer pointed to by aData. On exit, number of copied bytes. |
| OTAPI otError OTCALL otNetDataGetNextOnMeshPrefix | ( | otInstance * | aInstance, |
| otNetworkDataIterator * | aIterator, | ||
| otBorderRouterConfig * | aConfig | ||
| ) |
This function gets the next On Mesh Prefix in the partition's Network Data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the Network Data iterator context. To get the first on-mesh entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT. |
| [out] | aConfig | A pointer to where the On Mesh Prefix information will be placed. |
| OT_ERROR_NONE | Successfully found the next On Mesh prefix. |
| OT_ERROR_NOT_FOUND | No subsequent On Mesh prefix exists in the Thread Network Data. |
| otError otNetDataGetNextRoute | ( | otInstance * | aInstance, |
| otNetworkDataIterator * | aIterator, | ||
| otExternalRouteConfig * | aConfig | ||
| ) |
This function gets the next external route in the partition's Network Data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the Network Data iterator context. To get the first external route entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT. |
| [out] | aConfig | A pointer to where the External Route information will be placed. |
| OT_ERROR_NONE | Successfully found the next External Route. |
| OT_ERROR_NOT_FOUND | No subsequent external route entry exists in the Thread Network Data. |
| OTAPI uint8_t OTCALL otNetDataGetStableVersion | ( | otInstance * | aInstance | ) |
Get the Stable Network Data Version.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint8_t OTCALL otNetDataGetVersion | ( | otInstance * | aInstance | ) |
Get the Network Data Version.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otThreadBecomeChild | ( | otInstance * | aInstance | ) |
Attempt to reattach as a child.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OT_ERROR_NONE | Successfully begin attempt to become a child. |
| OT_ERROR_INVALID_STATE | Thread is disabled. |
| OTAPI otError OTCALL otThreadBecomeDetached | ( | otInstance * | aInstance | ) |
Detach from the Thread network.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OT_ERROR_NONE | Successfully detached from the Thread network. |
| OT_ERROR_INVALID_STATE | Thread is disabled. |
| OTAPI otError OTCALL otThreadDiscover | ( | otInstance * | aInstance, |
| uint32_t | aScanChannels, | ||
| uint16_t | aPanId, | ||
| bool | aJoiner, | ||
| bool | aEnableEui64Filtering, | ||
| otHandleActiveScanResult | aCallback, | ||
| void * | aCallbackContext | ||
| ) |
This function starts a Thread Discovery scan.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aScanChannels | A bit vector indicating which channels to scan (e.g. OT_CHANNEL_11_MASK). |
| [in] | aPanId | The PAN ID filter (set to Broadcast PAN to disable filter). |
| [in] | aJoiner | Value of the Joiner Flag in the Discovery Request TLV. |
| [in] | aEnableEui64Filtering | TRUE to filter responses on EUI-64, FALSE otherwise. |
| [in] | aCallback | A pointer to a function called on receiving an MLE Discovery Response or scan completes. |
| [in] | aCallbackContext | A pointer to application-specific context. |
| OT_ERROR_NONE | Accepted the Thread Discovery request. |
| OT_ERROR_BUSY | Already performing an Thread Discovery. |
| OTAPI bool OTCALL otThreadGetAutoStart | ( | otInstance * | aInstance | ) |
This function queries if the Thread stack is configured to automatically start on reinitialization.
| [in] | aInstance | A pointer to an OpenThread instance. |
| TRUE | It is configured to automatically start. |
| FALSE | It is not configured to automatically start. |
| OTAPI uint32_t OTCALL otThreadGetChildTimeout | ( | otInstance * | aInstance | ) |
Get the Thread Child Timeout used when operating in the Child role.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otDeviceRole OTCALL otThreadGetDeviceRole | ( | otInstance * | aInstance | ) |
Get the device role.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OT_DEVICE_ROLE_DISABLED | The Thread stack is disabled. |
| OT_DEVICE_ROLE_DETACHED | The device is not currently participating in a Thread network/partition. |
| OT_DEVICE_ROLE_CHILD | The device is currently operating as a Thread Child. |
| OT_DEVICE_ROLE_ROUTER | The device is currently operating as a Thread Router. |
| OT_DEVICE_ROLE_LEADER | The device is currently operating as a Thread Leader. |
| OTAPI const uint8_t* OTCALL otThreadGetExtendedPanId | ( | otInstance * | aInstance | ) |
Get the IEEE 802.15.4 Extended PAN ID.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const otIpCounters* OTCALL otThreadGetIp6Counters | ( | otInstance * | aInstance | ) |
Get the IPv6 counters.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint32_t OTCALL otThreadGetKeySequenceCounter | ( | otInstance * | aInstance | ) |
Get the thrKeySequenceCounter.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint32_t OTCALL otThreadGetKeySwitchGuardTime | ( | otInstance * | aInstance | ) |
Get the thrKeySwitchGuardTime.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otThreadGetLeaderData | ( | otInstance * | aInstance, |
| otLeaderData * | aLeaderData | ||
| ) |
This function get the Thread Leader Data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aLeaderData | A pointer to where the leader data is placed. |
| OT_ERROR_NONE | Successfully retrieved the leader data. |
| OT_ERROR_DETACHED | Not currently attached. |
| OT_ERROR_INVALID_ARGS | aLeaderData is NULL. |
| OTAPI otError OTCALL otThreadGetLeaderRloc | ( | otInstance * | aInstance, |
| otIp6Address * | aLeaderRloc | ||
| ) |
This function returns a pointer to the Leader's RLOC.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aLeaderRloc | A pointer to the Leader's RLOC. |
| OT_ERROR_NONE | The Leader's RLOC was successfully written to aLeaderRloc. |
| OT_ERROR_INVALID_ARGS | aLeaderRloc was NULL. |
| OT_ERROR_DETACHED | Not currently attached to a Thread Partition. |
| OTAPI uint8_t OTCALL otThreadGetLeaderRouterId | ( | otInstance * | aInstance | ) |
Get the Leader's Router ID.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint8_t OTCALL otThreadGetLeaderWeight | ( | otInstance * | aInstance | ) |
Get the Leader's Weight.
| [in] | aInstance | A pointer to an OpenThread instance. |
| const otIp6Address* otThreadGetLinkLocalIp6Address | ( | otInstance * | aInstance | ) |
This function returns the Thread link-local IPv6 address.
The Thread link local address is derived using IEEE802.15.4 Extended Address as Interface Identifier.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otLinkModeConfig OTCALL otThreadGetLinkMode | ( | otInstance * | aInstance | ) |
Get the MLE Link Mode configuration.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const otMasterKey* OTCALL otThreadGetMasterKey | ( | otInstance * | aInstance | ) |
Get the thrMasterKey.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const otIp6Address* OTCALL otThreadGetMeshLocalEid | ( | otInstance * | aInstance | ) |
This function returns a pointer to the Mesh Local EID.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const uint8_t* OTCALL otThreadGetMeshLocalPrefix | ( | otInstance * | aInstance | ) |
This function returns a pointer to the Mesh Local Prefix.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const char* OTCALL otThreadGetNetworkName | ( | otInstance * | aInstance | ) |
Get the Thread Network Name.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otThreadGetNextNeighborInfo | ( | otInstance * | aInstance, |
| otNeighborInfoIterator * | aIterator, | ||
| otNeighborInfo * | aInfo | ||
| ) |
This function gets the next neighbor information.
It is used to go through the entries of the neighbor table.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the iterator context. To get the first neighbor entry it should be set to OT_NEIGHBOR_INFO_ITERATOR_INIT. |
| [out] | aInfo | A pointer to the neighbor information. |
| OT_ERROR_NONE | Successfully found the next neighbor entry in table. |
| OT_ERROR_NOT_FOUND | No subsequent neighbor entry exists in the table. |
| OT_ERROR_INVALID_ARGS | aIterator or aInfo was NULL. |
| OTAPI otError OTCALL otThreadGetParentAverageRssi | ( | otInstance * | aInstance, |
| int8_t * | aParentRssi | ||
| ) |
The function retrieves the average RSSI for the Thread Parent.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aParentRssi | A pointer to where the parent rssi should be placed. |
| OTAPI otError OTCALL otThreadGetParentInfo | ( | otInstance * | aInstance, |
| otRouterInfo * | aParentInfo | ||
| ) |
The function retrieves diagnostic information for a Thread Router as parent.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aParentInfo | A pointer to where the parent router information is placed. |
| OTAPI otError OTCALL otThreadGetParentLastRssi | ( | otInstance * | aInstance, |
| int8_t * | aLastRssi | ||
| ) |
The function retrieves the RSSI of the last packet from the Thread Parent.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aLastRssi | A pointer to where the last rssi should be placed. |
| OT_ERROR_NONE | Successfully retrieved the RSSI data. |
| OT_ERROR_FAILED | Unable to get RSSI data. |
| OT_ERROR_INVALID_ARGS | aLastRssi is NULL. |
| OTAPI uint32_t OTCALL otThreadGetPartitionId | ( | otInstance * | aInstance | ) |
Get the Partition ID.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint16_t OTCALL otThreadGetRloc16 | ( | otInstance * | aInstance | ) |
Get the RLOC16.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI bool OTCALL otThreadIsDiscoverInProgress | ( | otInstance * | aInstance | ) |
This function determines if an MLE Thread Discovery is currently in progress.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI bool OTCALL otThreadIsSingleton | ( | otInstance * | aInstance | ) |
This function indicates whether a node is the only router on the network.
| [in] | aInstance | A pointer to an OpenThread instance. |
| TRUE | It is the only router in the network. |
| FALSE | It is a child or is not a single router in the network. |
| OTAPI otError OTCALL otThreadSendDiagnosticGet | ( | otInstance * | aInstance, |
| const otIp6Address * | aDestination, | ||
| const uint8_t | aTlvTypes[], | ||
| uint8_t | aCount | ||
| ) |
Send a Network Diagnostic Get request.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDestination | A pointer to destination address. |
| [in] | aTlvTypes | An array of Network Diagnostic TLV types. |
| [in] | aCount | Number of types in aTlvTypes |
| OTAPI otError OTCALL otThreadSendDiagnosticReset | ( | otInstance * | aInstance, |
| const otIp6Address * | aDestination, | ||
| const uint8_t | aTlvTypes[], | ||
| uint8_t | aCount | ||
| ) |
Send a Network Diagnostic Reset request.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDestination | A pointer to destination address. |
| [in] | aTlvTypes | An array of Network Diagnostic TLV types. Currently only Type 9 is allowed. |
| [in] | aCount | Number of types in aTlvTypes |
| OTAPI otError OTCALL otThreadSetAutoStart | ( | otInstance * | aInstance, |
| bool | aStartAutomatically | ||
| ) |
This function configures the Thread stack to automatically start on reinitialization.
It has no effect on the current Thread state.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aStartAutomatically | TRUE to automatically start; FALSE to not automatically start. |
| OTAPI void OTCALL otThreadSetChildTimeout | ( | otInstance * | aInstance, |
| uint32_t | aTimeout | ||
| ) |
Set the Thread Child Timeout used when operating in the Child role.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aTimeout | The timeout value. |
| OTAPI otError OTCALL otThreadSetEnabled | ( | otInstance * | aInstance, |
| bool | aEnabled | ||
| ) |
This function starts Thread protocol operation.
The interface must be up when calling this function.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aEnabled | TRUE if Thread is enabled, FALSE otherwise. |
| OT_ERROR_NONE | Successfully started Thread protocol operation. |
| OT_ERROR_INVALID_STATE | The network interface was not not up. |
| OTAPI otError OTCALL otThreadSetExtendedPanId | ( | otInstance * | aInstance, |
| const uint8_t * | aExtendedPanId | ||
| ) |
Set the IEEE 802.15.4 Extended PAN ID.
This function can only be called while Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aExtendedPanId | A pointer to the IEEE 802.15.4 Extended PAN ID. |
| OT_ERROR_NONE | Successfully set the Extended PAN ID. |
| OT_ERROR_INVALID_STATE | Thread protocols are enabled. |
| OTAPI void OTCALL otThreadSetKeySequenceCounter | ( | otInstance * | aInstance, |
| uint32_t | aKeySequenceCounter | ||
| ) |
Set the thrKeySequenceCounter.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aKeySequenceCounter | The thrKeySequenceCounter value. |
| OTAPI void OTCALL otThreadSetKeySwitchGuardTime | ( | otInstance * | aInstance, |
| uint32_t | aKeySwitchGuardTime | ||
| ) |
Set the thrKeySwitchGuardTime.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aKeySwitchGuardTime | The thrKeySwitchGuardTime value (in hours). |
| OTAPI otError OTCALL otThreadSetLinkMode | ( | otInstance * | aInstance, |
| otLinkModeConfig | aConfig | ||
| ) |
Set the MLE Link Mode configuration.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aConfig | A pointer to the Link Mode configuration. |
| OT_ERROR_NONE | Successfully set the MLE Link Mode configuration. |
| OTAPI otError OTCALL otThreadSetMasterKey | ( | otInstance * | aInstance, |
| const otMasterKey * | aKey | ||
| ) |
Set the thrMasterKey.
This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aKey | A pointer to a buffer containing the thrMasterKey. |
| OT_ERROR_NONE | Successfully set the thrMasterKey. |
| OT_ERROR_INVALID_ARGS | If aKeyLength is larger than 16. |
| OT_ERROR_INVALID_STATE | Thread protocols are enabled. |
| OTAPI otError OTCALL otThreadSetMeshLocalPrefix | ( | otInstance * | aInstance, |
| const uint8_t * | aMeshLocalPrefix | ||
| ) |
This function sets the Mesh Local Prefix.
This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aMeshLocalPrefix | A pointer to the Mesh Local Prefix. |
| OT_ERROR_NONE | Successfully set the Mesh Local Prefix. |
| OT_ERROR_INVALID_STATE | Thread protocols are enabled. |
| OTAPI otError OTCALL otThreadSetNetworkName | ( | otInstance * | aInstance, |
| const char * | aNetworkName | ||
| ) |
Set the Thread Network Name.
This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aNetworkName | A pointer to the Thread Network Name. |
| OT_ERROR_NONE | Successfully set the Thread Network Name. |
| OT_ERROR_INVALID_STATE | Thread protocols are enabled. |
| void otThreadSetReceiveDiagnosticGetCallback | ( | otInstance * | aInstance, |
| otReceiveDiagnosticGetCallback | aCallback, | ||
| void * | aCallbackContext | ||
| ) |
This function registers a callback to provide received raw Network Diagnostic Get response payload.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aCallback | A pointer to a function that is called when Network Diagnostic Get response is received or NULL to disable the callback. |
| [in] | aCallbackContext | A pointer to application-specific context. |