![]() |
0.01.00
|
This structure represents the local and peer IPv6 socket addresses. More...
#include <include/openthread/types.h>
Public Attributes | |
| otIp6Address | mSockAddr |
| The local IPv6 address. | |
| otIp6Address | mPeerAddr |
| The peer IPv6 address. | |
| uint16_t | mSockPort |
| The local transport-layer port. | |
| uint16_t | mPeerPort |
| The peer transport-layer port. | |
| int8_t | mInterfaceId |
| An IPv6 interface identifier. | |
| uint8_t | mHopLimit |
| The IPv6 Hop Limit. | |
| const void * | mLinkInfo |
| A pointer to link-specific information. More... | |
This structure represents the local and peer IPv6 socket addresses.
| const void* otMessageInfo::mLinkInfo |
A pointer to link-specific information.
In case mInterfaceId is set to OT_NETIF_INTERFACE_ID_THREAD, mLinkInfo points to