![]() |
0.01.00
|
This structure represents link-specific information for messages received from the Thread radio. More...
#include <include/openthread/types.h>
Public Attributes | |
| uint16_t | mPanId |
| Source PAN ID. | |
| uint8_t | mChannel |
| 802.15.4 Channel | |
| int8_t | mRss |
| Received Signal Strength in dBm. | |
| uint8_t | mLqi |
| Link Quality Indicator for a received message. | |
| bool | mLinkSecurity |
| Indicates whether or not link security is enabled. | |
This structure represents link-specific information for messages received from the Thread radio.