![]() |
0.01.00
|
This structure represents the IP level counters. More...
#include <include/openthread/types.h>
Public Attributes | |
| uint32_t | mTxSuccess |
| The number of IPv6 packets successfully transmitted. | |
| uint32_t | mRxSuccess |
| The number of IPv6 packets successfully received. | |
| uint32_t | mTxFailure |
| The number of IPv6 packets failed to transmit. | |
| uint32_t | mRxFailure |
| The number of IPv6 packets failed to receive. | |
This structure represents the IP level counters.