![]() |
0.01.00
|
This file implements the OpenThread Thread API (for both FTD and MTD). More...
#include "openthread-core-config.h"#include <openthread/thread.h>#include <openthread/platform/settings.h>#include "openthread-instance.h"#include "common/logging.hpp"#include "common/settings.hpp"Macros | |
| #define | WPP_NAME "thread_api.tmh" |
Functions | |
| uint32_t | otThreadGetChildTimeout (otInstance *aInstance) |
| Get the Thread Child Timeout used when operating in the Child role. More... | |
| void | otThreadSetChildTimeout (otInstance *aInstance, uint32_t aTimeout) |
| Set the Thread Child Timeout used when operating in the Child role. More... | |
| const uint8_t * | otThreadGetExtendedPanId (otInstance *aInstance) |
| Get the IEEE 802.15.4 Extended PAN ID. More... | |
| otError | otThreadSetExtendedPanId (otInstance *aInstance, const uint8_t *aExtendedPanId) |
| Set the IEEE 802.15.4 Extended PAN ID. More... | |
| otError | otThreadGetLeaderRloc (otInstance *aInstance, otIp6Address *aAddress) |
| This function returns a pointer to the Leader's RLOC. More... | |
| otLinkModeConfig | otThreadGetLinkMode (otInstance *aInstance) |
| Get the MLE Link Mode configuration. More... | |
| otError | otThreadSetLinkMode (otInstance *aInstance, otLinkModeConfig aConfig) |
| Set the MLE Link Mode configuration. More... | |
| const otMasterKey * | otThreadGetMasterKey (otInstance *aInstance) |
| Get the thrMasterKey. More... | |
| otError | otThreadSetMasterKey (otInstance *aInstance, const otMasterKey *aKey) |
| Set the thrMasterKey. More... | |
| const otIp6Address * | otThreadGetMeshLocalEid (otInstance *aInstance) |
| This function returns a pointer to the Mesh Local EID. More... | |
| const uint8_t * | otThreadGetMeshLocalPrefix (otInstance *aInstance) |
| This function returns a pointer to the Mesh Local Prefix. More... | |
| otError | otThreadSetMeshLocalPrefix (otInstance *aInstance, const uint8_t *aMeshLocalPrefix) |
| This function sets the Mesh Local Prefix. More... | |
| const otIp6Address * | otThreadGetLinkLocalIp6Address (otInstance *aInstance) |
| This function returns the Thread link-local IPv6 address. More... | |
| const char * | otThreadGetNetworkName (otInstance *aInstance) |
| Get the Thread Network Name. More... | |
| otError | otThreadSetNetworkName (otInstance *aInstance, const char *aNetworkName) |
| Set the Thread Network Name. More... | |
| uint32_t | otThreadGetKeySequenceCounter (otInstance *aInstance) |
| Get the thrKeySequenceCounter. More... | |
| void | otThreadSetKeySequenceCounter (otInstance *aInstance, uint32_t aKeySequenceCounter) |
| Set the thrKeySequenceCounter. More... | |
| uint32_t | otThreadGetKeySwitchGuardTime (otInstance *aInstance) |
| Get the thrKeySwitchGuardTime. More... | |
| void | otThreadSetKeySwitchGuardTime (otInstance *aInstance, uint32_t aKeySwitchGuardTime) |
| Set the thrKeySwitchGuardTime. More... | |
| otError | otThreadBecomeDetached (otInstance *aInstance) |
| Detach from the Thread network. More... | |
| otError | otThreadBecomeChild (otInstance *aInstance) |
| Attempt to reattach as a child. More... | |
| otError | otThreadGetNextNeighborInfo (otInstance *aInstance, otNeighborInfoIterator *aIterator, otNeighborInfo *aInfo) |
| This function gets the next neighbor information. More... | |
| otDeviceRole | otThreadGetDeviceRole (otInstance *aInstance) |
| Get the device role. More... | |
| otError | otThreadGetLeaderData (otInstance *aInstance, otLeaderData *aLeaderData) |
| This function get the Thread Leader Data. More... | |
| uint8_t | otThreadGetLeaderRouterId (otInstance *aInstance) |
| Get the Leader's Router ID. More... | |
| uint8_t | otThreadGetLeaderWeight (otInstance *aInstance) |
| Get the Leader's Weight. More... | |
| uint32_t | otThreadGetPartitionId (otInstance *aInstance) |
| Get the Partition ID. More... | |
| uint16_t | otThreadGetRloc16 (otInstance *aInstance) |
| Get the RLOC16. More... | |
| otError | otThreadGetParentInfo (otInstance *aInstance, otRouterInfo *aParentInfo) |
| The function retrieves diagnostic information for a Thread Router as parent. More... | |
| otError | otThreadGetParentAverageRssi (otInstance *aInstance, int8_t *aParentRssi) |
| The function retrieves the average RSSI for the Thread Parent. More... | |
| otError | otThreadGetParentLastRssi (otInstance *aInstance, int8_t *aLastRssi) |
| The function retrieves the RSSI of the last packet from the Thread Parent. More... | |
| const char * | otGetVersionString (void) |
| Get the OpenThread version string. More... | |
| otError | otThreadSetEnabled (otInstance *aInstance, bool aEnabled) |
| This function starts Thread protocol operation. More... | |
| bool | otThreadGetAutoStart (otInstance *aInstance) |
| This function queries if the Thread stack is configured to automatically start on reinitialization. More... | |
| otError | otThreadSetAutoStart (otInstance *aInstance, bool aStartAutomatically) |
| This function configures the Thread stack to automatically start on reinitialization. More... | |
| bool | otThreadIsSingleton (otInstance *aInstance) |
| This function indicates whether a node is the only router on the network. More... | |
| otError | otThreadDiscover (otInstance *aInstance, uint32_t aScanChannels, uint16_t aPanId, bool aJoiner, bool aEnableEui64Filtering, otHandleActiveScanResult aCallback, void *aCallbackContext) |
| This function starts a Thread Discovery scan. More... | |
| bool | otThreadIsDiscoverInProgress (otInstance *aInstance) |
| This function determines if an MLE Thread Discovery is currently in progress. More... | |
| const otIpCounters * | otThreadGetIp6Counters (otInstance *aInstance) |
| Get the IPv6 counters. More... | |
This file implements the OpenThread Thread API (for both FTD and MTD).
| const char* otGetVersionString | ( | void | ) |
Get the OpenThread version string.
PLATFORM_VERSION_ATTR_PREFIX and PLATFORM_VERSION_ATTR_SUFFIX are intended to be used to specify compiler directives to indicate what linker section the platform version string should be stored.
This is useful for specifying an exact locaiton of where the version string will be located so that it can be easily retrieved from the raw firmware image.
If PLATFORM_VERSION_ATTR_PREFIX is unspecified, the keyword static is used instead.
If both are unspecified, the location of the string in the firmware image will be undefined and may change.