0.01.00
settings.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016, The OpenThread Authors.
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions are met:
7  * 1. Redistributions of source code must retain the above copyright
8  * notice, this list of conditions and the following disclaimer.
9  * 2. Redistributions in binary form must reproduce the above copyright
10  * notice, this list of conditions and the following disclaimer in the
11  * documentation and/or other materials provided with the distribution.
12  * 3. Neither the name of the copyright holder nor the
13  * names of its contributors may be used to endorse or promote products
14  * derived from this software without specific prior written permission.
15  *
16  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
20  * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
26  * POSSIBILITY OF SUCH DAMAGE.
27  */
28 
35 #ifndef OT_PLATFORM_SETTINGS_H
36 #define OT_PLATFORM_SETTINGS_H 1
37 
38 #include <openthread/types.h>
39 
40 #ifdef __cplusplus
41 extern "C" {
42 #endif
43 
61 void otPlatSettingsInit(otInstance *aInstance);
62 
64 
85 
87 
106 
108 
131 
133 
175 otError otPlatSettingsGet(otInstance *aInstance, uint16_t aKey, int aIndex, uint8_t *aValue,
176  uint16_t *aValueLength);
177 
179 
204 otError otPlatSettingsSet(otInstance *aInstance, uint16_t aKey, const uint8_t *aValue, uint16_t aValueLength);
205 
207 
237 otError otPlatSettingsAdd(otInstance *aInstance, uint16_t aKey, const uint8_t *aValue, uint16_t aValueLength);
238 
240 
262 otError otPlatSettingsDelete(otInstance *aInstance, uint16_t aKey, int aIndex);
263 
265 
271 void otPlatSettingsWipe(otInstance *aInstance);
272 
278 #ifdef __cplusplus
279 } // extern "C"
280 #endif
281 
282 #endif // OT_PLATFORM_SETTINGS_H
This type represents all the static / global variables used by OpenThread allocated in one place...
Definition: openthread-instance.h:59
otError otPlatSettingsAdd(otInstance *aInstance, uint16_t aKey, const uint8_t *aValue, uint16_t aValueLength)
Adds a value to a setting.
This file defines the types and structures used in the OpenThread library API.
otError otPlatSettingsCommitChange(otInstance *aInstance)
Commit all settings changes since previous call to otPlatSettingsBeginChange()
void otPlatSettingsWipe(otInstance *aInstance)
Removes all settings from the setting store.
void otPlatSettingsInit(otInstance *aInstance)
Performs any initialization for the settings subsystem, if necessary.
otError otPlatSettingsSet(otInstance *aInstance, uint16_t aKey, const uint8_t *aValue, uint16_t aValueLength)
Sets or replaces the value of a setting.
otError otPlatSettingsGet(otInstance *aInstance, uint16_t aKey, int aIndex, uint8_t *aValue, uint16_t *aValueLength)
Fetches the value of a setting.
otError otPlatSettingsDelete(otInstance *aInstance, uint16_t aKey, int aIndex)
Removes a setting from the setting store.
otError otPlatSettingsAbandonChange(otInstance *aInstance)
Abandon all settings changes since previous call to otPlatSettingsBeginChange()
otError
This enumeration represents error codes used throughout OpenThread.
Definition: types.h:107
otError otPlatSettingsBeginChange(otInstance *aInstance)
Begin atomic change set.