![]() |
0.01.00
|
This module includes the platform abstraction for non-volatile storage of settings. More...
Functions | |
| void | otPlatSettingsInit (otInstance *aInstance) |
| Performs any initialization for the settings subsystem, if necessary. More... | |
| otError | otPlatSettingsBeginChange (otInstance *aInstance) |
| Begin atomic change set. More... | |
| otError | otPlatSettingsCommitChange (otInstance *aInstance) |
| Commit all settings changes since previous call to otPlatSettingsBeginChange() More... | |
| otError | otPlatSettingsAbandonChange (otInstance *aInstance) |
| Abandon all settings changes since previous call to otPlatSettingsBeginChange() More... | |
| otError | otPlatSettingsGet (otInstance *aInstance, uint16_t aKey, int aIndex, uint8_t *aValue, uint16_t *aValueLength) |
| Fetches the value of a setting. More... | |
| otError | otPlatSettingsSet (otInstance *aInstance, uint16_t aKey, const uint8_t *aValue, uint16_t aValueLength) |
| Sets or replaces the value of a setting. More... | |
| otError | otPlatSettingsAdd (otInstance *aInstance, uint16_t aKey, const uint8_t *aValue, uint16_t aValueLength) |
| Adds a value to a setting. More... | |
| otError | otPlatSettingsDelete (otInstance *aInstance, uint16_t aKey, int aIndex) |
| Removes a setting from the setting store. More... | |
| void | otPlatSettingsWipe (otInstance *aInstance) |
| Removes all settings from the setting store. More... | |
This module includes the platform abstraction for non-volatile storage of settings.
| otError otPlatSettingsAbandonChange | ( | otInstance * | aInstance | ) |
Abandon all settings changes since previous call to otPlatSettingsBeginChange()
This function may be called at the end of a sequence of changes. instead of otPlatSettingsCommitChange(). If implemented, it causes all changes made since otPlatSettingsBeginChange() to be rolled back and abandoned.
The implementation of this function is optional. If not implemented, it should return OT_ERROR_NOT_IMPLEMENTED.
| [in] | aInstance | The OpenThread instance structure. |
| OT_ERROR_NONE | The changes made since the last call to otPlatSettingsBeginChange() have been successfully rolled back. |
| OT_ERROR_INVALID_STATE | otPlatSettingsBeginChange() has not been called. |
| OT_ERROR_NOT_IMPLEMENTED | This function is not implemented on this platform. |
| otError otPlatSettingsAdd | ( | otInstance * | aInstance, |
| uint16_t | aKey, | ||
| const uint8_t * | aValue, | ||
| uint16_t | aValueLength | ||
| ) |
Adds a value to a setting.
This function adds the value to a setting identified by aKey, without replacing any existing values.
Note that the underlying implementation is not required to maintain the order of the items associated with a specific key. The added value may be added to the end, the beginning, or even somewhere in the middle. The order of any pre-existing values may also change.
Calling this function successfully may cause unrelated settings with multiple values to be reordered.
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aKey | The key associated with the setting to change. |
| [out] | aValue | A pointer to where the new value of the setting should be read from. MUST NOT be NULL if aValueLength is non-zero. |
| [in,out] | aValueLength | The length of the data pointed to by aValue. May be zero. |
| OT_ERROR_NONE | The given setting was added or staged to be added. |
| OT_ERROR_NOT_IMPLEMENTED | This function is not implemented on this platform. |
| otError otPlatSettingsBeginChange | ( | otInstance * | aInstance | ) |
Begin atomic change set.
This function is called at the start of a sequence of changes that should be made atomically.
This function, along with otPlatSettingsCommitChange() are designed to ensure atomicity of changes to multiple settings. Once this function has been called, any changes made to the settings store are only committed when otPlatSettingsCommitChange() is called.
The implementation of this function is optional. If not implemented, it should return OT_ERROR_NONE.
| [in] | aInstance | The OpenThread instance structure. |
| OT_ERROR_NONE | The settings commit lock has been set. |
| OT_ERROR_ALREADY | The commit lock is already set. |
| otError otPlatSettingsCommitChange | ( | otInstance * | aInstance | ) |
Commit all settings changes since previous call to otPlatSettingsBeginChange()
This function is called at the end of a sequence of changes. The implementation of this function is optional. If not implemented, it should return OT_ERROR_NOT_IMPLEMENTED.
| [in] | aInstance | The OpenThread instance structure. |
| OT_ERROR_NONE | The changes made since the last call to otPlatSettingsBeginChange() have been successfully committed. |
| OT_ERROR_INVALID_STATE | otPlatSettingsBeginChange() has not been called. |
| OT_ERROR_NOT_IMPLEMENTED | This function is not implemented on this platform. |
| otError otPlatSettingsDelete | ( | otInstance * | aInstance, |
| uint16_t | aKey, | ||
| int | aIndex | ||
| ) |
Removes a setting from the setting store.
This function deletes a specific value from the setting identified by aKey from the settings store.
Note that the underlying implementation is not required to maintain the order of the items associated with a specific key.
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aKey | The key associated with the requested setting. |
| [in] | aIndex | The index of the value to be removed. If set to -1, all values for this aKey will be removed. |
| OT_ERROR_NONE | The given key and index was found and removed successfully. |
| OT_ERROR_NOT_FOUND | The given key or index was not found in the setting store. |
| OT_ERROR_NOT_IMPLEMENTED | This function is not implemented on this platform. |
| otError otPlatSettingsGet | ( | otInstance * | aInstance, |
| uint16_t | aKey, | ||
| int | aIndex, | ||
| uint8_t * | aValue, | ||
| uint16_t * | aValueLength | ||
| ) |
Fetches the value of a setting.
This function fetches the value of the setting identified by aKey and write it to the memory pointed to by aValue. It then writes the length to the integer pointed to by aValueLength. The initial value of aValueLength is the maximum number of bytes to be written to aValue.
This function can be used to check for the existence of a key without fetching the value by setting aValue and aValueLength to NULL. You can also check the length of the setting without fetching it by setting only aValue to NULL.
Note that the underlying storage implementation is not required to maintain the order of settings with multiple values. The order of such values MAY change after ANY write operation to the store.
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aKey | The key associated with the requested setting. |
| [in] | aIndex | The index of the specific item to get. |
| [out] | aValue | A pointer to where the value of the setting should be written. May be set to NULL if just testing for the presence or length of a setting. |
| [in,out] | aValueLength | A pointer to the length of the value. When called, this pointer should point to an integer containing the maximum value size that can be written to aValue. At return, the actual length of the setting is written. This may be set to NULL if performing a presence check. |
| OT_ERROR_NONE | The given setting was found and fetched successfully. |
| OT_ERROR_NOT_FOUND | The given setting was not found in the setting store. |
| OT_ERROR_NOT_IMPLEMENTED | This function is not implemented on this platform. |
| void otPlatSettingsInit | ( | otInstance * | aInstance | ) |
Performs any initialization for the settings subsystem, if necessary.
| [in] | aInstance | The OpenThread instance structure. |
| otError otPlatSettingsSet | ( | otInstance * | aInstance, |
| uint16_t | aKey, | ||
| const uint8_t * | aValue, | ||
| uint16_t | aValueLength | ||
| ) |
Sets or replaces the value of a setting.
This function sets or replaces the value of a setting identified by aKey. If there was more than one value previously associated with aKey, then they are all deleted and replaced with this single entry.
Calling this function successfully may cause unrelated settings with multiple values to be reordered.
| [in] | aInstance | The OpenThread instance structure. |
| [in] | aKey | The key associated with the setting to change. |
| [out] | aValue | A pointer to where the new value of the setting should be read from. MUST NOT be NULL if aValueLength is non-zero. |
| [in] | aValueLength | The length of the data pointed to by aValue. May be zero. |
| OT_ERROR_NONE | The given setting was changed or staged. |
| OT_ERROR_NOT_IMPLEMENTED | This function is not implemented on this platform. |
| void otPlatSettingsWipe | ( | otInstance * | aInstance | ) |
Removes all settings from the setting store.
This function deletes all settings from the settings store, resetting it to its initial factory state.
| [in] | aInstance | The OpenThread instance structure. |