TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Modules | Data Structures | Typedefs
GAP Structures

Modules

 GAP Events
 

Data Structures

struct  gapAdvDataToken_t
 GAP Advertisement/Scan Response Data Token. More...
 
struct  gapAdvertisingParams_t
 Advertising Parameters. More...
 
struct  gapAuthParams_t
 Authentication Parameters. More...
 
struct  gapDevDiscReq_t
 Type of device discovery (Scan) to perform. More...
 
struct  gapDevRec_t
 Type of device discovery (Scan) to perform. More...
 
struct  gapEstLinkReq_t
 Establish Link Request parameters. More...
 
struct  gapEventHdr_t
 GAP event header format. More...
 
struct  gapPairingReq_t
 Pairing Request fields - the parsed fields of the SMP Pairing Request command. More...
 
struct  gapPeriConnectParams_t
 Connection parameters for the peripheral device. More...
 
struct  gapUpdateLinkParamReq_t
 Update Link Parameters Request parameters. More...
 
struct  gapUpdateLinkParamReqReply_t
 Update Link Parameters Request Reply parameters. More...
 

Typedefs

typedef uint16 gapParamIDs_t
 GAP Parameters IDs. More...
 

Detailed Description

Typedef Documentation

§ gapParamIDs_t

typedef uint16 gapParamIDs_t

GAP Parameters IDs.

GAP Parameter IDs

Copyright 2017, Texas Instruments Incorporated