TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gapUpdateLinkParamReqReply_t Struct Reference

Update Link Parameters Request Reply parameters. More...

Data Fields

uint8 accepted
 TRUE if host accepts parameter update, FALSE otherwise.
 
uint16 connectionHandle
 Connection handle of the update.
 
uint16 connLatency
 Connection Latency.
 
uint16 connTimeout
 Connection Timeout.
 
uint16 intervalMax
 Maximum Connection Interval.
 
uint16 intervalMin
 Minimum Connection Interval.
 

Detailed Description

Update Link Parameters Request Reply parameters.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated