TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gapAuthParams_t Struct Reference

Authentication Parameters. More...

Data Fields

uint16 connectionHandle
 Connection Handle from controller,.
 
smLinkSecurityReq_t secReqs
 Pairing Control info.
 

Detailed Description

Authentication Parameters.

securityInfo and identityInfo are only used if secReqs.bondable == BOUND, which means that the device is already bound and we should use the security information and keys.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated