TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gapPairingReq_t Struct Reference

Pairing Request fields - the parsed fields of the SMP Pairing Request command. More...

Data Fields

uint8 authReq
 Pairing Request Auth Req field.
 
uint8 ioCap
 Pairing Request ioCap field.
 
keyDist_t keyDist
 Pairing Request Key Distribution field.
 
uint8 maxEncKeySize
 Pairing Request Maximum Encryption Key Size field.
 
uint8 oobDataFlag
 Pairing Request OOB Data Flag field.
 

Detailed Description

Pairing Request fields - the parsed fields of the SMP Pairing Request command.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated