TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gapAdvertisingParams_t Struct Reference

Advertising Parameters. More...

Data Fields

uint8 channelMap
 Channel Map: Bit mask GAP Advertisement Channel Map.
 
uint8 eventType
 Advertise Event Type: GAP Advertising Event Types.
 
uint8 filterPolicy
 Filer Policy: GAP Advertiser Filter Scan Parameters. Ignored when directed advertising is used.
 
uint8 initiatorAddr [B_ADDR_LEN]
 Initiator's addr - used only with connectable directed eventType (ADV_EVTTYPE_CONNECTABLE_DIRECTED).
 
uint8 initiatorAddrType
 Initiator's address type: Address Types.
 

Detailed Description

Advertising Parameters.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated