TIOVX User Guide
|
Implementation of Target Object APIs. More...
#include <TI/tivx_config.h>
Go to the source code of this file.
Data Structures | |
struct | tivx_target_t |
Target object internal state. More... | |
struct | tivx_target_create_params_t |
Parameters that can be set during target creation. More... | |
Macros | |
#define | TIVX_TARGET_INST_MASK (0xFFu) |
Target ID bit mask. More... | |
#define | TIVX_TARGET_INST_SHIFT (0x0u) |
Target ID bit mask. More... | |
#define | TIVX_CPU_ID_MASK (0xFu) |
CPU ID bit mask. More... | |
#define | TIVX_CPU_ID_SHIFT (0x8) |
CPU ID bit shift. More... | |
#define | TIVX_TARGET_ID_MASK |
Target ID bit mask. | |
#define | TIVX_TARGET_ID_SHIFT (TIVX_TARGET_INST_SHIFT) |
Target ID bit shift. | |
#define | TIVX_MAKE_TARGET_ID(cpu, target_inst) (((((uint32_t)(((uint32_t)cpu) & (uint32_t)TIVX_CPU_ID_MASK)) << (uint32_t)TIVX_CPU_ID_SHIFT) |(((uint32_t)(((uint32_t)target_inst)&(uint32_t)TIVX_TARGET_INST_MASK)) << (uint32_t)TIVX_TARGET_INST_SHIFT))) |
Make target based on CPU ID. More... | |
#define | TIVX_GET_CPU_ID(target) ((((uint32_t)(target) >> (uint32_t)TIVX_CPU_ID_SHIFT) & (uint32_t)TIVX_CPU_ID_MASK)) |
Get CPU Id from given target. More... | |
#define | TIVX_GET_TARGET_INST(target) ((uint16_t)(((uint16_t)(target) >> TIVX_TARGET_INST_SHIFT)) & TIVX_TARGET_INST_MASK) |
Get the target instances from target. More... | |
#define | TIVX_TARGET_ID_INVALID (0xFFFFFFFFU) |
Const to denote invalid ID's. | |
#define | TIVX_CPU_ID_INVALID (0xFFFFFFFFu) |
Const to denote invalid ID's. | |
#define | TIVX_TARGET_MAX_TASK_NAME (12u) |
Max size of target name string. | |
#define | TIVX_TARGET_MAX_JOB_QUEUE_DEPTH (96u) |
Max depth of queue associated with target. More... | |
Typedefs | |
typedef struct _tivx_target * | tivx_target |
Target Object. | |
typedef void(* | own_execute_user_kernel_f) (tivx_obj_desc_node_t *node_obj_desc, uint16_t prm_obj_desc_id[]) |
The pointer to the user kernel wrapper within the tiovx framework. This is only executable on the host, therefore putting a function pointer that gets initialized to non-NULL only when ownRegisterFunctionsForHost is called from hostInit. More... | |
typedef void(* | own_target_cmd_desc_handler_f) (const tivx_obj_desc_cmd_t *cmd_obj_desc) |
The pointer to the handler of a subset of cases that the target command handler needs to service on the same core that the host runs on. This is only executable on the host, therefore putting a function pointer that gets initialized to non-NULL only when ownRegisterFunctionsForHost is called from hostInit. More... | |
Enumerations | |
enum | tivx_target_cmd_e { TIVX_CMD_NODE_CREATE = 0x00000001u, TIVX_CMD_NODE_DELETE = 0x00000002u, TIVX_CMD_NODE_CONTROL = 0x00000003u, TIVX_CMD_NODE_USER_CALLBACK = 0x00000004u, TIVX_CMD_DATA_REF_CONSUMED = 0x00000005u } |
Command ID for commands that can be send to a target. More... | |
Functions | |
void | ownRegisterFunctionsForHost (void) |
Register Various functions within target files to be linked for host usage. More... | |
vx_enum | ownTargetGetCpuId (vx_enum target_id) |
Get CPU ID associated with given target ID. More... | |
vx_status | ownTargetQueueObjDesc (vx_enum target_id, uint16_t obj_desc_id) |
Queue object descriptor to a given target. More... | |
void | ownTargetTriggerNode (uint16_t node_obj_desc_id) |
Trigger execution of a node obj desc. | |
void | ownTargetNodeDescAcquireAllParameters (tivx_obj_desc_node_t *node_obj_desc, uint16_t prm_obj_desc_id[], vx_bool *is_node_blocked) |
Acquire parameters for node execution. | |
void | ownTargetNodeDescAcquireAllParametersForPipeup (tivx_obj_desc_node_t *node_obj_desc, uint16_t prm_obj_desc_id[]) |
Acquire parameters for node execution during pipeup phase. | |
void | ownTargetNodeDescReleaseAllParameters (tivx_obj_desc_node_t *node_obj_desc, uint16_t prm_obj_desc_id[]) |
Release parameters that were previously acquired. | |
void | ownTargetSetDefaultCreateParams (tivx_target_create_params_t *params) |
Used to set default target create parameters in parameter structure. More... | |
vx_status | ownTargetCreate (vx_enum target_id, const tivx_target_create_params_t *params) |
Create a target object and associate with given target ID. More... | |
vx_status | ownTargetDelete (vx_enum target_id) |
Delete a target object. More... | |
void | ownTargetInit (void) |
Init global state of target module. More... | |
void | ownTargetDeInit (void) |
De-Init global state of target module. More... | |
void | ownTargetSetTimestamp (const tivx_obj_desc_node_t *node_obj_desc, tivx_obj_desc_t *obj_desc[]) |
Propagates time stamp of input parameters of a kernel to output parameters. | |
Implementation of Target Object APIs.
Definition in file tivx_target.h.