TIOVX User Guide
tivx_target_create_params_t Struct Reference

Parameters that can be set during target creation. More...

#include <tivx_target.h>

Data Fields

uint8_t * task_stack_ptr
 Pointer to task stack, if NULL then task stack is allcoated by OS and not supplied by user.
 
uint32_t task_stack_size
 Task stack size, if 0, OS allocates stack with default size.
 
uint32_t task_core_affinity
 If task runs on a SMP CPU then this value tells the affinity of task to a given core, Valid values are 0 .. max cores in the SMP CPU. when TIVX_TASK_AFFINITY_ANY is used OS decides the task affinity.
 
uint32_t task_priority
 task priority for task associated with this target TIVX_TASK_PRI_HIGHEST is highest priority, TIVX_TASK_PRI_LOWEST is lowest priority
 
char task_name [TIVX_TARGET_MAX_TASK_NAME]
 Task name associated with this target.
 

Detailed Description

Parameters that can be set during target creation.

Definition at line 228 of file tivx_target.h.


The documentation for this struct was generated from the following file: