PDK API Guide for J721E
|
Interrupt register routines.
============================================================================
Go to the source code of this file.
Osal Interrupt return Codes | |
#define | OSAL_INT_SUCCESS ((int32_t) 0) |
#define | OSAL_INT_ERR_INVALID_PARAMS ((int32_t) -1) |
#define | OSAL_INT_ERR_HWICREATE ((int32_t) -2) |
#define | OSAL_INT_ERR_EVENTCOMBINER_REG ((int32_t) -3) |
#define | OSAL_INT_ERR_DELETE ((int32_t) -4) |
#define | OSAL_INT_UNSUPPORTED ((int32_t) -5) |
typedef int32_t | OsalInterruptRetCode_e |
Return error codes for Osal Interrupt functions. More... | |
Data Structures | |
struct | OsalRegisterIntParams_corepac_t |
Interrupt Configuration parameters for the corepac (c6x/a15/m5/a8/a9) More... | |
struct | OsalRegisterIntParams_socmux_t |
Interrupt Configuration parameters for soc mux prior to reaching the core. More... | |
struct | OsalRegisterIntrParams_t |
Interrupt Configuration parameters This is the data structure used to configure the interrupts in the system. coreConfig: This part configures the interrupt for corepac such as c66x, arm, m4 socMuxConfig: This part configures the interrupt path for any SOC level mux such as CIC/GIC or cross bar, leading up to the corepac. More... | |
Macros | |
#define | OSAL_REGINT_INTVEC_EVENT_COMBINER (16) |
For C6x, if intVec=16, then event combiner is to be used. More... | |
Typedefs | |
typedef void(* | Osal_IsrRoutine) (uintptr_t arg) |
Functions | |
void | Osal_RegisterInterrupt_initParams (OsalRegisterIntrParams_t *interruptRegParams) |
Function to initialize the interrupt registration configuration data structure. More... | |
OsalInterruptRetCode_e | Osal_RegisterInterruptDirect (OsalRegisterIntrParams_t *interruptRegParams, HwiP_DirectFxn isrFxn, HwiP_Handle *hwiPHandlePtr) |
Function to register direct interrupt with parameters provided. More... | |
OsalInterruptRetCode_e | Osal_RegisterInterrupt (OsalRegisterIntrParams_t *interruptRegParams, HwiP_Handle *hwiPHandlePtr) |
Function to register interrupt with parameters provided. More... | |
OsalInterruptRetCode_e | Osal_DeleteInterrupt (HwiP_Handle hwiPhandle, int32_t corepacEventNum) |
Function to delete interrupt corresponding to an event number. More... | |
void | Osal_EnableInterrupt (int32_t corepacEvent, int32_t interruptNum) |
Function to enable the interrupt corresponding to an event number. More... | |
void | Osal_DisableInterrupt (int32_t corepacEvent, int32_t interruptNum) |
Function to disable the interrupt corresponding to an event number. More... | |
void | Osal_ClearInterrupt (int32_t corepacEvent, int32_t interruptNum) |
Function to clear the interrupt corresponding to an event number. More... | |