![]() |
PDK API Guide for J721E
|
Interrupt Configuration parameters This is the data structure used to configure the interrupts in the system. coreConfig: This part configures the interrupt for corepac such as c66x, arm, m4 socMuxConfig: This part configures the interrupt path for any SOC level mux such as CIC/GIC or cross bar, leading up to the corepac.
Data Fields | |
OsalRegisterIntParams_corepac_t | corepacConfig |
OsalRegisterIntParams_socmux_t | socMuxConfig |
OsalRegisterIntParams_corepac_t OsalRegisterIntrParams_t::corepacConfig |
configures the interrupt for corepac such as c66x, arm, m4
OsalRegisterIntParams_socmux_t OsalRegisterIntrParams_t::socMuxConfig |
configures the interrupt path for any SOC level mux such as CIC/GIC or cross bar, leading up to the corepac