![]() |
![]() |
TI-RTOS Drivers
tidrivers_msp43x_2_16_00_08
|
CCamera_Config | Camera Global configuration |
CCamera_FxnTable | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
CCamera_Params | Camera Parameters |
CClockP_FreqHz | Frequency-in-hertz struct |
CClockP_Params | Basic ClockP Parameters |
CDIR | |
Cdiskio_fxns | |
CEMAC_Config | EMAC Global configuration |
CEMAC_FxnTable | EMAC Function table structure |
CFATFS | |
CFIL | |
CFILINFO | |
CGPIOMSP430_Config | GPIO device specific driver configuration structure |
CGPIOMSP432_Config | GPIO device specific driver configuration structure |
CHwiP_Params | Basic HwiP Parameters |
CI2C_Config | I2C Global configuration |
CI2C_FxnTable | The definition of a I2C function table that contains the required set of functions to control a specific I2C driver implementation |
CI2C_Params | I2C Parameters |
CI2C_Transaction | I2C transaction |
CI2CEUSCIB_HWAttrs | I2CEUSCIB Hardware attributes |
CI2CEUSCIB_Object | I2CEUSCIB Object |
CI2CMSP432_HWAttrs | I2CMSP432 Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
CI2CMSP432_Object | I2CMSP432 Object |
CI2CUSCIB_HWAttrs | I2CUSCIB Hardware attributes |
CI2CUSCIB_Object | I2CUSCIB Object |
CI2S_BufDesc | I2S buffer descriptor for issue/reclaim mode |
CI2S_Config | I2S Global configuration |
CI2S_FxnTable | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
CI2S_Params | Basic I2S Parameters |
CList_Elem | |
CList_List | |
CMutexP_Params | Basic MutexP Parameters |
CNVS_Attrs | NVS attributes |
CNVS_Config | NVS Global configuration |
CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
CNVS_Params | NVS Parameters |
CNVSMSP432_CmdSetCopyBlockArgs | NVSMSP432 command structure for setting copy block |
CNVSMSP432_HWAttrs | NVSMSP432 attributes |
CNVSMSP432_Object | |
CPIN_State_s | Underlying data structure for type PIN_State |
CPower_NotifyObj | Power notify object structure |
CPowerMSP432_Config | Power global configuration (MSP432-specific) |
CPowerMSP432_Freqs | Structure holding device frequencies (in Hz) |
CPWM_Config | PWM Global configuration |
CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
CPWM_Params | PWM Parameters |
CPWMTimerMSP432_HWAttrs | PWMTimerMSP432 Hardware attributes |
CPWMTimerMSP432_Object | PWMTimerMSP432 Object |
CPWMTimerMSP432_Status | PWMTimerMSP432_Status |
CRingBuf_Object | |
CSDSPI_Config | SDSPI Global configuration |
CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
CSDSPI_Params | SDSPI Parameters |
CSDSPIEUSCIA_HWAttrsV1 | SDSPIEUSCIA Hardware attributes |
CSDSPIEUSCIA_Object | SDSPIEUSCIA Object |
CSDSPIEUSCIB_HWAttrsV1 | SDSPIEUSCIB Hardware attributes |
CSDSPIEUSCIB_Object | SDSPIEUSCIB Object |
CSDSPIMSP432_HWAttrs | SDSPIMSP432 Hardware attributes |
CSDSPIMSP432_Object | SDSPIMSP432 Object |
CSDSPIUSCIA_HWAttrs | SDSPIUSCIA Hardware attributes |
CSDSPIUSCIA_Object | SDSPIUSCIA Object |
CSDSPIUSCIB_HWAttrs | SDSPIUSCIB Hardware attributes |
CSDSPIUSCIB_Object | SDSPIUSCIB Object |
CSemaphoreP_Params | Basic SemaphoreP Parameters |
CSPI_Config | SPI Global configuration |
CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
CSPI_Params | SPI Parameters |
CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
CSPIEUSCIADMA_HWAttrs | SPIEUSCIADMA Hardware attributes |
CSPIEUSCIADMA_Object | SPIEUSCIADMA Object |
CSPIEUSCIBDMA_HWAttrs | SPIEUSCIBDMA Hardware attributes |
CSPIEUSCIBDMA_Object | SPIEUSCIBDMA Object |
CSPIMSP432DMA_HWAttrs | SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
CSPIMSP432DMA_Object | SPIMSP432DMA Object |
CSPIUSCIADMA_HWAttrs | SPIUSCIADMA Hardware attributes |
CSPIUSCIADMA_Object | SPIUSCIADMA Object |
CSPIUSCIBDMA_HWAttrs | SPIUSCIBDMA Hardware attributes |
CSPIUSCIBDMA_Object | SPIUSCIBDMA Object |
CUART_Config | UART Global configuration |
CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
CUART_Params | UART Parameters |
CUARTEUSCIA_BaudrateConfig | UARTEUSCIA Baudrate configuration |
CUARTEUSCIA_HWAttrs | UARTEUSCIA Hardware attributes |
CUARTEUSCIA_Object | UARTEUSCIA Object |
CUARTMSP432_BaudrateConfig | UARTMSP432 Baudrate configuration |
CUARTMSP432_FxnSet | Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only |
CUARTMSP432_HWAttrs | UARTMSP432 Hardware attributes |
CUARTMSP432_Object | UARTMSP432 Object |
CUARTUSCIA_BaudrateConfig | UARTUSCIA Baudrate configuration |
CUARTUSCIA_HWAttrs | UARTUSCIA Hardware attributes |
CUARTUSCIA_Object | UARTUSCIA Object |
CUSBMSCHFatFs_Config | USBMSCHFatFs Global configuration |
CUSBMSCHFatFs_FxnTable | The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation |
CUSBMSCHFatFs_Params | USBMSCHFatFs Parameters |
CWatchdog_Config | Watchdog Global configuration |
CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
CWatchdog_Params | Watchdog Parameters |
CWatchdogMSP430_HWAttrs | Watchdog hardware attributes for MSP430 |
CWatchdogMSP430_Object | Watchdog Object for MSP430 |
CWatchdogMSP432_HWAttrs | Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in: |
CWatchdogMSP432_Object | Watchdog Object for MSP432 |
CWiFi_Config | WiFi Global configuration |
CWiFi_FxnTable | The definition of a WiFi function table that contains the required set of functions to control a specific WiFi driver implementation |
CWiFi_Params | WiFi Parameters |
CWiFiCC3100_HWAttrs | WiFiCC3100 Hardware attributes |
CWiFiCC3100_Object | WiFiCC3100 Object |