![]() |
![]() |
TI-RTOS Drivers
tidrivers_msp43x_2_16_00_08
|
SDSPIUSCIB Hardware attributes. More...
#include <SDSPIUSCIB.h>
Data Fields | |
uint32_t | baseAddr |
uint8_t | clockSource |
uint8_t | portSCK |
uint32_t | pinSCK |
uint8_t | portMISO |
uint32_t | pinMISO |
uint8_t | portMOSI |
uint32_t | pinMOSI |
uint8_t | portCS |
uint32_t | pinCS |
SDSPIUSCIB Hardware attributes.
The SDSPIUSCIB configuration structure describes to the SDSPIUSCIB driver implementation hardware specifies on which SPI peripheral, GPIO Pins and Ports are to be used.
The SDSPIUSCIB driver uses this information to:
These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For TivaWare these definitions are found in:
An example configuration structure could look as the following:
uint32_t SDSPIUSCIB_HWAttrs::baseAddr |
SPI Peripheral's base address
uint8_t SDSPIUSCIB_HWAttrs::clockSource |
SPIUSCI Clock source
uint8_t SDSPIUSCIB_HWAttrs::portSCK |
SPI port uses for the SCK, MISO, and MOSI pins
uint32_t SDSPIUSCIB_HWAttrs::pinSCK |
SPI SCK pin
uint8_t SDSPIUSCIB_HWAttrs::portMISO |
SPI port uses for the SCK, MISO, and MOSI pins
uint32_t SDSPIUSCIB_HWAttrs::pinMISO |
SPI MISO pin
uint8_t SDSPIUSCIB_HWAttrs::portMOSI |
SPI port uses for the SCK, MISO, and MOSI pins
uint32_t SDSPIUSCIB_HWAttrs::pinMOSI |
SPI MOSI pin
uint8_t SDSPIUSCIB_HWAttrs::portCS |
GPIO Port used for the chip select
uint32_t SDSPIUSCIB_HWAttrs::pinCS |
GPIO Pin used for the chip select