Functions |
Int32 | SPHENC1_control (SPHENC1_Handle handle, SPHENC1_Cmd id, SPHENC1_DynamicParams *params, SPHENC1_Status *status) |
| Execute the control() method in this instance of a speech encoder algorithm.
|
SPHENC1_Handle | SPHENC1_create (Engine_Handle e, String name, SPHENC1_Params *params) |
| Create an instance of a speech encoder algorithm.
|
Void | SPHENC1_delete (SPHENC1_Handle handle) |
| Delete the instance of a speech encoder algorithm.
|
Int32 | SPHENC1_process (SPHENC1_Handle handle, XDM1_SingleBufDesc *inBuf, XDM1_SingleBufDesc *outBuf, SPHENC1_InArgs *inArgs, SPHENC1_OutArgs *outArgs) |
| Execute the process() method in this instance of a speech encoder algorithm.
|
XDAS_Int32 | SPHENC1_processAsync (SPHENC1_Handle handle, XDM1_SingleBufDesc *inBuf, XDM1_SingleBufDesc *outBuf, SPHENC1_InArgs *inArgs, SPHENC1_OutArgs *outArgs) |
| Perform asynchronous submission to this instance of a speech encoder algorithm.
|
XDAS_Int32 | SPHENC1_processWait (SPHENC1_Handle handle, XDM1_SingleBufDesc *inBuf, XDM1_SingleBufDesc *outBuf, SPHENC1_InArgs *inArgs, SPHENC1_OutArgs *outArgs, UInt timeout) |
| Wait for a return message from a previous invocation of SPHENC1_processAsync() in this instance of an speech encoder algorithm.
|
Detailed Description
This is the SPHENC1 speech encoder interface. Several of the data types in this API are specified by the XDM ISPHENC1 interface; please see the XDM documentation for those details.
Macro Definition Documentation
Special value for timeout parameter indicating never timeout.
#define SPHENC1_VISATYPE "ti.sdo.ce.speech1.ISPHENC1" |
#define SPHENC1_STUBSNAME "SPHENC1_STUBS" |
Name of stub functions. Use this name when registering the SPHENC1_STUBS functions with Engine_addStubFxns.
- See also:
- Engine_addStubFxns
Typedef Documentation
Opaque handle to a SPHENC1 codec.
Defines the creation time parameters for all ISPHENC1 instance objects.
@remarks Some of the fields in this structure are optional and depend
on the class of speech encoder you're creating.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
Defines the input arguments for all ISPHENC1 instance process function.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
Defines the run time output arguments for all ISPHENC1 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
This structure defines the codec parameters that can be modified after creation via ISPHENC1_Fxns.control().
@remarks It is not necessary that a given implementation support all
dynamic parameters to be configurable at run time. If a
particular algorithm does not support run-time updates to
a parameter that the application is attempting to change
at runtime, it may indicate this as an error.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
Defines instance status parameters.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
Function Documentation
Execute the control() method in this instance of a speech encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created speech encoder instance. |
[in] | id | Command id for XDM control operation. |
[in] | params | Runtime control parameters used for encoding. |
[out] | status | Status info upon completion of encode operation. |
- Precondition:
handle
is a valid (non-NULL) speech encoder handle and the speech encoder is in the created state.
- Return values:
-
- See also:
- SPHENC1_create()
-
SPHENC1_delete()
-
ISPHENC1_Fxns::control()
Create an instance of a speech encoder algorithm.
Instance handles must not be concurrently accessed by multiple threads;
each thread must either obtain its own handle (via SPHENC1_create()) or
explicitly serialize access to a shared handle.
@param[in] e Handle to an opened engine.
@param[in] name String identifier of the type of speech encoder
to create.
@param[in] params Creation parameters.
@retval NULL An error has occurred.
@retval non-NULL The handle to the newly created speech encoder
instance.
@remarks @c params is optional. If it's not supplied, codec-specific
default params will be used.
@remark Depending on the configuration of the engine opened, this
call may create a local or remote instance of the speech1
encoder.
@remarks In general, @c name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form <b>":priority"</b>, <b>":priority:flag"</b>, or <b>"::flag"</b>.
Delete the instance of a speech encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created speech encoder instance. |
- Precondition:
handle
is a valid (non-NULL) handle which is in the created state.
- Postcondition:
- All resources allocated as part of the SPHENC1_create() operation (memory, DMA channels, etc.) are freed.
- See also:
- SPHENC1_create()
Execute the process() method in this instance of a speech encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created speech encoder instance. |
[in,out] | inBuf | A buffer descriptor containing an input buffer. |
[out] | outBuf | A buffer descriptor containing an output buffer. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
- Precondition:
handle
is a valid (non-NULL) speech encoder handle and the speech encoder is in the created state.
- Return values:
-
- See also:
- SPHENC1_create()
-
SPHENC1_delete()
-
SPHENC1_control()
-
SPHENC1_processAsync()
-
SPHENC1_processWait()
-
ISPHENC1_Fxns::process() - the reflected algorithm interface, which may contain further usage details.
Perform asynchronous submission to this instance of a speech encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created speech encoder instance. |
[in] | inBuf | A buffer descriptor containing the input buffer. |
[out] | outBuf | A buffer descriptor containing the output buffer. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
- Precondition:
handle
is a valid (non-NULL) speech encoder handle and the speech encoder is in the created state.
- Return values:
-
- See also:
- SPHENC1_create()
-
SPHENC1_delete()
-
SPHENC1_control()
-
SPHENC1_process()
-
SPHENC1_processWait()
-
ISPHENC1_Fxns::process()
Wait for a return message from a previous invocation of SPHENC1_processAsync() in this instance of an speech encoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created speech encoder instance. |
[in] | inBuf | A buffer descriptor containing the input buffer. |
[out] | outBuf | A buffer descriptor containing the output buffer. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
[in] | timeout | Amount of "time" to wait (from 0 -> SPHENC1_FOREVER) |
- Precondition:
handle
is a valid (non-NULL) speech encoder handle and the speech encoder is in the created state.
- Return values:
-
- See also:
- SPHENC1_create()
-
SPHENC1_delete()
-
SPHENC1_control()
-
SPHENC1_process()
-
SPHENC1_processAsync()