![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Data Structures | |
struct | Engine_Attrs |
Attributes of an Engine. More... | |
struct | Engine_AlgInfo |
Properties of an Engine algorithm. More... | |
struct | Engine_AlgInfo2 |
Properties of an Engine algorithm. More... | |
struct | Engine_AlgDesc |
Descriptor for an alg. This object can be passed to Engine_addAlg() , to dynamically add an alg to an engine. More... | |
struct | Engine_DllAlgDesc |
Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type. More... | |
struct | Engine_Desc |
This structure is passed to Engine_add() , and contains parameters to specify an engine. More... |
Macros | |
#define | CE_NULL_algs NULL |
#define | CE_DECLARE_TYPE(name, types) |
Macros for runtime configuration. These macros can be used to create a static table of algorithms. However, the preferred method of building engine and alg tables, is to use the run-time APIs, Engine_add() and Engine_addAlg(). | |
#define | CE_LOCAL_ALG(name, algName, ialgFxns, idma3Fxns, iresFxns, groupId, memType) |
Generates a structure containing data for a local algorithm. | |
#define | CE_LOCAL_ALG2(algName, ialgFxns, idma3Fxns, iresFxns, groupId, memType, types) |
Generates a structure containing data for a local algorithm. This macro takes a 'types' string as an argument to avoid having to use the CE_DECLARE_TYPES() macro call. | |
#define | CE_DECLARE_LOCAL_ALG(name, algName, ialgFxns, idma3Fxns, iresFxns, groupId, memType, types) |
Generates a static variable of type Engine_AlgDesc. It is used in this manner: | |
#define | ALG_TABLE_NAME_LHS(name) CE_##name |
Use this macro and the CE_END_ALG_TABLE() macro around CE_LOCAL_ALG() to generate an algorithm table for an engine. | |
#define | ALG_TABLE_RHS(name) name##_algs[] |
#define | CE_BEGIN_ALG_TABLE(name) static Engine_AlgDesc ALG_TABLE_RHS(ALG_TABLE_LHS(name)) |
#define | CE_END_ALG_TABLE(name) |
Use this macro after CE_BEGIN_ALG_TABLE() and CE_LOCAL_ALG() for generating an algorithm table for an engine. | |
#define | CE_ENGINE(algTab, engName, serverName, memMap, useExtLoader, heapId) |
Generates a structure containing data for an engine. | |
#define | CE_BEGIN_ENGINE_TABLE(name) |
Use this macro and the CE_END_ENGINE_TABLE() macro around CE_ENGINE() to generate an engine table for the application. | |
#define | CE_END_ENGINE_TABLE(name) |
Use this macro and the CE_BEGIN_ENGINE_TABLE() macro around CE_ENGINE() to generate an engine table for the application. | |
#define | Engine_MODNAME "ti.sdo.ce.Engine" |
Name to pass to Diags_setMask() to enable logging for Engine functions. | |
#define | Engine_EOK 0 |
#define | Engine_EEXIST 1 |
#define | Engine_ENOMEM 2 |
#define | Engine_EDSPLOAD 3 |
#define | Engine_ENOCOMM 4 |
#define | Engine_ENOSERVER 5 |
#define | Engine_ECOMALLOC 6 |
#define | Engine_ERUNTIME 7 |
#define | Engine_ECODECCREATE 8 |
#define | Engine_ECODECSTART 9 |
#define | Engine_EINVAL 10 |
#define | Engine_EBADSERVER 11 |
#define | Engine_ENOTAVAIL 12 |
#define | Engine_EWRONGSTATE 13 |
#define | Engine_EINUSE 14 |
#define | Engine_ENOTFOUND 15 |
#define | Engine_ETIMEOUT 16 |
#define | Engine_GETALGDESCFXN "GetEngineAlgDesc" |
Name of function that a dynamically loaded codec must supply. |
Typedefs | |
typedef struct Engine_Obj * | Engine_Handle |
Opaque handle to an engine. | |
typedef Int | Engine_Error |
Engine error code. | |
typedef struct Engine_Attrs | Engine_Attrs |
Attributes of an Engine. | |
typedef struct Engine_AlgInfo | Engine_AlgInfo |
Properties of an Engine algorithm. | |
typedef struct Engine_AlgInfo2 | Engine_AlgInfo2 |
Properties of an Engine algorithm. | |
typedef enum Engine_CachedMemType | Engine_CachedMemType |
Engine Cacheable Memory types. | |
typedef struct Engine_AlgDesc | Engine_AlgDesc |
Descriptor for an alg. This object can be passed to Engine_addAlg() , to dynamically add an alg to an engine. | |
typedef struct Engine_DllAlgDesc | Engine_DllAlgDesc |
Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type. | |
typedef Int(* | Engine_GetAlgDescFxn )(Engine_DllAlgDesc *dllAlgDesc) |
Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc structure. | |
typedef struct Engine_Desc | Engine_Desc |
This structure is passed to Engine_add() , and contains parameters to specify an engine. |
Enumerations | |
enum | Engine_CachedMemType { Engine_USECACHEDMEM_DEFAULT = -1, Engine_USECACHEDMEM_NONCACHED = 0, Engine_USECACHEDMEM_CACHED = 1 } |
Engine Cacheable Memory types. More... |
Functions | |
Void | CERuntime_exit (Void) |
Exit the Codec Engine Runtime. | |
Void | CERuntime_init (Void) |
Initialize the Codec Engine Runtime. | |
Engine_Error | Engine_addStubFxns (String fxnsName, IALG_Fxns *fxns) |
Register stub functions through which a remote algorithm can be called. | |
Engine_Error | Engine_add (Engine_Desc *pDesc) |
Add an Engine to the database of engines that can be opened with Engine_open() | |
Engine_Error | Engine_addAlg (String name, Engine_Handle engine, String location, Engine_AlgDesc *pAlgDesc) |
Dynamically add an algorithm to an Engine. | |
Engine_Error | Engine_removeAlg (String name, Engine_Handle engine, String algName) |
Dynamically remove an algorithm that was added to an Engine with Engine_addAlg(). | |
Void | Engine_close (Engine_Handle engine) |
Close an Engine. | |
Void | Engine_initAlgDesc (Engine_AlgDesc *pAlgDesc) |
Initialize an Engine_AlgDesc structure with default values. | |
Void | Engine_initAttrs (Engine_Attrs *pAttrs) |
Initialize an Engine_Attrs structure with default values. | |
Void | Engine_initDesc (Engine_Desc *pDesc) |
Initialize an Engine_Desc structure with default values. | |
Engine_Handle | Engine_open (String name, Engine_Attrs *attrs, Engine_Error *ec) |
Open an Engine. | |
Int | Engine_fwriteTrace (Engine_Handle engine, String prefix, FILE *out) |
Write Server's trace buffer to specifed file stream. | |
Engine_Error | Engine_getAlgInfo (String name, Engine_AlgInfo *algInfo, Int index) |
Get details of an algorithm configured into an engine. | |
Engine_Error | Engine_getAlgInfo2 (String name, Engine_Handle engine, Engine_AlgInfo2 *algInfo2, Int index) |
Get details of an algorithm. | |
Engine_Error | Engine_getDesc (String name, Engine_Desc *desc) |
Fill in an Engine_Desc structure with the values of the Engine descriptor for an Engine. | |
Engine_Error | Engine_getLastError (Engine_Handle engine) |
Get error code of the last failed operation. | |
String | Engine_getName (Engine_Handle engine) |
Get the name of an opened engine. | |
Engine_Error | Engine_getNumAlgs (String name, Int *numAlgs) |
Get the number of algorithms configured into an Engine. | |
Engine_Error | Engine_getNumAlgs2 (String name, Engine_Handle engine, Int *numAlgs) |
Get the number of algorithms statically configured into an engine or the total number of algorithms both statically configured and dynamically added through server information when the engine was opened. | |
Server_Handle | Engine_getServer (Engine_Handle engine) |
Get handle to an Engine's Server. | |
UInt32 | Engine_getUsedMem (Engine_Handle engine) |
Get Server's total memory usage. | |
Engine_Error | Engine_remove (String engineName) |
Remove an engine from the list of engines that can be opened. | |
Engine_Error | Engine_setDesc (String name, Engine_Desc *desc) |
Set values for an Engine's descriptor. This function should only be called when the Engine has not yet been opened. | |
Int | Engine_setTrace (Engine_Handle engine, String mask) |
Set Server's trace mask. |
Variables | |
Engine_Attrs | Engine_ATTRS |
Default engine attributes. |
#define CE_NULL_algs NULL |
#define CE_DECLARE_TYPE | ( | name, | |
types | |||
) |
Macros for runtime configuration. These macros can be used to create a static table of algorithms. However, the preferred method of building engine and alg tables, is to use the run-time APIs, Engine_add() and Engine_addAlg().
[in] | name | This is a symbol that will be associated with the types argument. It will be used to generate an internal variable name, so don't use the same name for two different calls to CE_DECLARE_TYPE() . name should be used in CE_LOCAL_ALG() to associate an alg to types . |
[in] | types | This is a ';' separated string of inheritance hierarchies. It is used to identify the codec class of an algorithm. For example, the declaration: CE_DECLARE_TYPE (mydecoder, "ti.sdo.ce.speech1.ISPHDEC1") indicates that mydecoder (a name that will be used in CE_LOCAL_ALG() to declare a speech decoder), inherits the ti.sdo.ce.speech1.ISPHDEC1 interface. |
Another example is the following: CE_DECLARE_TYPE(decoder, "ti.sdo.ce.video.IVIDDEC;ti.sdo.ce.test.xvideo.IVIDE") This says that the decoder inherits the ti.sdo.ce.test.xvideo.IVIDE interface, which in turn inherits the ti.sdo.ce.video.IVIDDEC interface.
#define CE_LOCAL_ALG | ( | name, | |
algName, | |||
ialgFxns, | |||
idma3Fxns, | |||
iresFxns, | |||
groupId, | |||
memType | |||
) |
Generates a structure containing data for a local algorithm.
[in] | name | This symbol is used to associate the algorithm with one of the types passed to CE_DECLARE_TYPE() . |
[in] | algName | This is the string name that the applicaion will use to create the algorithm, for example, "sphenc1_copy". |
[in] | ialgFxns | The address of the IALG_Fxns table for the algorithm. |
[in] | idma3Fxns | The address of the algorithm's IDMA3_Fxns table, if it has one, otherwise NULL. |
[in] | iresFxns | If the algorithm uses IRES, the address of its IRES_Fxns table, otherwise NULL. |
[in] | groupId | Scratch group Id of algorithm. |
[in] | memType | The type of memory (cached, non-cached, or whatever the default is), to allocate for the algorithm. Choose from the following values for memType: |
Engine_USECACHEDMEM_DEFAULT - default memory allocation Engine_USECACHEDMEM_NONCACHED - non-cached memory allocation Engine_USECACHEDMEM_CACHED - cached memory allocation
CE_BEGIN_ALG_TABLE()
and CE_END_ALG_TABLE()
macro calls.#define CE_LOCAL_ALG2 | ( | algName, | |
ialgFxns, | |||
idma3Fxns, | |||
iresFxns, | |||
groupId, | |||
memType, | |||
types | |||
) |
Generates a structure containing data for a local algorithm. This macro takes a 'types' string as an argument to avoid having to use the CE_DECLARE_TYPES() macro call.
[in] | algName | This is the string name that the applicaion will use to create the algorithm, for example, "sphenc1_copy". |
[in] | ialgFxns | The address of the IALG_Fxns table for the algorithm. |
[in] | idma3Fxns | The address of the algorithm's IDMA3_Fxns table, if it has one, otherwise NULL. |
[in] | iresFxns | If the algorithm uses IRES, the address of its IRES_Fxns table, otherwise NULL. |
[in] | groupId | Scratch group Id of algorithm. |
[in] | memType | The type of memory (cached, non-cached, or whatever the default is), to allocate for the algorithm. Choose from the following values for memType: |
Engine_USECACHEDMEM_DEFAULT - default memory allocation Engine_USECACHEDMEM_NONCACHED - non-cached memory allocation Engine_USECACHEDMEM_CACHED - cached memory allocation
[in] | types | The ';' separated string of inheritance hierarchies. This must be constant in order to initialize the structure. |
CE_BEGIN_ALG_TABLE()
and CE_END_ALG_TABLE()
macro calls.#define CE_DECLARE_LOCAL_ALG | ( | name, | |
algName, | |||
ialgFxns, | |||
idma3Fxns, | |||
iresFxns, | |||
groupId, | |||
memType, | |||
types | |||
) |
Generates a static variable of type Engine_AlgDesc. It is used in this manner:
[in] | name | The name to be given to the static Engine_AlgDesc variable. |
[in] | algName | This is the string name that the applicaion will use to create the algorithm, for example, "sphenc1_copy". |
[in] | ialgFxns | The address of the IALG_Fxns table for the algorithm. |
[in] | idma3Fxns | The address of the algorithm's IDMA3_Fxns table, if it has one, otherwise NULL. (DEPRECATED) |
[in] | iresFxns | If the algorithm uses IRES, the address of its IRES_Fxns table, otherwise NULL. |
[in] | groupId | Scratch group Id of algorithm. |
[in] | memType | The type of memory (cached, non-cached, or whatever the default is), to allocate for the algorithm. Choose from the following values for memType: |
Engine_USECACHEDMEM_DEFAULT - default memory allocation Engine_USECACHEDMEM_NONCACHED - non-cached memory allocation Engine_USECACHEDMEM_CACHED - cached memory allocation
[in] | types | The ';' separated string of inheritance hierarchies. This must be constant in order to initialize the structure. |
#define ALG_TABLE_NAME_LHS | ( | name | ) | CE_##name |
Use this macro and the CE_END_ALG_TABLE() macro around CE_LOCAL_ALG() to generate an algorithm table for an engine.
[in] | name | A symbol used to generate internal variable names. Use the same name in CE_END_ALG_TABLE(), and in the call to CE_ENGINE(), to associate an engine with this algorithm table. |
#define ALG_TABLE_RHS | ( | name | ) | name##_algs[] |
#define CE_BEGIN_ALG_TABLE | ( | name | ) | static Engine_AlgDesc ALG_TABLE_RHS(ALG_TABLE_LHS(name)) |
#define CE_END_ALG_TABLE | ( | name | ) |
Use this macro after CE_BEGIN_ALG_TABLE() and CE_LOCAL_ALG() for generating an algorithm table for an engine.
[in] | name | This must be the same symbol name passed to the previous CE_BEGIN_ALG_TABLE() call. |
#define CE_ENGINE | ( | algTab, | |
engName, | |||
serverName, | |||
memMap, | |||
useExtLoader, | |||
heapId | |||
) |
Generates a structure containing data for an engine.
[in] | algTab | Symbol to associate an alg table to this engine. Use the name passed to CE_BEGIN_ALG_TABLE() to associate that alg table with this engine. |
[in] | engName | The name of the engine to open |
[in] | serverName | The name of the Server image to load (if any). On SysLink-based systems, this is the name of a file and is passed unchanged to ProcMgr_Load(). |
[in] | memMap | The name of a memory map (if any). On SysLink-based systems, this file is used to map slave memory into the MMU using ProcMgr_map(). |
[in] | useExtLoader | Set to TRUE if an external loader will be used to load the server. If set to FALSE, Codec Engine will load the server when the Engine is opened. |
[in] | heapId | Optional heap id to be used for this Engine. This is used internally, for example, by Comm_alloc(). Use a value of 0 for heapId as the default. |
CE_BEGIN_ENGINE_TABLE()
and CE_END_ENGINE_TABLE()
macro calls.#define CE_BEGIN_ENGINE_TABLE | ( | name | ) |
Use this macro and the CE_END_ENGINE_TABLE() macro around CE_ENGINE() to generate an engine table for the application.
The usage is: CE_BEGIN_ENGINE_TABLE(name) CE_ENGINE(algTab_1, ...) CE_ENGINE(algTab_2, ...) ... CE_ENGINE(algTab_n, ...) CE_END_ENGINE_TABLE(name)
[in] | name | A symbol used to generate internal variable names. Use the same name in CE_END_ENGINE_TABLE(). |
#define CE_END_ENGINE_TABLE | ( | name | ) |
Use this macro and the CE_BEGIN_ENGINE_TABLE() macro around CE_ENGINE() to generate an engine table for the application.
The usage is: CE_BEGIN_ENGINE_TABLE(name) CE_ENGINE(algTab_1, ...) CE_ENGINE(algTab_2, ...) ... CE_ENGINE(algTab_n, ...) CE_END_ENGINE_TABLE(name)
[in] | name | A symbol used to generate internal variable names. Use the same name in CE_BEGIN_ENGINE_TABLE(). |
#define Engine_MODNAME "ti.sdo.ce.Engine" |
Name to pass to Diags_setMask() to enable logging for Engine functions.
#define Engine_EOK 0 |
Success.
#define Engine_EEXIST 1 |
Name does not exist.
#define Engine_ENOMEM 2 |
Unable to allocate memory.
#define Engine_EDSPLOAD 3 |
Unable to load the DSP.
#define Engine_ENOCOMM 4 |
Unable to create a comm connection to the DSP.
#define Engine_ENOSERVER 5 |
Unable to locate the server on the DSP.
#define Engine_ECOMALLOC 6 |
Unable to allocate communication buffer.
#define Engine_ERUNTIME 7 |
Internal engine runtime failure.
#define Engine_ECODECCREATE 8 |
Creation of the Codec failed.
#define Engine_ECODECSTART 9 |
Start of the Codec failed. For codecs which are implemented as a thread, this implies that the codec thread of execution failed to start.
#define Engine_EINVAL 10 |
Bad paramater passed to method.
#define Engine_EBADSERVER 11 |
Incompatible server specified.
#define Engine_ENOTAVAIL 12 |
Service not available.
#define Engine_EWRONGSTATE 13 |
Call can not be made at this time.
#define Engine_EINUSE 14 |
Call can't be made at this time because a required name/resource is in use.
#define Engine_ENOTFOUND 15 |
Entity was not found.
#define Engine_ETIMEOUT 16 |
Timeout-based operation timed out.
#define Engine_GETALGDESCFXN "GetEngineAlgDesc" |
Name of function that a dynamically loaded codec must supply.
typedef struct Engine_Obj* Engine_Handle |
Opaque handle to an engine.
typedef Int Engine_Error |
Engine error code.
typedef struct Engine_Attrs Engine_Attrs |
Attributes of an Engine.
typedef struct Engine_AlgInfo Engine_AlgInfo |
Properties of an Engine algorithm.
typedef struct Engine_AlgInfo2 Engine_AlgInfo2 |
Properties of an Engine algorithm.
typeTab
array of strings is replaced by a single string called types
. The string, types
, represents a ';' separated list of inheritance hierarchies of the algorithm, for example, "ti.sdo.ce.video.IVIDDEC;ti.sdo.ce.test.xvideo.IVIDE".typedef enum Engine_CachedMemType Engine_CachedMemType |
Engine Cacheable Memory types.
typedef struct Engine_AlgDesc Engine_AlgDesc |
Descriptor for an alg. This object can be passed to Engine_addAlg()
, to dynamically add an alg to an engine.
typedef struct Engine_DllAlgDesc Engine_DllAlgDesc |
Descriptor for a dynamically loaded alg. A dynamic library for a codec must export a function that fills in a structure of this type.
typedef Int(* Engine_GetAlgDescFxn)(Engine_DllAlgDesc *dllAlgDesc) |
Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc
structure.
Engine_addAlg()
to fill in the dynamic codec's descriptor.typedef struct Engine_Desc Engine_Desc |
This structure is passed to Engine_add()
, and contains parameters to specify an engine.
enum Engine_CachedMemType |
Engine Cacheable Memory types.
Void CERuntime_exit | ( | Void | ) |
Exit the Codec Engine Runtime.
Void CERuntime_init | ( | Void | ) |
Initialize the Codec Engine Runtime.
Engine_Error Engine_addStubFxns | ( | String | fxnsName, |
IALG_Fxns * | fxns | ||
) |
Register stub functions through which a remote algorithm can be called.
[in] | fxnsName | The name of the stub function table (e.g. "UNIVERSAL_STUBS") |
[in] | fxns | Address of stub function table (e.g. &UNIVERSAL_STUBS) |
fxns
argument can often be found in the class-specific VISA header file (e.g. UNIVERSAL_STUBS is declared in ti/sdo/ce/universal/universal.h).Engine_EOK | Success. |
Engine_ENOMEM | Memory allocation failed. |
Engine_Error Engine_add | ( | Engine_Desc * | pDesc | ) |
Add an Engine to the database of engines that can be opened with Engine_open()
[in] | pDesc | The handle of an Engine Descriptor object. Before setting the fields of pDesc, it must first be initialized with Engine_initDesc() . |
Engine_EINVAL | Bad parameter passed, such as pDesc = NULL, or pDesc->name = NULL. |
Engine_EINUSE | An engine with the name pDesc->name already exists. |
Engine_ENOMEM | A memory allocation failed. |
Engine_EOK | Success. |
pDesc->name
.Engine_Error Engine_addAlg | ( | String | name, |
Engine_Handle | engine, | ||
String | location, | ||
Engine_AlgDesc * | pAlgDesc | ||
) |
Dynamically add an algorithm to an Engine.
name
and engine
should be non-NULL.[in] | name | The name of the engine. name is specified in the engine configuration, or the name of an engine added with Engine_add() . This can only be non-NULL if the engine is not opened, otherwise, use an engine handle and set name to NULL. |
[in] | engine | The handle of an engine returned by Engine_open(). If engine is non-NULL, set name to NULL. |
[in] | location | String identifying the location of the algorithm. Often this is a file name, but for systems without a file system, it may be a system-specific string identifier. This may be NULL if the algorithm is built into the executable. |
[in] | pAlgDesc | Parameters describing the algorithm being added. Before setting the fields of this structure, it should first be initialized with Engine_initAlgDesc() , to set all fields to default values. If location is non-NULL (a dynamic library), then the following fields of pAlgDesc must be specified: pAlgDesc->name pAlgDesc->isLocal pAlgDesc->groupId All other Engine_AlgDesc fields will be from the dynamic library. If location is NULL (not a dynamic library), the user must set the following fields of pAlgDesc: pAlgDesc->name pAlgDesc->fxns pAlgDesc->idmaFxns, if applicable pAlgDesc->iresFxns, if applicable pAlgDesc->isLocal pAlgDesc->groupId pAlgDesc->types |
engine
is a valid (non-NULL) engine handle which is in the open state.name
, an error will be returned.Engine_EOK | Success. |
Engine_EINUSE | The Engine name is non-NULL, and the Engine is open. |
Engine_EINVAL | pAlgDesc or pAlgDesc->name is NULL. |
Engine_EINVAL | Both name and engine are NULL. Ensure one of these is non-NULL. |
Engine_EINVAL | Both name and engine are non-NULL. Ensure that one of these is NULL. |
Engine_EEXIST | There is no engine with the given name. |
Engine_EINUSE | The name of the alg in pAlgDesc->name is already in use. |
Engine_Error Engine_removeAlg | ( | String | name, |
Engine_Handle | engine, | ||
String | algName | ||
) |
Dynamically remove an algorithm that was added to an Engine with Engine_addAlg().
name
and engine
that were passed to Engine_addAlg() should be used here. In particular, if name
was used to add the alg, all handles to the engine must be closed before calling Engine_removeAlg().[in] | name | The name of the engine or NULL, that was passed to Engine_addAlg(). |
[in] | engine | The handle to an engine, previously acquired by a call to Engine_open(), or NULL, that was used in Engine_addAlg(). |
[in] | algName | Name of the algorithm to remove. |
Engine_EOK | Success. |
Engine_EEXIST | The engine name does not exist. |
Engine_ENOTFOUND | algName could not be found in engine . |
Engine_EINUSE | The Engine name is still open. |
Void Engine_close | ( | Engine_Handle | engine | ) |
Close an Engine.
[in] | engine | The handle to an engine, previously acquired by a call to Engine_open(). |
engine
must not be referenced by any algorithm instance objects; i.e., you must first delete all algorithm instances associated with engine
before closing it.engine
is a valid (non-NULL) engine handle which is in the open state.Void Engine_initAlgDesc | ( | Engine_AlgDesc * | pAlgDesc | ) |
Initialize an Engine_AlgDesc structure with default values.
[in] | pAlgDesc | Location of Engine_AlgDesc object to initialize. The fields of pAlgDesc will be set to the following: |
pAlgDesc->name = NULL; pAlgDesc->uuid.data = 0; pAlgDesc->fxns = NULL; pAlgDesc->idmaFxns = NULL; pAlgDesc->typeTab = NULL; pAlgDesc->isLocal = TRUE; pAlgDesc->groupId = 0; pAlgDesc->rpcProtocolVersion = 0; pAlgDesc->iresFxns = NULL; pAlgDesc->codecClassConfig = NULL; pAlgDesc->memType = Engine_USECACHEDMEM_DEFAULT; pAlgDesc->types = NULL;
Void Engine_initAttrs | ( | Engine_Attrs * | pAttrs | ) |
Initialize an Engine_Attrs structure with default values.
[in] | pAttrs | Location of Engine_Attrs object to initialize. |
Void Engine_initDesc | ( | Engine_Desc * | pDesc | ) |
Initialize an Engine_Desc structure with default values.
[in] | pDesc | Location of Engine_Desc object to initialize. The fields of pDesc will be set to the following: |
pDesc->name = NULL; pDesc->remoteName = NULL; pDesc->heapId = 0;
Engine_Handle Engine_open | ( | String | name, |
Engine_Attrs * | attrs, | ||
Engine_Error * | ec | ||
) |
Open an Engine.
The handle returned may be used to create one or more instances of an algorithm contained in the specified Engine.
An Engine may be opened more than once; each open returns a unique handle that can be used to create algorithm instances or get status of the Engine.
Engine handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via Engine_open()) or explicitly serialize access to a shared handle.
[in] | name | The name of the engine to open. name is specified in the engine configuration. |
[in] | attrs | Attributes for the open engine. |
[out] | ec | Optional output error code |
NULL | An error has occurred. |
non-NULL | The handle to the opened engine. |
name
is a non-NULL string.name
is a valid, pre-configured name of an engine.ec
is non-NULL, *ec
is set to a non-zero value indicating the cause of the failure.ec
is non-NULL, the Engine_Error value is set to one of the following values:Int Engine_fwriteTrace | ( | Engine_Handle | engine, |
String | prefix, | ||
FILE * | out | ||
) |
Write Server's trace buffer to specifed file stream.
[in] | engine | The handle to the opened engine. |
[in] | prefix | A string to prepend to each line output; this allows one to easily identify trace from the server from the application's trace, for example. |
[in] | out | A open FILE stream used to output the Server's trace characters. |
Integer | number of characters copied to the specified FILE stream. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state.Engine_Error Engine_getAlgInfo | ( | String | name, |
Engine_AlgInfo * | algInfo, | ||
Int | index | ||
) |
Get details of an algorithm configured into an engine.
[in] | name | The name of the engine. name is specified in the engine configuration. |
[out] | algInfo | Structure to store algorithm details. The algInfoSize field of this structure must be set to sizeof(Engine_AlgInfo) by the application. |
[out] | index | The index of the algorithm to get the information. |
Engine_EOK | Success. |
Engine_EEXIST | There is no engine with the given name. |
Engine_ENOTFOUND | index is greater than or equal to the total number of algorithms configured for the engine, or index < 0. |
Engine_EINVAL | The value of algInfoSize passed to this function does not match the CE library's sizeof(Engine_AlgInfo) . |
name
is a non-NULL string.algInfo
is non-NULL.name
is a valid engine name and 0 <= index
< the total number of algorithms configured for the engine, then algInfo
will contain the information for the engine's ith (i = index
) algorithm.Engine_Error Engine_getAlgInfo2 | ( | String | name, |
Engine_Handle | engine, | ||
Engine_AlgInfo2 * | algInfo2, | ||
Int | index | ||
) |
Get details of an algorithm.
[in] | name | The name of the engine. name is specified in the engine configuration. This may be NULL if engine contains a valid engine handle. |
[in] | engine | The handle of an engine returned by Engine_open(). If this is NULL, only information for a static alg can be obtained. |
[out] | algInfo2 | Structure to store algorithm details. The algInfoSize field of this structure must be set to sizeof(Engine_AlgInfo2) by the application. |
[out] | index | The index of the algorithm to get the information. |
Engine_EOK | Success. |
Engine_EEXIST | There is no engine with the given name. |
Engine_ENOTFOUND | index is greater than or equal to the total number of algorithms configured for the engine, or index < 0. |
Engine_EINVAL | The value of algInfoSize passed to this function does not match the CE library's sizeof(Engine_AlgInfo2) . |
name
is a non-NULL string or engine
is non-NULL.algInfo2
is non-NULL.name
is a valid engine name and 0 <= index
< the total number of algorithms configured for the engine, then algInfo2
will contain the information for the engine's ith (i = index
) algorithm.Engine_Error Engine_getDesc | ( | String | name, |
Engine_Desc * | desc | ||
) |
Fill in an Engine_Desc structure with the values of the Engine descriptor for an Engine.
[in] | name | The name of the Engine. name is specified in the engine configuration or a a name that was passed to Engine_add() . |
[out] | desc | The structure where the descriptor of the Engine specified by name will be copied to. |
Engine_EOK | Success. |
Engine_EEXIST | There is no engine with the given name. |
name
is a non-NULL string.desc
is non-NULL.name
is a valid engine name, then desc will contain the descriptor of the engine name
.Engine_Error Engine_getLastError | ( | Engine_Handle | engine | ) |
Get error code of the last failed operation.
[in] | engine | The handle to the opened engine. |
error | code (Engine_Error) of the last failed engine operation. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state. String Engine_getName | ( | Engine_Handle | engine | ) |
Get the name of an opened engine.
[in] | engine | The handle to the opened engine. |
NULL | An error has occurred. |
non-NULL | The name of the opened engine. |
Engine_Error Engine_getNumAlgs | ( | String | name, |
Int * | numAlgs | ||
) |
Get the number of algorithms configured into an Engine.
[in] | name | The name of the Engine. name is specified in the engine configuration. |
[out] | numAlgs | The number of algorithms that are configured in the given engine. |
Engine_EOK | Success. |
Engine_EEXIST | There is no engine with the given name. |
name
is a non-NULL string.numAlgs
is non-NULL.name
is a valid engine name, then numAlgs will contain the number of algorithms configured for the given engine.Engine_Error Engine_getNumAlgs2 | ( | String | name, |
Engine_Handle | engine, | ||
Int * | numAlgs | ||
) |
Get the number of algorithms statically configured into an engine or the total number of algorithms both statically configured and dynamically added through server information when the engine was opened.
[in] | name | The name of the engine. name is specified in the engine configuration. name can be NULL, if engine is a valid Engine_Handle. |
[in] | engine | The handle of an engine returned by Engine_open(). If engine is NULL, name must be non-NULL, and only the number of statically configured algorithms will be returned in numAlgs . specified in the engine configuration. |
[out] | numAlgs | The number of algorithms that are configured in the given engine. |
Engine_EOK | Success. |
Engine_EEXIST | There is no engine with the given name. |
name
is a non-NULL string or engine
is non-NULL.numAlgs
is non-NULL.name
is a valid engine name, then numAlgs will contain the number of algorithms configured for the given engine.Server_Handle Engine_getServer | ( | Engine_Handle | engine | ) |
Get handle to an Engine's Server.
This function returns the handle to an Engines server, that can be used with Server APIs to obtain information from and control the remote DSP server.
[in] | engine | The handle to the opened engine. |
Handle | to engine's server. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state. UInt32 Engine_getUsedMem | ( | Engine_Handle | engine | ) |
Get Server's total memory usage.
[in] | engine | The handle to the opened engine. |
Total | amount of used memory (in MAUs). If the amount is not available, 0 is returned and the reason can be retrieved via Engine_getLastError(). |
engine
is a valid (non-NULL) engine handle and the engine is in the open state.Engine_Error Engine_remove | ( | String | engineName | ) |
Remove an engine from the list of engines that can be opened.
[in] | engineName | The name of the engine to be removed. |
engineName
is non-NULL.Engine_EINUSE | The engine cannot be removed because an instance of it is still opened. |
Engine_EEXIST | No engine by this name exists. |
Engine_EOK | Success. |
Engine_Error Engine_setDesc | ( | String | name, |
Engine_Desc * | desc | ||
) |
Set values for an Engine's descriptor. This function should only be called when the Engine has not yet been opened.
[in] | name | The name of the Engine. name is specified in the engine configuration or a a name that was passed to Engine_add() . |
[in] | desc | The structure where descriptor values for the Engine specified by name will be copied from. |
Engine_EOK | Success. |
Engine_EEXIST | There is no engine with the given name. |
Engine_EINUSE | The Engine name has already been opened. |
name
is a non-NULL string.desc
is non-NULL.name
is a valid engine name, then the desscriptor for the engine name
will have been updated with values from desc
.Engine_getDesc()
to fill in the descriptor, override the fields you want to change, and then pass the descriptor to Engine_setDesc(). Only the following fields of the Engine_Desc are allowed to be modified: memMap
useExtLoader
heapId
Int Engine_setTrace | ( | Engine_Handle | engine, |
String | mask | ||
) |
Set Server's trace mask.
[in] | engine | The handle to the opened engine. |
[in] | mask | Trace mask, e.g. "*=01234567" |
Engine_ENOSERVER | No server for this engine. |
Engine_EINUSE | Trace resource is already in use. |
Engine_ERUNTIME | Internal runtime error has occurred. |
engine
is a valid (non-NULL) engine handle and the engine is in the open state.Engine_Attrs Engine_ATTRS |
Default engine attributes.