![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines the input arguments for all ISPHENC1 instance process function. More...
#include <isphenc1.h>
Data Fields | |
XDAS_Int16 | size |
XDAS_Int16 | nullTrafficChannel |
XDM1_SingleBufDesc | data |
Defines the input arguments for all ISPHENC1 instance process function.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int16 ISPHENC1_InArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int16 ISPHENC1_InArgs::nullTrafficChannel |
Enable/disable the null traffic channel.
XDM1_SingleBufDesc ISPHENC1_InArgs::data |
Raw data input for data transmission.