![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Enumerations | |
enum | ISPEECH1_NullTrafficMode { ISPEECH1_NULLTRAFFICMODE_OFF = 0, ISPEECH1_NULLTRAFFICMODE_ON = 1, ISPEECH1_NULLTRAFFICMODE_DEFAULT = ISPEECH1_NULLTRAFFICMODE_OFF } |
Null traffic channel setting. More... | |
enum | ISPEECH1_PostFilter { ISPEECH1_POSTFILTER_OFF = 0, ISPEECH1_POSTFILTER_ON = 1, ISPEECH1_POSTFILTER_DEFAULT = ISPEECH1_POSTFILTER_ON } |
Post filter setting. More... | |
enum | ISPEECH1_VADFlag { ISPEECH1_VADFLAG_OFF = 0, ISPEECH1_VADFLAG_ON = 1, ISPEECH1_VADFLAG_DEFAULT = ISPEECH1_VADFLAG_ON } |
Voice Activity Detection (VAD) setting. More... |
This is the XDM speech interface shared between the various codecs.
Null traffic channel setting.
enum ISPEECH1_PostFilter |
enum ISPEECH1_VADFlag |