![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Macros | |
#define | VISA_EOK 0 |
Success. | |
#define | VISA_ERUNTIME -1 |
Internal runtime error. | |
#define | VISA_EFAIL -2 |
General system error. | |
#define | VISA_EUNSUPPORTED -3 |
The API is not suported for the given system configuration. | |
#define | VISA_ETIMEOUT -100 |
Timeout occurred. | |
#define | VISA_FOREVER Engine_FOREVER |
Special value for timeout parameter indicating never timeout. |
Typedefs | |
typedef Int | VISA_Status |
VISA result data type. |
Functions | |
VISA_Status | VISA_getAlgMemRecs (VISA_Handle visa, IALG_MemRec *memTab, Int size, Int *numRecs) |
Get the IALG_MemRec memory assigned to an algorithm instance. | |
VISA_Status | VISA_getAlgNumRecs (VISA_Handle visa, Int *numRecs) |
Get the number of IALG_MemRecs assigned to an algorithm. | |
Ptr | VISA_getCodecClassConfig (VISA_Handle visa) |
Get codec-specific values for the VISA class-specific (or codec-specific if the codec doesn't extend VISA) stub-and/ or-skeleton configuration data (that some classes have) | |
UInt | VISA_getMaxMsgSize (VISA_Handle visa) |
Returns max size of messages allocated by VISA_allocMsg() | |
Void | _VISA_init (Void) |
Ininitilize VISA module. | |
Void | _VISA_exit (Void) |
Exit VISA module. | |
Bool | VISA_isLocal (VISA_Handle visa) |
Indicates whether VISA codecs run on a remote or local CPU. |
Codec Engine Algorithm-independent shared definitions and services.
#define VISA_EOK 0 |
Success.
#define VISA_ERUNTIME -1 |
Internal runtime error.
#define VISA_EFAIL -2 |
General system error.
#define VISA_EUNSUPPORTED -3 |
The API is not suported for the given system configuration.
#define VISA_ETIMEOUT -100 |
Timeout occurred.
#define VISA_FOREVER Engine_FOREVER |
Special value for timeout parameter indicating never timeout.
typedef Int VISA_Status |
VISA result data type.
VISA_Status VISA_getAlgMemRecs | ( | VISA_Handle | visa, |
IALG_MemRec * | memTab, | ||
Int | size, | ||
Int * | numRecs | ||
) |
Get the IALG_MemRec memory assigned to an algorithm instance.
[in] | visa | Handle to an algorithm instance. |
[out] | memTab | Location to store the IALG_MemRecs. |
[in] | size | Maximum number of IALG_MemRecs to put in memTab array. |
[out] | numRecs | Actual number of IALG_MemRecs copied into memTab array. |
visa
handle.VISA_EOK | Success. |
VISA_EFAIL | Failure. |
VISA_Status VISA_getAlgNumRecs | ( | VISA_Handle | visa, |
Int * | numRecs | ||
) |
Get the number of IALG_MemRecs assigned to an algorithm.
[in] | visa | Handle to an algorithm instance. |
[out] | numRecs | Location to store the number of IALG_MemRecs used. |
visa
handle.VISA_EOK | Success. |
VISA_EFAIL | Failure. |
Ptr VISA_getCodecClassConfig | ( | VISA_Handle | visa | ) |
Get codec-specific values for the VISA class-specific (or codec-specific if the codec doesn't extend VISA) stub-and/ or-skeleton configuration data (that some classes have)
[in] | visa | Handle to an algorithm instance. |
address | of the codec class config data structure, or NULL if codec class config data not defined for the codec; the format of the structure is class-specific, and the data in it is codec- specific |
visa
must be a valid algorithm instance handle. UInt VISA_getMaxMsgSize | ( | VISA_Handle | visa | ) |
Returns max size of messages allocated by VISA_allocMsg()
maxMsgSize | Max size of messages allocated by VISA_allocMsg() |
Void _VISA_init | ( | Void | ) |
Ininitilize VISA module.
Void _VISA_exit | ( | Void | ) |
Bool VISA_isLocal | ( | VISA_Handle | visa | ) |
Indicates whether VISA codecs run on a remote or local CPU.
FALSE | VISA codecs run on remote CPU |
TRUE | VISA codecs run on local CPU |