Codec Engine Application Programming Interface (API)  ce-w08
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Data Structures | Typedefs | Functions
VISA - CE Stub SPIs

Data Structures

struct  VISA_MsgHeader
 VISA message header. More...

Typedefs

typedef struct VISA_MsgHeader VISA_MsgHeader
 VISA message header.

Functions

VISA_Msg VISA_allocMsg (VISA_Handle visa)
 Obtain an algorithm instance's message.
VISA_Status VISA_call (VISA_Handle visa, VISA_Msg *msg)
 Invoke the operation specified in the message and wait for it to complete.
VISA_Status VISA_callAsync (VISA_Handle visa, VISA_Msg *msg)
 Invoke the operation specified in the message and return without waiting for it to complete.
VISA_Status VISA_wait (VISA_Handle visa, VISA_Msg *msg, UInt timeout)
 Wait for the oldest operation from a command specified with VISA_callAsync() to complete.
Void VISA_freeMsg (VISA_Handle visa, VISA_Msg msg)
 Release an algorithm instance's message.
Void VISA_getContext (VISA_Handle visa, UInt32 *pContext)
 Get optional context parameter.
Void VISA_setContext (VISA_Handle visa, UInt32 context)
 Set optional context parameter.

Detailed Description

Codec Engine System Programming Interface (SPI) for stub implementors.


Typedef Documentation

VISA message header.

Remarks:
This must be the first field in a message

Function Documentation

VISA_Msg VISA_allocMsg ( VISA_Handle  visa)

Obtain an algorithm instance's message.

Parameters:
[in]visaHandle to an algorithm instance.
Return values:
NULLGeneral system error
non-NULLThe remote algorithm's message.
Remarks:
This is typically called by an algorithm class' stub.
See also:
VISA_allocMsg()
VISA_Status VISA_call ( VISA_Handle  visa,
VISA_Msg msg 
)

Invoke the operation specified in the message and wait for it to complete.

Parameters:
[in]visaHandle to an algorithm instance.
[out]msgThe remote algorithm's message, to be sent to the skeleton.
Remarks:
This is typically called by an algorithm class' stub.
Return values:
VISA_EOKSuccess
VISA_ERUNTIMEGeneral system error
See also:
VISA_callAsync()
VISA_Status VISA_callAsync ( VISA_Handle  visa,
VISA_Msg msg 
)

Invoke the operation specified in the message and return without waiting for it to complete.

Parameters:
[in]visaHandle to an algorithm instance.
[out]msgThe remote algorithm's message, to be sent to the skeleton.
Remarks:
This is typically called by an algorithm class' stub.
Return values:
VISA_EOKSuccess
VISA_ERUNTIMEGeneral system error
See also:
VISA_wait()
VISA_call()
VISA_Status VISA_wait ( VISA_Handle  visa,
VISA_Msg msg,
UInt  timeout 
)

Wait for the oldest operation from a command specified with VISA_callAsync() to complete.

Parameters:
[in]visaHandle to an algorithm instance.
[out]msgPlaceholder for the remote algorithm's return message, retrieved from the skeleton.
[in]timeoutAmount of "time" to wait ("time" depends on underlying mechanism, such as that used with MSGQ_Get()).
Remarks:
This is typically called by an algorithm class' stub.
Return values:
VISA_EOKSuccess
VISA_ERUNTIMEGeneral system error
VISA_ETIMEOUTOperation timed out
See also:
VISA_callAsync()
Void VISA_freeMsg ( VISA_Handle  visa,
VISA_Msg  msg 
)

Release an algorithm instance's message.

Parameters:
[in]visaHandle to an algorithm instance.
[in]msgMessage to free, obtained through a call to VISA_allocMsg().
Return values:
NULLGeneral system error
non-NULLThe remote algorithm's message.
Remarks:
This is typically called by an algorithm class' stub.
See also:
VISA_allocMsg()
Void VISA_getContext ( VISA_Handle  visa,
UInt32 *  pContext 
)

Get optional context parameter.

Parameters:
[in]visaHandle to an algorithm instance.
[out]pContextLocation to store context.
Precondition:
visa must be a valid algorithm instance handle.
pContext must be a valid pointer.
Remarks:
The VISA_setContext() / VISA_getContext() pair does not work across processors. That is, the context can only be stored and retrieved on the local processor.
See also:
VISA_setContext()
Void VISA_setContext ( VISA_Handle  visa,
UInt32  context 
)

Set optional context parameter.

Parameters:
[in]visaHandle to an algorithm instance.
[in]contextContext.
Precondition:
visa must be a valid algorithm instance handle.
Remarks:
The VISA_setContext() / VISA_getContext() pair does not work across processors. That is, the context can only be stored and retrieved on the local processor.
See also:
VISA_getContext()
Copyright 2013, Texas Instruments Incorporated