7.9.8.107. OnHalt

GEL callback function called after a halt operation is performed on the current target

Syntax

OnHalt();

Parameters

None

Description

If defined in a loaded GEL file, OnHalt() is called after the target is halted.

Example

OnHalt() {GEL_TextOut("OnHalt called …n")}