7.9.8.68. GEL_Restart()ΒΆ

Resets the PC to the program entry point.

Syntax

GEL_Restart();

Parameters

None.

Description

 The GEL_Restart() function resets the program to its entry point. This assumes that a program (with symbol information) has been loaded into the target and the target program is able to be restarted. If the target program relies on the loader to initialize various RAM locations, the program may not function correctly after being restarted.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_Reset();

Related Topics

GEL_Reset

GEL_Run

GEL_Halt