7.9.8.49. GEL_MemoryLoadData()ΒΆ

Loads a block of memory from a file.

Syntax

GEL_MemoryLoadData(startAddress, page, length, "fileName" )

Parameters

startAddress is the first address in the block.

page identifies the type of memory to fill: 0 (Program memory), 1 (Data memory) or 2 (I/O space)

For processors that do not have more than one type of memory, use 0 for this Parameters. For simulated targets, the I/O space Parameters is not supported.

length defines the number of values to load from the file

fileName name of the file to load data from. The fileName must be enclosed in quotation marks.

Description

GEL_MemoryLoadData() is an extention to GEL_MemoryLoad() and supports loading data in addtional formats to target memory from a specified file.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_MemoryLoadData( 0x100, 0 , 0x100, "c:\mydir\myfile.dat" );

Related Topics

GEL_MemorySaveData

GEL_MemoryListSupportedTypes

GEL_MemorySave

GEL_MemoryLoad