7.9.8.62. GEL_ReConnectΒΆ

GEL built-in function that can be called on a connected target to re-send the connection sequence to it.

Syntax

GEL_ReConnect()

Parameters

None

Description

The function effectively disconnects and connects the target and then returns. Unlike calling GEL_Disconnect() followed by GEL_Connect(), it will not generate any GEL callbacks nor trigger a UI update. This function exists only for specific devices that require the jtag/swd connection sequence to be re-sent in specific scenarios, such as when communicating with a bootloader.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Related Topics

GEL_Connect

GEL_Disconnect

GEL_IsConnected