7.9.8.81. GEL_StepOverΒΆ

Executes a function or the next statement.

Format

GEL_StepOver();

Parameters

None

Description

The debugger executes the function and then halts after the function returns. If a breakpoint is encountered within the function, execution halts at the breakpoint.

The Step Over command can also be used to execute statements that are not function calls. In this case, the debugger executes the next statement then halts.

If you are in C source mode, this command steps over an entire C instruction; otherwise, it steps over a single assembly instruction. However, to protect the processor's pipeline, several instructions following a delayed branch or call may be considered part of the same statement. In this case, the Step Over command may execute more than one instruction at a time.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_StepOver();

Related Topics

GEL_ClearProfileConfiguration

GEL_StepInto

GEL_StepOut

GEL_SyncHalt

GEL_SyncStepInto

GEL_SyncStepOut

GEL_SyncStepOver