7.9.8.94. OnChildRunning()ΒΆ
GEL callback function called on the parent processor when one of its child is running.
Syntax
OnChildRunning();
Parameters
Description
If defined in a loaded GEL file on the parent processor, OnChildRunning() is called when one of its child is running.