7.9.8.92. GEL_UnloadGEL()ΒΆ

Unloads a GEL file.

Syntax

GEL_UnloadGel("fileName");

Parameters

fileNamenames the GEL file to be unloaded. The fileName must be enclosed in quotation marks.

Description

This function unloads the functions defined in the specified GEL file.

The fileName Parameters is case sensitive. The filename must be specified exactly as it was when the file was loaded. If the file is not in the current directory, the fileName Parameters must provide the full path. A double backslash escape sequence is required to ensure that you get a backslash into the fileName Parameters.

Note: When a file is opened using menu commands, Windows capitalizes the drive letter.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_UnloadGel("C:\MyDir\myfile.gel");

Related Topics

GEL_LoadGel

GEL_UnloadAllGels