7.9.8.84. GEL_SyncStepOutΒΆ
Performs a StepOut operation on every target that is in the same group as the current target.
Format
GEL_SyncStepOut([iterations]);
Parameters
iterations(optional) specifies the number of times the command is to be repeated. If iterations is not specified, executes a single StepOut is performed.
Description
Performs a StepOut operation on every target that is in the same group as the current target. The operation performed is the same as the "StepOut" option selected from the PDM debug menu.
As with the other synchronous operations, the operation is performed on all targets simultaneously.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_SyncStepOut (3);
GEL_SyncStepOut ( );
Related Topics