7.9.8.67. GEL_SetTimerΒΆ

Scheduals a gel command to run periodically.

Format

GEL_SetTimer(milliseconds, timer_id, "callback");

Parameters

millisecondsspecifies the amount of time in milliseconds that should elapse between callbacks.

timer_idspecifies a number to uniquely identify this timer.

callbackis a string representing the GEL expression to evaluate every time the timer fires.

Description

Sets a timer that repeatedly fires every milliseconds. Every time the timer fires, the GEL expression defined in callback is executed. The timer keeps firing until GEL_CancelTimer is called. If a timer is already set with the specified id, no action is taken.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_SetTimer(2000, 1, "*0x8010 = 0");

GEL_SetTimer(5000, 2, "MyCallback()");

Related Topics

GEL_CancelTimer