7.9.8.14. GEL_DisconnectΒΆ

GEL built-in function that can be called on a connected target to disconnect it.

Syntax

GEL_Disconnect()

Parameters

None

Description

The function disconnects the target and then returns. It throws an exception if the target is already disconnected or cannot be disconnected.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Related Topics

GEL_Connect

GEL_IsConnected