|
MAVRK Embedded Software 0.91
Software Libraries for the MAVRK motherboard and related components
|
| ADS123x.h [code] | |
| ADS123x_PC_Interface.h [code] | |
| ADS123x_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for ADS123x devices |
| ADS123x_PC_Interface_Functions.c | Performs PC Interface functions between an ADS1x3x and the PC Interface |
| ADS123x_SPI_Functions.c | Performs SPI Communication for ADS1x3x Devices |
| ADS1248_constants.c | |
| ADS1259.h [code] | |
| ADS1259_Device_Interface.h [code] | |
| ADS1259_Device_Status.c | |
| ADS1259_Functions.c | |
| ADS1259_PC_Interface.h [code] | |
| ADS1259_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for ADS1x48 devices |
| ADS1259_PC_Interface_Functions.c | Performs PC Interface functions between an ADS1x48 and the PC Interface |
| ADS1259_SPI_Functions.c | |
| ADS1x3x_Device_Interface.h [code] | |
| ADS1x48_PC_Interface.h [code] | |
| ADS1x48_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for ADS1x48 devices |
| ADS1x48_PC_Interface_Functions.c | Performs PC Interface functions between an ADS1x48 and the PC Interface |
| ADS1x4x.h [code] | |
| ADS1x4x_Device_Interface.h [code] | |
| ADS1x4x_Device_Status.c | Functions that gather the status for ADS1x48 devices |
| ADS1x4x_Functions.c | Functions that setup the ADS1x4x device for operations |
| ADS1x4x_SPI_Functions.c | Performs SPI Communication for ADS1x4x Devices |
| ADS1x9x.h [code] | |
| ADS1x9x_Constant_Tables.c | Predefined constant tables for ASD1298 DAC |
| ADS1x9x_Device_Interface.h [code] | |
| ADS1x9x_Device_Status.c | Functions that gather the status for ADS1x9x devices |
| ADS1x9x_Functions.c | Functions that setup the ADS1x9x device for operations |
| ADS1x9x_PC_Interface.h [code] | |
| ADS1x9x_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for ADS1x9x devices |
| ADS1x9x_PC_Interface_Functions.c | Performs PC Interface functions between an ADS1x9x and the PC Interface |
| ADS1x9x_SPI_Functions.c | Performs SPI Communication for ADS1x9x Devices |
| ADS78xx_ADS83xx.h [code] | |
| ADS78xx_ADS83xx_PC_Interface.h [code] | |
| ADS78xx_ADS83xx_PC_Interface_Functions.c | Performs PC Interface functions between an ADS83xx and the PC Interface |
| ADS7924.h [code] | |
| ADS7924_Functions.c | Functions that setup the ADS7924 device for operations |
| ADS7924_I2C_Functions.c | Performs I2C Communication for ADS7924 Devices |
| ADS7924_PC_Interface.h [code] | |
| ADS7924_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for ADS7924 devices |
| ADS7924_PC_Interface_Functions.c | Performs PC Interface functions between an ADS7924 and the PC Interface |
| Board_to_Board_Passthrough.h [code] | |
| Board_to_Board_Passthrough_Functions.c | Functions that setup and control the I/O and flags for Board to Board communication on the MAVRK system |
| BootLoader_Interface.h [code] | |
| BootLoader_Interface_Functions.c | Performs generic Interface functions between the standard MAVRK device and the Boot Loader Software |
| BQ24765_MultiCell_Battery_Charger.c | Performs |
| BQ24765_MultiCell_Battery_Charger.h [code] | |
| BQ24765_PC_Interface.h [code] | |
| BQ24765_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK component to the PC Application for BQ24765 Multi-Cell Battery Charger |
| BQ24765_PC_Interface_Functions.c | Performs PC Interface functions between the PMU-BAT-MVK or PMU-CARRIER-MVK modules and the PC Interface |
| BQ25504_PC_Interface.h [code] | |
| BQ25504_PC_Interface_Functions.c | Performs PC Interface functions for the BQ25504 module |
| BQ27410_Fuel_Gauge.c | Performs read and write I2C commands to BQ27410 Fuel Gauge device |
| BQ27410_Fuel_Gauge.h [code] | |
| BQ27410_Fuel_Gauge_Data_Flash.c | Performs read and write I2C commands to BQ27410 Data Flash |
| BQ27410_PC_Interface.h [code] | |
| BQ27410_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK component to the PC Application for BQ27410 Battery Fuel Gauge |
| BQ27410_PC_Interface_Functions.c | Performs PC Interface functions between the BQ27410 modules and the PC Interface |
| CC1100_constants.c | |
| CC1100_unmodulated_carrier.c | Structure of register settings to set up system registers of the cc1100 |
| CC1101_constants.c | |
| CC1120_constants.c | |
| cc2500_constants.c | |
| CC2500_unmodulated_carrier.c | |
| cc2550_constants.c | |
| CC430F5137_constants.c | |
| CC_Channel_Functions.c | |
| CC_Device_Processor_Interface.h [code] | |
| CC_Device_Status.c | Read the status of registers on the Chipcon Radio |
| CC_Device_unmodulated_carrier.c | Structure of register settings to set up system registers of the cc2500 and cc1100 |
| CC_FIFO_Functions.c | Functions that interact with the FIFOs on the TI Chipcon Radio |
| CC_Modem_Functions.c | Functions that interact with CC based modems in the RF Slot |
| CC_Primary_Settings.c | Functions that discover and initialize the TI Chipcon Radio |
| cc_radio.h [code] | |
| CC_Radio_API.c | High Level Functions related to transmitting and receiving using the TI Chipcon Radios |
| CC_Radio_Functions.c | Functions related to controlling radio TX/RX functions of the TI Chipcon Radios |
| CC_Radio_PC_Interface.h [code] | |
| CC_Radio_PC_Interface_Command_Decode.c | Setup the interface between the Chipcon Radio part and the PC Application |
| CC_Radio_PC_Interface_Functions.c | Performs PC Interface functions between an Chipcon Radio and the PC Interface |
| CC_SPI_Functions.c | Functions that Control the SPI Interface on the Chipcon Radio |
| CDCE913.h [code] | |
| CDCE913_Constant_Tables.c | Some predefined constant tables for CDCE913 Programmable 1-PLL VCXO Clock Synthesizer |
| CDCE913_Device_Interface.h [code] | |
| CDCE913_Functions.c | Functions that allow changes in the CDCE913 Programmable 1-PLL VCXO Clock Synthesizer configuration |
| CDCE913_PC_Interface.h [code] | |
| CDCE913_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for ADS1x48 devices |
| CDCE913_PC_Interface_Functions.c | |
| crc.h [code] | |
| crc_algs.c | Functions that perform the equivalent CRC16 and CRC32 to the hardware components |
| DAC7563_DAC8563_DAC8163.h [code] | |
| diskio.h [code] | |
| doxygen_mainpage.h [code] | |
| DRV8814_DRV8825_MCU_Interface.h [code] | |
| DRV8814_DRV8825_Motor_Drive.h [code] | |
| DRV8814_MCU_Interface_Functions.c | Performs MCU Interface style of functions between a DRV8814 Motor Driver and the MCU Slot |
| DRV8814_Motor_Drive.c | Functions that setup and control the I/O (GPIOs and LEDs) for the DRV8814 with an MSP430F2234 |
| DRV8814_Motor_Drive.h [code] | |
| DRV8814_Motor_Drive_API.c | |
| DRV8814_PC_Interface.h [code] | |
| DRV8814_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for DRV8814 motor drive |
| DRV8814_PC_Interface_Functions.c | Performs PC Interface functions between a DRV8814 Motor Driver and the PC Interface |
| DRV8825_MCU_Interface_Functions.c | Performs MCU Interface style of functions between a DRV8825 Motor Driver and the MCU Slot |
| DRV8825_Motor_Drive.c | Functions that setup and control the I/O (GPIOs and LEDs) for the DRV8825 with an MSP430F2234 |
| DRV8825_Motor_Drive.h [code] | |
| DRV8825_Motor_Drive_API.c | |
| DRV8825_PC_Interface.h [code] | |
| DRV8825_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for DRV8814 motor drive |
| DRV8825_PC_Interface_Functions.c | Performs PC Interface functions between a DRV8825 Motor Driver and the PC Interface |
| DRV8830_I2C_Functions.c | Performs low level I2C communications with the DRV8830 Low Voltage Motor Driver |
| DRV8830_Motor_Drive.c | Functions that setup and control the DRV8830 |
| DRV8830_Motor_Drive.h [code] | |
| DRV8830_Motor_Drive_API.c | Functions that setup and allow the use of the DRV8830 |
| DRV8830_PC_Interface.h [code] | |
| DRV8830_PC_Interface_Functions.c | Performs PC Interface functions between a DRV8830 Motor Driver and the PC Interface |
| DRV8833_Motor_Drive.h [code] | |
| DRV8833_Motor_Drive_API.c | Functions that setup and allow the use of the DRV8833 |
| DRV8833_PC_Interface.h [code] | |
| DRV8833_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for DRV8833 motor drive |
| DRV8833_PC_Interface_Functions.c | Performs PC Interface functions between a DRV8833 Motor Driver and the PC Interface |
| EEPROM24xx128.c | Functions that setup and controls the EEPROM on the MAVRK Pro Motherboard |
| EEPROM24xx128.h [code] | |
| F22x4_ADC10.h [code] | |
| F22x4_Basic_Clock_Plus.h [code] | |
| F22x4_CPU.h [code] | |
| F22x4_DRV8814_DRV8825_Com_Port_Functions.c | Functions that setup and controls the communication interfaces on the MSP430F22x4 on the MAVRK Pro motherboard |
| F22x4_DRV8814_DRV8825_Modular_EVM_IO_Functions.c | Functions that setup and control the I/O (GPIOs and LEDs) for the DRV8814-MVK with an MSP430F22x4 |
| F22x4_DRV8833_Motor_Drive.c | |
| F22x4_interrupts.h [code] | |
| F22x4_io.h [code] | |
| F22x4_Modular_EVM_IO.h [code] | |
| F22x4_system.h [code] | |
| F22x4_Timer.h [code] | |
| F22x4_Timer_A.h [code] | |
| F22x4_Timer_B.h [code] | |
| F22x4_usci.h [code] | |
| F22x4_USCI_Defs.h [code] | |
| F22x4_WDT.h [code] | |
| F5137_ADC12.h [code] | |
| F5137_BQ25504_Device_Interface.h [code] | |
| F5137_Com_Port_Functions.c | |
| F5137_Comparator.h [code] | |
| F5137_CPU.h [code] | |
| F5137_CRC16.c | Functions that setup the CRC Operations for the MSP430F5438 |
| F5137_CRC16.h [code] | |
| F5137_DMA.h [code] | |
| F5137_DRV8830_Motor_Drive.c | Functions that setup and control the I/O (GPIOs and LEDs) for the DRV8833 with the CC430F5137 |
| F5137_DRV8833_Motor_Drive.c | Functions that setup and control the I/O (GPIOs and LEDs) for the DRV8833 with the CC430F5137 |
| F5137_Hardware_Multiplier.h [code] | |
| F5137_interrupts.h [code] | |
| F5137_io.h [code] | |
| F5137_Modular_EVM_IO.h [code] | |
| F5137_Modular_EVM_IO_Functions.c | Functions that setup and controls the I/O (GPIOs and LEDs) for the Modular EVM Board |
| F5137_Modular_EVM_LED_Functions.c | |
| F5137_Power_Management.h [code] | |
| F5137_REF.h [code] | |
| F5137_RF1A.h [code] | |
| F5137_RF1A_Device_Interface.c | Functions that setup and controls the Chipcon Radio CC430F5137 (F5137 MCU + CC1101 Radio) |
| F5137_RF1A_Device_Interface.h [code] | |
| F5137_RF_Micro_Debug_Device_Interface.c | Functions that manage the part specific Device Interface between the MSP430F5438 and the RF_UDEBUG_MVK board |
| F5137_RTC.h [code] | |
| F5137_system.h [code] | |
| F5137_TCA8418_Device_Interface.c | Functions that setup the TI TCA8418 Keypad Scan IC Device with the MSP430F5137 processor |
| F5137_Timer.h [code] | |
| F5137_Timer_A.h [code] | |
| F5137_Unified_Clock_system.h [code] | |
| F5137_US_BQ25504_Interface.c | Functions that setup the microMAVRK sensors |
| F5137_US_DIG_Temp_Interface.c | Functions that interface the micro MAVRK CC430F5137 processor to the US-DIG-TEMP-MVK board with 7 temperature sensors, along with light and humidity sensors |
| F5137_US_DIG_Temp_Interface.h [code] | |
| F5137_usci.h [code] | |
| F5137_usci_Defs.h [code] | |
| F5137_WDT.h [code] | |
| F5438_ADC12.h [code] | |
| F5438_ADS123x_Device_Interface.c | Functions that manage the part specific Device Interface between the MSP430F5438 and the family of ADS1x3x parts |
| F5438_ADS1259_Device_Interface.c | |
| F5438_ADS1x4x_Device_Interface.c | Functions that setup and controls the interfaces for ADS1x4x devices |
| F5438_ADS1x9x_Device_Interface.c | Functions that manage the part specific Device Interface between the MSP430F5438 and the family of ADS1x9x parts |
| F5438_AFE_CARRIER_Device_Interface.c | Functions that setup and controls the AFE Carrier interfaces |
| F5438_AFE_CARRIER_Device_Interface.h [code] | |
| F5438_CC_Device_Interface.c | Functions that setup the Chipcon Radio with the MSP430F5438 processor |
| F5438_CDCE913_Device_Interface.c | Functions that setup and controls the interfaces for ADS1x4x devices |
| F5438_CPU.h [code] | |
| F5438_CRC16.c | Functions that setup the CRC Operations for the MSP430F5438 |
| F5438_CRC16.h [code] | |
| F5438_DMA.h [code] | |
| F5438_Hardware_Multiplier.h [code] | |
| F5438_interrupts.h [code] | |
| F5438_io.h [code] | |
| F5438_PC_Interface.h [code] | |
| F5438_PC_Interface_Functions.c | Performs PC Interface functions between an TMP Sensors and the PC Interface |
| F5438_Power_Management.h [code] | |
| F5438_ProMB_Com_Port_Functions.c | Functions that setup and controls the communication interfaces on the MSP430F5438 on the MAVRK Pro motherboard |
| F5438_ProMB_LED_Functions.c | Functions that setup and control the LED's present on the MSP430 MCU, RF Breakout and AFE Breakout boards when used on the MAVRK Pro Motherboard |
| F5438_ProMB_Modular_EVM_IO.h [code] | |
| F5438_ProMB_Modular_EVM_IO_Functions.c | Functions that setup and control the I/O (GPIOs and LEDs) for the MAVRK Pro Motherboard & F5438 Modular EVM Board combination |
| F5438_REF.h [code] | |
| F5438_RF_Micro_Debug_Device_Interface.c | Functions that manage the part specific Device Interface between the MSP430F5438 and the RF_UDEBUG_MVK board |
| F5438_RTC.h [code] | |
| F5438_system.h [code] | |
| F5438_TCA8418_Device_Interface.c | Functions that setup the TI TCA8418 Keypad Scan IC Device with the MSP430F5438 processor |
| F5438_TCA8418_Device_Interface.h [code] | |
| F5438_Timer.h [code] | |
| F5438_Timer_A.h [code] | |
| F5438_Timer_B.h [code] | |
| F5438_Unified_Clock_system.h [code] | |
| F5438_usci.h [code] | |
| F5438_usci_Defs.h [code] | |
| F5438_WDT.h [code] | |
| ff.c | |
| ff.h [code] | |
| ffconf.h [code] | |
| Flash_Programming.c | Functions that allow to write and read flash memory |
| Flash_Programming.h [code] | |
| Generic_Temp_Sensor.h [code] | |
| Generic_Temp_Sensor_Functions.c | Functions related to TMP20 sensor functionality |
| Generic_Temp_Sensor_PC_Interface_Command_Decode.c | Decodes command coming from the PC |
| Humidity_Sensor.h [code] | |
| Humidity_Sensor_Functions.c | Functionality pertaining to humidity sensor |
| Humidity_Sensor_PC_Interface_Command_Decode.c | Used to decode the commands coming from the PC QT GUI for the humidity sensor |
| I2C_Functions.c | Functions that perform standard read and write to slave devices on the I2C bus |
| I2C_Functions.h [code] | |
| INA220_Current_Power_Monitor.c | Performs |
| INA220_Current_Power_Monitor.h [code] | |
| INA226_Current_Power_Monitor.c | Performs |
| INA226_Current_Power_Monitor.h [code] | |
| init_ADS123x.c | Performs initialization for ADS123x Devices |
| init_ADS1259.c | Performs initialization for ADS1259 Devices |
| init_ADS1x48.c | Performs initialization for ADS1x4x Devices |
| init_ADS1x9x.c | Performs initialization for ADS1x9x Devices |
| init_ADS78xx_ADS83xx.c | Performs initialization for ADS78xx and ADS83xx Devices |
| init_ADS7924.c | |
| init_CC430F5137.c | |
| init_CC_Device.c | Functions that discover and initialize the TI Chipcon Radio |
| init_CDCE913.c | Performs initialization for CDCE913 Programmable 1-PLL VCXO Clock Synthesizer |
| init_DAC7563.c | |
| init_F22x4_ADC10.c | |
| init_F22x4_Basic_Clock_Plus.c | |
| init_F22x4_CPU.c | Functions that setup the MSP430 CPU system |
| init_F22x4_io.c | |
| init_F22x4_Timer_A.c | Set's up the MSP430 Timer A Clock |
| init_F22x4_Timer_B.c | Functions that setup and control the MSP430 Timer B |
| init_F22x4_USCI.c | |
| init_F22x4_USCI_0.c | |
| init_F22x4_WDT.c | Functions that setup the MSP430F22x4 Watch Dog Timer (WDT) |
| init_F5137_ADC12.c | |
| init_F5137_Comparator.c | Functions that setup the MSP430F5137 uC comparator peripheral |
| init_F5137_CPU.c | Functions that setup the MSP430 CPU system |
| init_F5137_DMA.c | Functions that setup the MSP430 DMA system |
| init_F5137_Hardware_Multiplier.c | Functions that setup the MSP430 Multiplier system |
| init_F5137_io.c | Functions that setup the MSP430 GPIO ports |
| init_F5137_Power_Management.c | Functions that setup the MSP430F5137 Power System |
| init_F5137_RF1A.c | Functions that setup the CC430 Radio System |
| init_F5137_RTC.c | Functions that setup the MSP430 Real Time Clock |
| init_F5137_Timer_A_0.c | Functions that setup the MSP430 Timer A0 Clock |
| init_F5137_Timer_A_1.c | Functions that setup the MSP430 Timer A1 Clock |
| init_F5137_Unified_Clock_system.c | Functions that setup the CC430F5137 Unified Clock System |
| init_F5137_USCI.c | Functions that setup the CC430F5137 USCI UART/SPI/I2C port |
| init_F5137_USCI_0.c | Functions that setup the CC430F5137 USCI_0 UART/SPI/I2C port |
| init_F5137_WDT.c | Functions that setup the CC430F5137 Watch Dog Timer (WDT) |
| init_F5438.c | Functions that setup the MSP430F5438A uC peripherals |
| init_F5438_ADC12.c | Functions that setup the MSP430 ADC system |
| init_F5438_BootLoader.c | Functions that setup the MAVRK BootLoader Software |
| init_F5438_CPU.c | Functions that setup the MSP430 CPU system |
| init_F5438_DMA.c | Functions that setup the MSP430 DMA system |
| init_F5438_Hardware_Multiplier.c | Functions that setup the MSP430 Multiplier system |
| init_F5438_io.c | Functions that setup the MSP430 GPIO ports |
| init_F5438_Power_Management.c | Functions that setup the MSP430F5438A Power System |
| init_F5438_RTC.c | Functions that setup the MSP430 Real Time Clock |
| init_F5438_Timer_A_0.c | Functions that setup the MSP430 Timer A0 Clock |
| init_F5438_Timer_A_1.c | Functions that setup the MSP430 Timer A1 Clock |
| init_F5438_Timer_B_0.c | Functions that setup the MSP430 Timer B0 Clock |
| init_F5438_Unified_Clock_system.c | Functions that setup the MSP430F5438A Unified Clock System |
| init_F5438_USCI.c | Functions that setup the MSP430F5438A USCI UART/SPI/I2C port |
| init_F5438_USCI_0.c | Functions that setup the MSP430F5438A USCI_0 UART/SPI/I2C port |
| init_F5438_USCI_1.c | Functions that setup the MSP430F5438A USCI_1 UART/SPI/I2C port |
| init_F5438_USCI_2.c | Functions that setup the MSP430F5438A USCI_2 UART/SPI/I2C port |
| init_F5438_USCI_3.c | Functions that setup the MSP430F5438A USCI_3 UART/SPI/I2C port |
| init_F5438_WDT.c | Functions that setup the MSP430F5438A Watch Dog Timer (WDT) |
| init_INA220.c | Performs initialization of the INA220 Current and Power Monitoring device |
| init_INA226.c | Performs initialization of the INA226 Current and Power Monitoring device |
| init_MSP430F22x4.c | Functions that setup the MSP430F22x4 uC peripherals |
| init_MSP430F5438.c | Functions that setup the MSP430F5137 uC peripherals |
| init_PGA280.c | Performs initialization for PGA280 Devices |
| init_TCA8418.c | |
| init_TMP112.c | Performs initialization for TMP112 Temperature Sensor Device |
| init_TPA2038.c | Performs initialization for TPA2038 Devices |
| integer.h [code] | |
| Light_Sensor.h [code] | |
| Light_Sensor_Functions.c | Used for light sensor functions that perform various light sensor tasks |
| Light_Sensor_PC_Interface_Command_Decode.c | Used to decode commands comming from the PC QT interface, specifically for the lights sensor |
| MAVRK_Arch.h [code] | |
| MAVRK_Common.c | Functions that perform the common functions to collect error and perform timed delay loops |
| MAVRK_Common.h [code] | |
| MAVRK_Network.h [code] | |
| MAVRK_Network_API.c | High level functions interfacing to various network types |
| MAVRK_Return_Error_Codes.h [code] | |
| MAVRK_Test_Utilities.c | |
| MAVRK_Test_Utilities.h [code] | |
| MICRO_MAVRK_Device_Interface.h [code] | |
| MICRO_MAVRK_PC_Interface_Command_Decode.c | |
| MICRO_MAVRK_PC_Interface_Functions.c | |
| mmc.c | |
| mmc.h [code] | |
| Motor_Drive_Command_Interface.h [code] | |
| Motor_Drive_Command_Interface_Functions.c | Performs PC Interface functions between an TMP Sensors and the PC Interface |
| Packet_Sniffer_API.c | High Level Functions related to the Packet Sniffer |
| Packet_Sniffer_Command_Decode.c | Setup the interface between the Chipcon Radio part and the PC Application |
| Packet_Sniffer_PC_Interface.h [code] | |
| Packet_Sniffer_PC_Interface_Functions.c | Performs PC Interface functions between an Chipcon Radio and the PC Interface |
| Passive_Sensor.h [code] | |
| Passive_Sensor_API.c | Performs PC Interface functions between a Passive Sensor part and the PC Interface |
| PC_Interface.h [code] | |
| PC_Interface_Functions.c | Performs generic PC Interface functions between a standard MAVRK device and the PC Interface |
| PC_Interface_Radio_Encapsulation.c | Contains functions for encapsulating PC interface packets by radio network packets for transmission wirelessly |
| PGA280.h [code] | |
| PGA280_Functions.c | Functions that setup the PGA280 device for operations |
| PGA280_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for PGA280 Programmable Gain Amplifier |
| PGA280_PC_Interface_Functions.c | Performs PC Interface functions between an PGA280 and the PC Interface |
| PGA280_SPI_Functions.c | |
| PMU_Seven_Segment.h [code] | |
| PMU_Seven_Segment_LED_Functions.c | Functions that setup and control the Seven Segment LED driver for the PMU BAT Board |
| RF_1A_constants.c | |
| RF_1A_Device_Status.c | |
| RF_1A_Interface_Functions.c | |
| RF_1A_Radio_Functions.c | |
| RF_Micro_Debug_Device_Interface.h [code] | |
| RS485_Network.h [code] | |
| RS485_RS232_Functions.c | Functions for using the RS485 and RS232 devices on the SCI-RS485-232-MVK module |
| RSSI_Scanner.h [code] | |
| RSSI_Scanner_Functions.c | High Level Functions related to the RSSI scanner |
| SCI_Carrier.h [code] | |
| SCI_Carrier_API.c | API's for setting up the SCI Carrier |
| SD_Hardware.h [code] | |
| SD_Hardware_Layer_F5137.c | Function for low level interface to memory |
| SD_Hardware_Layer_F5438.c | Function for low level interface to memory |
| SD_Memory.h [code] | |
| SD_Memory_API.c | Functions for high level interface to memory |
| Serial_Cooperative_Threader.c | |
| Serial_Cooperative_Threader.h [code] | |
| SPI_Functions.c | Functions that perform standard read or writes to devices on the SPI bus |
| SPI_Functions.h [code] | |
| stdef.h [code] | |
| TCA8418_Key_Scan.c | API's for the MAVRK RF-TCA8418-MVK Module (TCA8418 I2C CONTROLLED KEYPAD SCAN IC) |
| TCA8418_Key_Scan.h [code] | |
| TCA8418_Key_Scan_API.c | High Level Functions related to the TCA8418 Keyboard Scanner |
| TCA8418_PC_Interface.h [code] | |
| TCA8418_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for TCA8418 key scanner |
| TCA8418_PC_Interface_Functions.c | Performs PC Interface functions between an TCA8418 Keypad Scanner and the PC Interface |
| TCA_PCA_I2C_IO_Expander.c | API's for the TCA_PCA I2C -> GPIO Expander |
| TCA_PCA_I2C_IO_Expander.h [code] | |
| TMP103_Temp_Sensor.c | Perform interactions with the TMP103 via the I2C bus |
| TMP103_Temp_Sensor.h [code] | |
| TMP106_Temp_Sensor.c | Perform interactions with the TMP106 via the I2C bus |
| TMP106_Temp_Sensor.h [code] | |
| TMP112_PC_Interface.h [code] | |
| TMP112_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for TMP112 TMP Sensors |
| TMP112_PC_Interface_Functions.c | Performs PC Interface functions between an TMP112 Sensors and the PC Interface |
| TMP112_Temp_Sensor.c | Perform interactions with the TMP112 via the I2C bus |
| TMP112_Temp_Sensor.h [code] | |
| TMP_Sensor_PC_Interface.h [code] | |
| TMP_Sensor_PC_Interface_Functions.c | Performs PC Interface functions between an TMP Sensors and the PC Interface |
| TPA2038.h [code] | |
| TPA2038_Constant_Tables.c | |
| TPA2038_Functions.c | Functions that setup the TPA2038 device for operations |
| TPA2038_PC_Interface.h [code] | |
| TPA2038_PC_Interface_Command_Decode.c | Setup the interface from the MAVRK board to the PC Application for TPA2038 Audio Amplifier |
| TPA2038_PC_Interface_Functions.c | Performs PC Interface functions between a TPA2038 Audio Amplifier and the PC Interface |
| TPL0401.h [code] | |
| TPL0401_Functions.c | Functions that setup the TPL0401 device for operations |
| UART_PC_Int_Threader.c | Register File to set up UART that is intended to talk back and forth with the PC based GUI software |
| UART_State_Machine.c | Register File to set up UART State Machine |
| UART_State_Machine.h [code] | |
| US_DIG_Temp_Interface.c | General functions that interface the US-DIG-TEMP-MVK board with 7 temperature sensors along with light and humidity sensors to the project routines |
| US_DIG_Temp_Interface.h [code] | |
| Wired_Serial_Half_Duplex_Network.c | Functionality for a wired serial half duplex network implemented currently using the RS485 transceiver |
| Wired_Serial_Network.h [code] | |
| Wireless_Frequency_Hopping.h [code] | |
| Wireless_Frequency_Hopping_Network.c | API for wireless frequency hopping systems |
| Wireless_Network.c | Functionality for the original radio network |
| Wireless_Network.h [code] | |
| Wireless_Network_Common.c | Common functions for the wireless network |
| Wireless_Network_Common.h [code] |
1.7.3