SimpleLink MCU SDK Driver APIs
tidrivers_msp43x_3_01_01_03
|
CaptureMSP432 Hardware Attributes. More...
#include <CaptureMSP432.h>
Data Fields | |
uint32_t | timerBaseAddress |
uint32_t | clockSource |
uint32_t | clockDivider |
uint32_t | capturePort |
uint32_t | intPriority |
CaptureMSP432 Hardware Attributes.
Capture hardware attributes that tell the CaptureMSP432 driver specific hardware configurations and interrupt/priority settings.
A sample structure is shown below:
uint32_t CaptureMSP432_HWAttrs::timerBaseAddress |
uint32_t CaptureMSP432_HWAttrs::clockSource |
uint32_t CaptureMSP432_HWAttrs::clockDivider |
uint32_t CaptureMSP432_HWAttrs::capturePort |
uint32_t CaptureMSP432_HWAttrs::intPriority |