TI-RTOS for TivaC  2.14.04.31
Data Structures | Typedefs | Variables
UARTCC3200.h File Reference

Detailed Description

UART driver implementation for a CC3200 UART controller.

============================================================================

Stack requirements

The UARTCC3200 driver is (ring) buffered driver where it stores data it may already received in a user-supplied background buffer.

See also
UARTCC3200_HWAttrs

While permitted, it is STRONGLY suggested to avoid implementations where you call UART_read() within it own callback function (when in UART_MODE_CALLBACK).

Doing so, will require additional (task and system) stack for each nested UART_read() call.

Tool chain Number of bytes per nested UART_read() call
GNU 96 bytes + callback function stack requirements
IAR 40 bytes + callback function stack requirements
TI 80 bytes + callback function stack requirements

It is important to note a potential worst case scenario: A full ring buffer with data; say 32 bytes The callback function calls UART_read() with a size of 1 (byte) No other variables are allocated in the callback function No other function calls are made in the callback function

As a result, you need an additional task and system stack of: 32 bytes * (80 bytes for TI + 0 bytes by the callback function) = 2.5kB

The UART header file should be included in an application as follows:


#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ports/ClockP.h>
#include <ti/drivers/ports/HwiP.h>
#include <ti/drivers/ports/SemaphoreP.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/uart/RingBuf.h>
Include dependency graph for UARTCC3200.h:

Go to the source code of this file.

Data Structures

struct  UARTCC3200_FxnSet
 Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only. More...
 
struct  UARTCC3200_HWAttrs
 UARTCC3200 Hardware attributes. More...
 
struct  UARTCC3200_Object
 UARTCC3200 Object. More...
 

Typedefs

typedef struct UARTCC3200_FxnSet UARTCC3200_FxnSet
 Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only. More...
 
typedef struct UARTCC3200_HWAttrs UARTCC3200_HWAttrs
 UARTCC3200 Hardware attributes. More...
 
typedef struct UARTCC3200_Object UARTCC3200_Object
 UARTCC3200 Object. More...
 
typedef struct UARTCC3200_ObjectUARTCC3200_Handle
 

Variables

const UART_FxnTable UARTCC3200_fxnTable
 

Typedef Documentation

Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only.

These functions should not be used by the user and are solely intended for the UARTCC3200 driver. The UARTCC3200_FxnSet is a pair of complement functions that are design to operate with one another in a task context and in an ISR context. The readTaskFxn is called by UARTCC3200_read() to drain a circular buffer, whereas the readIsrFxn is used by the UARTCC3200_hwiIntFxn to fill up the circular buffer.

readTaskFxn: Function called by UART read These variables are set and avilalable for use to the readTaskFxn. object->readBuf = buffer; //Pointer to a user buffer object->readSize = size; //Desired no. of bytes to read object->readCount = size; //Remaining no. of bytes to read

readIsrFxn: The required ISR counterpart to readTaskFxn

UARTCC3200 Hardware attributes.

The fields, baseAddr, intNum, and flowControl, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC3200Ware these definitions are found in:

  • inc/hw_memmap.h
  • inc/hw_ints.h
  • driverlib/uart.h

intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

A sample structure is shown below:

1 unsigned char uartCC3200RingBuffer[2][32];
2 
3 const UARTCC3200_HWAttrs uartCC3200HWAttrs[] = {
4  {
5  .baseAddr = UARTA0_BASE,
6  .intNum = INT_UARTA0,
7  .intPriority = (~0),
8  .flowControl = UART_FLOWCONTROL_NONE,
9  .ringBufPtr = uartCC3200RingBuffer[0],
10  .ringBufSize = sizeof(uartCC3200RingBuffer[0])
11  },
12  {
13  .baseAddr = UARTA1_BASE,
14  .intNum = INT_UARTA1,
15  .intPriority = (~0),
16  .flowControl = UART_FLOWCONTROL_TX | UART_FLOWCONTROL_RX,
17  .ringBufPtr = uartCC3200RingBuffer[1],
18  .ringBufSize = sizeof(uartCC3200RingBuffer[1])
19  },
20 };

UARTCC3200 Object.

The application must not access any member variables of this structure!

Variable Documentation

const UART_FxnTable UARTCC3200_fxnTable
Copyright 2015, Texas Instruments Incorporated