TI-RTOS for TivaC  2.14.04.31
UARTCC3200.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
73 #ifndef ti_drivers_uart_UARTCC3200__include
74 #define ti_drivers_uart_UARTCC3200__include
75 
76 #ifdef __cplusplus
77 extern "C" {
78 #endif
79 
80 #include <stdint.h>
81 #include <stdbool.h>
82 
83 #include <ti/drivers/ports/ClockP.h>
84 #include <ti/drivers/ports/HwiP.h>
85 #include <ti/drivers/ports/SemaphoreP.h>
86 #include <ti/drivers/Power.h>
87 #include <ti/drivers/UART.h>
88 #include <ti/drivers/uart/RingBuf.h>
89 
90 /* UART function table pointer */
92 
114 typedef struct UARTCC3200_FxnSet {
115  bool (*readIsrFxn) (UART_Handle handle);
116  int (*readTaskFxn) (UART_Handle handle);
118 
163 typedef struct UARTCC3200_HWAttrs {
165  unsigned int baseAddr;
167  unsigned int intNum;
169  unsigned int intPriority;
171  uint32_t flowControl;
173  unsigned char *ringBufPtr;
175  size_t ringBufSize;
177 
183 typedef struct UARTCC3200_Object {
184  /* UART state variable */
185  struct {
186  bool opened:1; /* Has the obj been opened */
187  UART_Mode readMode:1; /* Mode for all read calls */
188  UART_Mode writeMode:1; /* Mode for all write calls */
189  UART_DataMode readDataMode:1; /* Type of data being read */
190  UART_DataMode writeDataMode:1; /* Type of data being written */
191  UART_ReturnMode readReturnMode:1; /* Receive return mode */
192  UART_Echo readEcho:1; /* Echo received data back */
193  /*
194  * Flag to determine if a timeout has occurred when the user called
195  * UART_read(). This flag is set by the timeoutClk clock object.
196  */
197  bool bufTimeout:1;
198  /*
199  * Flag to determine when an ISR needs to perform a callback; in both
200  * UART_MODE_BLOCKING or UART_MODE_CALLBACK
201  */
202  bool callCallback:1;
203  /*
204  * Flag to determine if the ISR is in control draining the ring buffer
205  * when in UART_MODE_CALLBACK
206  */
207  bool drainByISR:1;
208  /* Flag to keep the state of the read Power constraints */
209  bool rxEnabled:1;
210  /* Flag to keep the state of the write Power constraints */
211  bool txEnabled:1;
212  } state;
213 
214  HwiP_Handle hwiHandle; /* Hwi handle for interrupts */
215  ClockP_Handle timeoutClk; /* Clock object to for timeouts */
216  uint32_t baudRate; /* Baud rate for UART */
217  UART_LEN dataLength; /* Data length for UART */
218  UART_STOP stopBits; /* Stop bits for UART */
219  UART_PAR parityType; /* Parity bit type for UART */
220 
221  /* UART read variables */
222  RingBuf_Object ringBuffer; /* local circular buffer object */
223  /* A complement pair of read functions for both the ISR and UART_read() */
225  unsigned char *readBuf; /* Buffer data pointer */
226  size_t readSize; /* Desired number of bytes to read */
227  size_t readCount; /* Number of bytes left to read */
228  SemaphoreP_Handle readSem; /* UART read semaphore */
229  unsigned int readTimeout; /* Timeout for read semaphore */
230  UART_Callback readCallback; /* Pointer to read callback */
231 
232  /* UART write variables */
233  const unsigned char *writeBuf; /* Buffer data pointer */
234  size_t writeSize; /* Desired number of bytes to write*/
235  size_t writeCount; /* Number of bytes left to write */
236  SemaphoreP_Handle writeSem; /* UART write semaphore*/
237  unsigned int writeTimeout; /* Timeout for write semaphore */
238  UART_Callback writeCallback; /* Pointer to write callback */
239  unsigned int writeEmptyClkTimeout; /* TX FIFO timeout tick count */
240 
241  /* For Power management */
242  ClockP_Handle txFifoEmptyClk; /* UART TX FIFO empty clock */
243  Power_NotifyObj postNotify; /* LPDS wake-up notify object */
245 
246 #ifdef __cplusplus
247 }
248 #endif
249 
250 #endif /* ti_drivers_uart_UARTCC3200__include */
HwiP_Handle hwiHandle
Definition: UARTCC3200.h:214
UART_STOP
UART stop bit settings.
Definition: UART.h:379
size_t writeCount
Definition: UARTCC3200.h:235
bool callCallback
Definition: UARTCC3200.h:202
size_t readSize
Definition: UARTCC3200.h:226
bool(* readIsrFxn)(UART_Handle handle)
Definition: UARTCC3200.h:115
UART_Echo readEcho
Definition: UARTCC3200.h:192
struct UARTCC3200_FxnSet UARTCC3200_FxnSet
Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only.
UART_LEN dataLength
Definition: UARTCC3200.h:217
unsigned int writeTimeout
Definition: UARTCC3200.h:237
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:497
UART_PAR parityType
Definition: UARTCC3200.h:219
UART_PAR
UART parity type settings.
Definition: UART.h:389
bool opened
Definition: UARTCC3200.h:186
UART_Mode
UART mode settings.
Definition: UART.h:291
bool drainByISR
Definition: UARTCC3200.h:207
uint32_t baudRate
Definition: UARTCC3200.h:216
UART_DataMode
UART data mode settings.
Definition: UART.h:339
UART_ReturnMode
UART return mode settings.
Definition: UART.h:324
bool rxEnabled
Definition: UARTCC3200.h:209
UART_Mode readMode
Definition: UARTCC3200.h:187
UART_Echo
UART echo settings.
Definition: UART.h:357
size_t ringBufSize
Definition: UARTCC3200.h:175
UART_Callback readCallback
Definition: UARTCC3200.h:230
int(* readTaskFxn)(UART_Handle handle)
Definition: UARTCC3200.h:116
struct UARTCC3200_Object UARTCC3200_Object
UARTCC3200 Object.
SemaphoreP_Handle writeSem
Definition: UARTCC3200.h:236
struct UARTCC3200_Object::@0 state
ClockP_Handle txFifoEmptyClk
Definition: UARTCC3200.h:242
unsigned int baseAddr
Definition: UARTCC3200.h:165
UART_DataMode readDataMode
Definition: UARTCC3200.h:189
RingBuf_Object ringBuffer
Definition: UARTCC3200.h:222
unsigned int intPriority
Definition: UARTCC3200.h:169
UARTCC3200_FxnSet readFxns
Definition: UARTCC3200.h:224
unsigned char * readBuf
Definition: UARTCC3200.h:225
UART_DataMode writeDataMode
Definition: UARTCC3200.h:190
Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only.
Definition: UARTCC3200.h:114
UARTCC3200 Object.
Definition: UARTCC3200.h:183
bool txEnabled
Definition: UARTCC3200.h:211
UART driver interface.
UART_Callback writeCallback
Definition: UARTCC3200.h:238
uint32_t flowControl
Definition: UARTCC3200.h:171
struct UARTCC3200_HWAttrs UARTCC3200_HWAttrs
UARTCC3200 Hardware attributes.
ClockP_Handle timeoutClk
Definition: UARTCC3200.h:215
void(* UART_Callback)(UART_Handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:284
UARTCC3200 Hardware attributes.
Definition: UARTCC3200.h:163
unsigned int readTimeout
Definition: UARTCC3200.h:229
unsigned char * ringBufPtr
Definition: UARTCC3200.h:173
UART_LEN
UART data length settings.
Definition: UART.h:367
size_t readCount
Definition: UARTCC3200.h:227
UART_Mode writeMode
Definition: UARTCC3200.h:188
Power_NotifyObj postNotify
Definition: UARTCC3200.h:243
struct UARTCC3200_Object * UARTCC3200_Handle
const UART_FxnTable UARTCC3200_fxnTable
unsigned int intNum
Definition: UARTCC3200.h:167
UART_ReturnMode readReturnMode
Definition: UARTCC3200.h:191
const unsigned char * writeBuf
Definition: UARTCC3200.h:233
size_t writeSize
Definition: UARTCC3200.h:234
UART Global configuration.
Definition: UART.h:540
SemaphoreP_Handle readSem
Definition: UARTCC3200.h:228
bool bufTimeout
Definition: UARTCC3200.h:197
unsigned int writeEmptyClkTimeout
Definition: UARTCC3200.h:239
UART_STOP stopBits
Definition: UARTCC3200.h:218
Copyright 2015, Texas Instruments Incorporated