TI-RTOS for TivaC  2.14.04.31
Data Fields
UARTCC3200_HWAttrs Struct Reference

UARTCC3200 Hardware attributes. More...

#include <UARTCC3200.h>

Data Fields

unsigned int baseAddr
 
unsigned int intNum
 
unsigned int intPriority
 
uint32_t flowControl
 
unsigned char * ringBufPtr
 
size_t ringBufSize
 

Detailed Description

UARTCC3200 Hardware attributes.

The fields, baseAddr, intNum, and flowControl, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC3200Ware these definitions are found in:

intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

A sample structure is shown below:

unsigned char uartCC3200RingBuffer[2][32];
const UARTCC3200_HWAttrs uartCC3200HWAttrs[] = {
{
.baseAddr = UARTA0_BASE,
.intNum = INT_UARTA0,
.intPriority = (~0),
.flowControl = UART_FLOWCONTROL_NONE,
.ringBufPtr = uartCC3200RingBuffer[0],
.ringBufSize = sizeof(uartCC3200RingBuffer[0])
},
{
.baseAddr = UARTA1_BASE,
.intNum = INT_UARTA1,
.intPriority = (~0),
.flowControl = UART_FLOWCONTROL_TX | UART_FLOWCONTROL_RX,
.ringBufPtr = uartCC3200RingBuffer[1],
.ringBufSize = sizeof(uartCC3200RingBuffer[1])
},
};

Field Documentation

unsigned int UARTCC3200_HWAttrs::baseAddr

UART Peripheral's base address

unsigned int UARTCC3200_HWAttrs::intNum

UART Peripheral's interrupt vector

unsigned int UARTCC3200_HWAttrs::intPriority

UART Peripheral's interrupt priority

uint32_t UARTCC3200_HWAttrs::flowControl

Hardware flow control setting defined by driverlib

unsigned char* UARTCC3200_HWAttrs::ringBufPtr

Pointer to an application ring buffer

size_t UARTCC3200_HWAttrs::ringBufSize

Size of ringBufPtr


The documentation for this struct was generated from the following file:
Copyright 2015, Texas Instruments Incorporated