J784S4 SA3UL Firewall Descriptions

Introduction

This chapter provides information on firewalls that system firmware configures for the crypto-accelerator SAUL by default at boot time for HS devices. The reasons for choosing specific firewalls and/or regions to configure during system firmware initialization are internal. The guide to read the tables in this chapter is provided below. For more details on firewalls, refer to the “Interconnect Firewalls” section of the TRM and Firewall TISCI Description. For more details on SAUL access, please refer to SAUL Access Outside of SYSFW.

Table Legend

  • Firewall ID: The unique identifier for each firewall
  • Owner: The host ID that owns the firewall
  • CBA_PERMISSION_x: Each permission slot takes the form of [user, permission], where “user” is a host ID and “permission” is a combination of r-read, w-write, c-cache, d-debug. Additionally, each firewall region/channel can have up to 3 slots for configuring permissions.

Table Guide

  • If a firewall is owned by TIFS/DMSC, it means that only TIFS/DMSC can configure it.
  • If a firewall is owned by none, it means any host can configure it.
  • If a firewall is owned by rm, it means that the corresponding resource is managed by the resource manager based on the RM boardcfg.

Note

For additional firewall information, checkout the Firewall FAQ.

List of Region Based SAUL Firewalls

Firewall ID Region Owner Background/Foreground Region Dev Group Start Address End Address CBA_PERMISSION_0 CBA_PERMISSION_1 CBA_PERMISSION_2
1196 0 tifs Foreground SOC_DEVGRP_MCU_WAKEUP 0x40900000 0x40900FFF tifs,rwd everyone,r  
1196 1 tifs Foreground SOC_DEVGRP_MCU_WAKEUP 0x40901000 0x409011FF tifs,rwd hsm,r  
1196 2 none Foreground SOC_DEVGRP_MCU_WAKEUP 0x4070C000 0x4070C3FF everyone,rwd    
1196 3 none Foreground SOC_DEVGRP_MCU_WAKEUP 0x40910000 0x4091007F everyone,rwd    
1196 4 tifs Foreground SOC_DEVGRP_MCU_WAKEUP 0x40920000 0x4092FFFF tifs,rwd