![]() |
![]() |
AESECBLPF3 Object. More...
#include <AESECBLPF3.h>
Data Fields | |
AESCommonLPF3_Object | common |
AESECB_Operation * | operation |
AESECB_CallbackFxn | callbackFxn |
AESECB_OperationType | operationType |
bool | threadSafe |
const uint8_t * | input |
uint8_t * | output |
size_t | inputLength |
size_t | totalDataLength |
volatile size_t | totalDataLengthRemaining |
int_fast16_t | hsmStatus |
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly. More... | |
bool | segmentedOperationInProgress |
AESECBLPF3 Object.
The application must not access any member variables of this structure!
AESCommonLPF3_Object AESECBLPF3_Object::common |
AESECB_Operation* AESECBLPF3_Object::operation |
AESECB_CallbackFxn AESECBLPF3_Object::callbackFxn |
AESECB_OperationType AESECBLPF3_Object::operationType |
bool AESECBLPF3_Object::threadSafe |
const uint8_t* AESECBLPF3_Object::input |
uint8_t* AESECBLPF3_Object::output |
size_t AESECBLPF3_Object::inputLength |
size_t AESECBLPF3_Object::totalDataLength |
volatile size_t AESECBLPF3_Object::totalDataLengthRemaining |
int_fast16_t AESECBLPF3_Object::hsmStatus |
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
bool AESECBLPF3_Object::segmentedOperationInProgress |